BootloaderHeader_t Struct ReferenceApplication Interface > Common Application Interface
Description
Common header for bootloader tables.
Definition at line 115
of file btl_interface.h
.
#include <
btl_interface.h
>
Data Fields | |
uint32_t | type |
Type of image. | |
uint32_t | layout |
Version number of the bootloader/application table. | |
uint32_t | version |
Version number of the image. | |
The documentation for this struct was generated from the following file:
btl_interface.h