GblInputBuffer_t Struct ReferenceComponents > Image Parser > GBL Parser
Description
GBL parser input buffer.
Definition at line 263
of file btl_gbl_parser.h
.
#include <
btl_gbl_parser.h
>
Data Fields | |
const uint8_t * | buffer |
Pointer to a buffer. | |
const size_t | length |
Length of the buffer. | |
size_t | offset |
Offset of the buffer. | |
The documentation for this struct was generated from the following file:
btl_gbl_parser.h