BootloaderStorageImplementationInformation_t Struct ReferenceApplication Interface > Application Storage Interface
Description
Information about the bootloader storage implementation Note: From Gecko Bootloader version >= 2.1, the pointer partType will only contain a zero value. The partType variable can be used to find information about the attached storage.
Definition at line 66
of file btl_interface_storage.h
.
#include <
btl_interface_storage.h
>
Data Fields | |
uint16_t | version |
The version of this data structure. | |
uint16_t | capabilitiesMask |
A bitmask describing the capabilities of this particular storage. | |
uint32_t | pageEraseMs |
Maximum time it takes to erase a page. (in milliseconds) | |
uint32_t | partEraseMs |
Maximum time it takes to erase the entire part. (in milliseconds) | |
uint32_t | pageSize |
The size of a single erasable page in bytes. | |
uint32_t | partSize |
The total size of the storage in bytes. | |
char * | partDescription |
Pointer to a string describing the attached storage. | |
uint8_t | wordSizeBytes |
The number of bytes in a word for the storage. | |
uint32_t | partType |
Value representing the attached storage. | |
The documentation for this struct was generated from the following file:
btl_interface_storage.h