ApplicationProperties_t Struct ReferenceApplication Interface > Application Properties
Description
Application Properties struct.
Definition at line 122
of file application_properties.h
.
#include <
application_properties.h
>
Data Fields | |
uint8_t | magic [16] |
Magic value indicating this is an ApplicationProperties_t struct. Must equal APPLICATION_PROPERTIES_MAGIC. | |
uint32_t | structVersion |
Version number of this struct. | |
uint32_t | signatureType |
Type of signature this application is signed with. | |
uint32_t | signatureLocation |
Location of the signature. Typically points to the end of the application. | |
ApplicationData_t | app |
Information about the application. | |
ApplicationCertificate_t * | cert |
Pointer to information about the certificate. | |
uint8_t * | longTokenSectionAddress |
Pointer to Long Token Data Section. | |
const uint8_t | decryptKey [16] |
Parser Decryption Key. | |
The documentation for this struct was generated from the following file:
application_properties.h