BootloaderResetCause_t Struct ReferenceApplication Interface > Common Application Interface > Reset Information

Description

Reset cause of the bootloader.

Definition at line 54 of file btl_reset_info.h .

#include < btl_reset_info.h >

Data Fields

uint16_t reason
Reset reason as defined in the reset information .
uint16_t signature
Signature indicating whether the reset reason is valid.

The documentation for this struct was generated from the following file:
  • btl_reset_info.h