BootloaderInformation_t Struct ReferenceApplication Interface > Common Application Interface

Description

Information about the current bootloader.

Definition at line 105 of file btl_interface.h .

#include < btl_interface.h >

Data Fields

BootloaderType_t type
The type of bootloader.
uint32_t version
Version number of the bootloader.
uint32_t capabilities
Capability mask for the bootloader.

The documentation for this struct was generated from the following file:
  • btl_interface.h