AesCtrContext Struct ReferenceComponents > Security > AES
Description
Context variable type for AES-CTR (and AES-CCM)
Definition at line 52
of file btl_security_types.h
.
#include <
btl_security_types.h
>
Data Fields | |
sl_se_key_descriptor_t | aesKeyDesc |
SE Manager Key descriptor. | |
mbedtls_aes_context | aesContext |
mbedTLS AES context | |
size_t | offsetInBlock |
Position in block of last byte en/decrypted. | |
uint8_t | streamBlock [16] |
Current CTR encrypted block. | |
uint8_t | counter [16] |
Current counter/CCM value. | |
The documentation for this struct was generated from the following file:
btl_security_types.h