Reset InformationApplication Interface > Common Application Interface
Description
Passing information when resetting into and out of the bootloader.
To signal the bootloader to run, the application needs to write the BootloaderResetCause_t structure to the first address of RAM, setting BootloaderResetCause_t::reason to BOOTLOADER_RESET_REASON_BOOTLOAD.
The reset cause is only valid if BootloaderResetCause_t::signature is set to BOOTLOADER_RESET_SIGNATURE_VALID.
When the bootloader reboots back into the app, it sets the reset reason to BOOTLOADER_RESET_REASON_GO if the bootload succeeded, or BOOTLOADER_RESET_REASON_BADIMAGE if the bootload failed due to errors when parsing the upgrade image.
- Note
- The reset information is automatically filled out before reset if the bootloader_rebootAndInstall function is called.
Data Structures | |
struct | BootloaderResetCause_t |
Reset cause of the bootloader. | |
Macros | |
#define | BOOTLOADER_RESET_REASON_UNKNOWN 0x0200u |
Unknown bootloader cause (should never occur) | |
#define | BOOTLOADER_RESET_REASON_GO 0x0201u |
Bootloader caused reset telling app to run. | |
#define | BOOTLOADER_RESET_REASON_BOOTLOAD 0x0202u |
Application requested that bootloader runs. | |
#define | BOOTLOADER_RESET_REASON_BADIMAGE 0x0203u |
Bootloader detected bad external upgrade image. | |
#define | BOOTLOADER_RESET_REASON_FATAL 0x0204u |
Fatal Error or assert in bootloader. | |
#define | BOOTLOADER_RESET_REASON_FORCE 0x0205u |
Forced bootloader activation. | |
#define | BOOTLOADER_RESET_REASON_OTAVALID 0x0206u |
OTA Bootloader mode activation. | |
#define | BOOTLOADER_RESET_REASON_DEEPSLEEP 0x0207u |
Bootloader initiated deep sleep. | |
#define | BOOTLOADER_RESET_REASON_BADAPP 0x0208u |
Application verification failed. | |
#define | BOOTLOADER_RESET_REASON_UPGRADE 0x0209u |
Bootloader requested that first stage upgrades main bootloader. | |
#define | BOOTLOADER_RESET_REASON_TIMEOUT 0x020Au |
Bootloader timed out waiting for upgrade image. | |
#define | BOOTLOADER_RESET_REASON_FAULT 0x020Bu |
Soft-reset was forced to handle a fault. | |
#define | BOOTLOADER_RESET_REASON_TZ_FAULT 0x020Cu |
Soft-reset was forced to handle a security fault. | |
#define | BOOTLOADER_RESET_SIGNATURE_VALID 0xF00Fu |
Reset signature is valid. | |
#define | BOOTLOADER_RESET_SIGNATURE_INVALID 0xC33Cu |
Reset signature is invalid. | |