FlashBootloader Core
Description
Interface to internal flash.
Used for writing application images to the main flash.
Macros | |
#define | SL_GBL_MSC_LDMA_CHANNEL 2 |
DMA Channel for MSC write. | |
Functions | |
bool | flash_erasePage (uint32_t address) |
bool | flash_writeBuffer_dma (uint32_t address, void *data, size_t length, int ch) |
bool | flash_writeBuffer (uint32_t address, void *data, size_t length) |
Function Documentation
bool flash_erasePage | ( | uint32_t | address | ) |
Erase a flash page.
- Parameters
-
[in] address
Start address of the flash page to erase.
- Returns
- True if operation was successful
bool flash_writeBuffer_dma | ( | uint32_t | address, |
void * | data, |
||
size_t | length, |
||
int | ch |
||
) |
Write buffer to internal flash.
- Parameters
-
address
Starting address to write data to. Must be half-word aligned. data
Data buffer to write to internal flash length
Amount of bytes in the data buffer to write ch
DMA channel to use
- Returns
- True if operation was successful
bool flash_writeBuffer | ( | uint32_t | address, |
void * | data, |
||
size_t | length |
||
) |
Write buffer to internal flash.
- Parameters
-
address
Starting address to write data to. Must be half-word aligned. data
Data buffer to write to internal flash length
Amount of bytes in the data buffer to write
- Returns
- True if operation was successful