BootloaderStorageInformation_t Struct ReferenceApplication Interface > Application Storage Interface
Description
Information about the bootloader storage
Note: The flashInfo variable is only usable with Gecko Bootloader version >= 2.0. All previous versions of the Gecko Bootloader do not support the flashInfo data field.
Definition at line 91
of file btl_interface_storage.h
.
#include <
btl_interface_storage.h
>
Data Fields | |
uint32_t | version |
The version of this data structure. | |
uint32_t | capabilities |
The capabilities of the storage component. | |
BootloaderStorageType_t | storageType |
Type of storage. | |
uint32_t | numStorageSlots |
Number of storage slots. | |
BootloaderStorageImplementationInformation_t * | info |
A pointer to detailed information about the attached storage. | |
BootloaderStorageImplementationInformation_t | flashInfo |
Detailed information about the attached storage(available for use only with Gecko Bootloader version >= 2.0) | |
The documentation for this struct was generated from the following file:
btl_interface_storage.h