em_can.h File Reference
Controller Area Network API.
- Version
- 5.5.0
License
Copyright 2016 Silicon Laboratories, Inc. www.silabs.com
Permission is granted to anyone to use this software for any purpose, including commercial applications, and to alter it and redistribute it freely, subject to the following restrictions:
- The origin of this software must not be misrepresented; you must not claim that you wrote the original software.
- Altered source versions must be plainly marked as such, and must not be misrepresented as being the original software.
- This notice may not be removed or altered from any source distribution.
DISCLAIMER OF WARRANTY/LIMITATION OF REMEDIES: Silicon Labs has no obligation to support this Software. Silicon Labs is providing the Software "AS IS", with no express or implied warranties of any kind, including, but not limited to, any implied warranties of merchantability or fitness for any particular purpose or warranties against infringement of any proprietary rights of a third party.
Silicon Labs will not be liable for any consequential, incidental, or special damages, or any other relief, or for any claim by any third party, arising from your use of this Software.
Definition in file
em_can.h
.
#include "
em_bus.h
"
#include "
em_device.h
"
#include <stdbool.h>
Data Structures |
|
| struct | CAN_Init_TypeDef |
| struct | CAN_MessageObject_TypeDef |
Macros |
|
| #define | CAN_INIT_DEFAULT |
Enumerations |
|
| enum |
CAN_ErrorCode_TypeDef
{
canErrorNoError = CAN_STATUS_LEC_NONE, canErrorStuff = CAN_STATUS_LEC_STUFF, canErrorForm = CAN_STATUS_LEC_FORM, canErrorAck = CAN_STATUS_LEC_ACK, canErrorBit1 = CAN_STATUS_LEC_BIT1, canErrorBit0 = CAN_STATUS_LEC_BIT0, canErrorCrc = CAN_STATUS_LEC_CRC, canErrorUnused = CAN_STATUS_LEC_UNUSED } |
| enum |
CAN_Mode_TypeDef
{
canModeNormal , canModeBasic , canModeLoopBack , canModeSilentLoopBack , canModeSilent } |
Functions |
|
| void | CAN_AbortSendMessage ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
|
Abort sending a message.
|
|
| void | CAN_ConfigureMessageObject ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool valid, bool tx, bool remoteTransfer, bool endOfBuffer, bool wait) |
|
Configure valid, TX/RX, remoteTransfer for a specific Message Object.
|
|
| __STATIC_INLINE void | CAN_Enable ( CAN_TypeDef *can, bool enable) |
|
Enable the Host Controller to send messages.
|
|
| uint32_t | CAN_GetClockFrequency ( CAN_TypeDef *can) |
|
Get the CAN module frequency.
|
|
| __STATIC_INLINE uint32_t | CAN_GetErrorCount ( CAN_TypeDef *can) |
|
Get the error count.
|
|
| __STATIC_INLINE CAN_ErrorCode_TypeDef | CAN_GetLastErrorCode ( CAN_TypeDef *can) |
|
Get the last error code and clear its register.
|
|
| __STATIC_INLINE uint32_t | CAN_HasNewdata ( CAN_TypeDef *can) |
|
Indicates which message objects have received new data.
|
|
| void | CAN_Init ( CAN_TypeDef *can, const CAN_Init_TypeDef *init) |
|
Initialize CAN.
|
|
| __STATIC_INLINE bool | CAN_IsEnabled ( CAN_TypeDef *can) |
|
Give the communication capabilities state.
|
|
| __STATIC_INLINE void | CAN_MessageIntClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear one or more pending CAN message interrupts.
|
|
| __STATIC_INLINE void | CAN_MessageIntDisable ( CAN_TypeDef *can, uint32_t flags) |
|
Disable CAN message interrupts.
|
|
| __STATIC_INLINE void | CAN_MessageIntEnable ( CAN_TypeDef *can, uint32_t flags) |
|
Enable CAN message interrupts.
|
|
| __STATIC_INLINE uint32_t | CAN_MessageIntGet ( CAN_TypeDef *can) |
|
Get pending CAN message interrupt flags.
|
|
| __STATIC_INLINE uint32_t | CAN_MessageIntGetEnabled ( CAN_TypeDef *can) |
|
Get CAN message interrupt flags that are pending and enabled.
|
|
| __STATIC_INLINE void | CAN_MessageIntSet ( CAN_TypeDef *can, uint32_t flags) |
|
Set one or more CAN message interrupts.
|
|
| bool | CAN_MessageLost ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum) |
|
Read a Message Object to find if a message was lost ; reset the 'Message Lost' flag.
|
|
| void | CAN_ReadMessage ( CAN_TypeDef *can, uint8_t interface, CAN_MessageObject_TypeDef *message) |
|
Read data from a Message Object in RAM and store it in a message.
|
|
| __STATIC_INLINE void | CAN_ReadyWait ( CAN_TypeDef *can, uint8_t interface) |
|
Waiting function.
|
|
| void | CAN_Reset ( CAN_TypeDef *can) |
|
Set all CAN registers to RESETVALUE. Leave the CAN device disabled.
|
|
| void | CAN_ResetMessages ( CAN_TypeDef *can, uint8_t interface) |
|
Reset all Message Objects and set their data to 0.
|
|
| void | CAN_SendMessage ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message, bool wait) |
|
Send data from the Message Object message.
|
|
| void | CAN_SendRequest ( CAN_TypeDef *can, uint8_t interface, uint8_t msgNum, bool wait) |
|
Send a request for writing or reading RAM of the Message Object msgNum.
|
|
| void | CAN_SetBitTiming ( CAN_TypeDef *can, uint32_t bitrate, uint16_t propagationTimeSegment, uint16_t phaseBufferSegment1, uint16_t phaseBufferSegment2, uint16_t synchronisationJumpWidth) |
|
Set the bitrate and its parameters.
|
|
| void | CAN_SetIdAndFilter ( CAN_TypeDef *can, uint8_t interface, bool useMask, const CAN_MessageObject_TypeDef *message, bool wait) |
|
Set the ID and the filter for a specific Message Object.
|
|
| void | CAN_SetMode ( CAN_TypeDef *can, CAN_Mode_TypeDef mode) |
|
Set the CAN operation mode.
|
|
| void | CAN_SetRoute ( CAN_TypeDef *can, bool active, uint16_t pinRxLoc, uint16_t pinTxLoc) |
|
Set the ROUTE registers.
|
|
| __STATIC_INLINE void | CAN_StatusClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear CAN status.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusGet ( CAN_TypeDef *can) |
|
Get CAN status.
|
|
| __STATIC_INLINE void | CAN_StatusIntClear ( CAN_TypeDef *can, uint32_t flags) |
|
Clear one or more pending CAN status interrupts.
|
|
| __STATIC_INLINE void | CAN_StatusIntDisable ( CAN_TypeDef *can, uint32_t flags) |
|
Disable CAN status interrupts.
|
|
| __STATIC_INLINE void | CAN_StatusIntEnable ( CAN_TypeDef *can, uint32_t flags) |
|
Enable CAN status interrupts.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusIntGet ( CAN_TypeDef *can) |
|
Get pending CAN status interrupt flags.
|
|
| __STATIC_INLINE uint32_t | CAN_StatusIntGetEnabled ( CAN_TypeDef *can) |
|
Get pending and enabled CAN status interrupt flags.
|
|
| __STATIC_INLINE void | CAN_StatusIntSet ( CAN_TypeDef *can, uint32_t flags) |
|
Set one or more CAN status interrupts.
|
|
| void | CAN_WriteData ( CAN_TypeDef *can, uint8_t interface, const CAN_MessageObject_TypeDef *message) |
|
Write data from a message to the MIRx registers.
|
|