USB_DIEP_TypeDef Struct ReferenceDevicesDevices > | USB
USB_DIEP USB DIEP Register
.
       Definition at line
       
        47
       
       of file
       
        efm32gg11b_usb_diep.h
       
       .
      
      
       #include <
       
     
        efm32gg11b_usb_diep.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | CTL | 
| __IOM uint32_t | DMAADDR | 
| __IM uint32_t | DTXFSTS | 
| __IOM uint32_t | INT | 
| uint32_t | RESERVED0 [1] | 
| uint32_t | RESERVED1 [1] | 
| uint32_t | RESERVED2 [1] | 
| __IOM uint32_t | TSIZ | 
Field Documentation
| __IOM uint32_t USB_DIEP_TypeDef::CTL | 
Device Control in Endpoint 1 Control Register
        Definition at line
        
         48
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| __IOM uint32_t USB_DIEP_TypeDef::DMAADDR | 
Device in Endpoint 1 DMA Address Register
        Definition at line
        
         53
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| __IM uint32_t USB_DIEP_TypeDef::DTXFSTS | 
Device in Endpoint Transmit FIFO Status Register 1
        Definition at line
        
         54
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| __IOM uint32_t USB_DIEP_TypeDef::INT | 
Device in Endpoint 1 Interrupt Register
        Definition at line
        
         50
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| uint32_t USB_DIEP_TypeDef::RESERVED0[1] | 
Reserved for future use
        Definition at line
        
         49
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| uint32_t USB_DIEP_TypeDef::RESERVED1[1] | 
Reserved for future use
        Definition at line
        
         51
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| uint32_t USB_DIEP_TypeDef::RESERVED2[1] | 
Reserved future
        Definition at line
        
         55
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
| __IOM uint32_t USB_DIEP_TypeDef::TSIZ | 
Device in Endpoint 1 Transfer Size Register
        Definition at line
        
         52
        
        of file
        
         efm32gg11b_usb_diep.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
       
efm32gg11b_usb_diep.h