QSPI_WriteConfig_TypeDef Struct ReferenceEMLIB > QSPI
QSPI Device Write Instruction Configuration Structure.
Definition at line
112
of file
em_qspi.h
.
#include <
em_qspi.h
>
Data Fields |
|
| QSPI_TransferType_TypeDef | addrTransfer |
| bool | autoWEL |
|
Enable/disable automatic issuing of WEL (Write Enable Latch) command before a write operation.
|
|
| QSPI_TransferType_TypeDef | dataTransfer |
| uint8_t | dummyCycles |
| uint8_t | opCode |
Field Documentation
| QSPI_TransferType_TypeDef QSPI_WriteConfig_TypeDef::addrTransfer |
Transfer type used for address.
Definition at line
120
of file
em_qspi.h
.
Referenced by QSPI_WriteConfig() .
| bool QSPI_WriteConfig_TypeDef::autoWEL |
Enable/disable automatic issuing of WEL (Write Enable Latch) command before a write operation.
When writing to a flash device, the WEL within the flash device must be high before a write sequence can be issued. The QSPI peripheral can automatically issue the WEL command before triggering a write sequence. The command used for enabling the WEL is WREN (0x06) and is common between devices.
Definition at line
136
of file
em_qspi.h
.
Referenced by QSPI_WriteConfig() .
| QSPI_TransferType_TypeDef QSPI_WriteConfig_TypeDef::dataTransfer |
Transfer type used for data.
Definition at line
123
of file
em_qspi.h
.
Referenced by QSPI_WriteConfig() .
| uint8_t QSPI_WriteConfig_TypeDef::dummyCycles |
Number of dummy read clock cycles.
Definition at line
117
of file
em_qspi.h
.
Referenced by QSPI_WriteConfig() .
| uint8_t QSPI_WriteConfig_TypeDef::opCode |
The documentation for this struct was generated from the following file:
-
C:/repos/embsw_super_h1/platform/emlib/inc/
em_qspi.h