RTC_TypeDef Struct ReferenceDevices > RTC

RTC Register Declaration

Definition at line 49 of file efm32gg11b_rtc.h .

#include < efm32gg11b_rtc.h >

Data Fields

__IOM uint32_t CNT
RTC_COMP_TypeDef COMP [6]
__IOM uint32_t CTRL
__IOM uint32_t IEN
__IM uint32_t IF
__IOM uint32_t IFC
__IOM uint32_t IFS
uint32_t RESERVED0 [2]

Field Documentation

__IOM uint32_t RTC_TypeDef::CNT

Counter Value Register

Definition at line 51 of file efm32gg11b_rtc.h .

RTC_COMP_TypeDef RTC_TypeDef::COMP[6]

Compare channels

Definition at line 58 of file efm32gg11b_rtc.h .

__IOM uint32_t RTC_TypeDef::CTRL

Control Register

Definition at line 50 of file efm32gg11b_rtc.h .

__IOM uint32_t RTC_TypeDef::IEN

Interrupt Enable Register

Definition at line 55 of file efm32gg11b_rtc.h .

__IM uint32_t RTC_TypeDef::IF

Interrupt Flag Register

Definition at line 52 of file efm32gg11b_rtc.h .

__IOM uint32_t RTC_TypeDef::IFC

Interrupt Flag Clear Register

Definition at line 54 of file efm32gg11b_rtc.h .

__IOM uint32_t RTC_TypeDef::IFS

Interrupt Flag Set Register

Definition at line 53 of file efm32gg11b_rtc.h .

uint32_t RTC_TypeDef::RESERVED0[2]

Reserved registers

Definition at line 57 of file efm32gg11b_rtc.h .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/ efm32gg11b_rtc.h