LDMA_TypeDef Struct ReferenceDevices > LDMA
LDMA Register Declaration
Definition at line 49
of file efm32gg11b_ldma.h
.
#include <
efm32gg11b_ldma.h
>
Data Fields | |
LDMA_CH_TypeDef | CH [24] |
__IM uint32_t | CHBUSY |
__IOM uint32_t | CHDONE |
__IOM uint32_t | CHEN |
__IOM uint32_t | CTRL |
__IOM uint32_t | DBGHALT |
__IOM uint32_t | IEN |
__IM uint32_t | IF |
__IOM uint32_t | IFC |
__IOM uint32_t | IFS |
__IOM uint32_t | LINKLOAD |
__IOM uint32_t | REQCLEAR |
__IOM uint32_t | REQDIS |
__IM uint32_t | REQPEND |
uint32_t | RESERVED0 [5] |
uint32_t | RESERVED1 [7] |
uint32_t | RESERVED2 [4] |
__IM uint32_t | STATUS |
__IOM uint32_t | SWREQ |
__IOM uint32_t | SYNC |
Field Documentation
LDMA_CH_TypeDef LDMA_TypeDef::CH[24] |
DMA Channel Registers
Definition at line 70
of file efm32gg11b_ldma.h
.
__IM uint32_t LDMA_TypeDef::CHBUSY |
DMA Channel Busy Register
Definition at line 55
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::CHDONE |
DMA Channel Linking Done Register (Single-Cycle RMW)
Definition at line 56
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::CHEN |
DMA Channel Enable Register (Single-Cycle RMW)
Definition at line 54
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::CTRL |
DMA Control Register
Definition at line 50
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::DBGHALT |
DMA Channel Debug Halt Register
Definition at line 57
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::IEN |
Interrupt Enable Register
Definition at line 67
of file efm32gg11b_ldma.h
.
__IM uint32_t LDMA_TypeDef::IF |
Interrupt Flag Register
Definition at line 64
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::IFC |
Interrupt Flag Clear Register
Definition at line 66
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::IFS |
Interrupt Flag Set Register
Definition at line 65
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::LINKLOAD |
DMA Channel Link Load Register
Definition at line 61
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::REQCLEAR |
DMA Channel Request Clear Register
Definition at line 62
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::REQDIS |
DMA Channel Request Disable Register
Definition at line 59
of file efm32gg11b_ldma.h
.
__IM uint32_t LDMA_TypeDef::REQPEND |
DMA Channel Requests Pending Register
Definition at line 60
of file efm32gg11b_ldma.h
.
uint32_t LDMA_TypeDef::RESERVED0[5] |
Reserved for future use
Definition at line 53
of file efm32gg11b_ldma.h
.
uint32_t LDMA_TypeDef::RESERVED1[7] |
Reserved for future use
Definition at line 63
of file efm32gg11b_ldma.h
.
uint32_t LDMA_TypeDef::RESERVED2[4] |
Reserved registers
Definition at line 69
of file efm32gg11b_ldma.h
.
__IM uint32_t LDMA_TypeDef::STATUS |
DMA Status Register
Definition at line 51
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::SWREQ |
DMA Channel Software Transfer Request Register
Definition at line 58
of file efm32gg11b_ldma.h
.
__IOM uint32_t LDMA_TypeDef::SYNC |
DMA Synchronization Trigger Register (Single-Cycle RMW)
Definition at line 52
of file efm32gg11b_ldma.h
.
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
efm32gg11b_ldma.h