QSPI_StigCmd_TypeDef Struct ReferenceEMLIB > QSPI
Defines command to be executed using STIG mechanism.
Definition at line 167
of file em_qspi.h
.
#include <
em_qspi.h
>
Data Fields | |
uint32_t | address |
uint8_t | addrSize |
uint8_t | cmdOpcode |
uint8_t | dummyCycles |
bool | modeBitEnable |
void * | readBuffer |
uint16_t | readDataSize |
void * | writeBuffer |
uint8_t | writeDataSize |
Field Documentation
uint32_t QSPI_StigCmd_TypeDef::address |
uint8_t QSPI_StigCmd_TypeDef::addrSize |
Number of Address Bytes.
Definition at line 173
of file em_qspi.h
.
Referenced by QSPI_ExecStigCmd().
uint8_t QSPI_StigCmd_TypeDef::cmdOpcode |
uint8_t QSPI_StigCmd_TypeDef::dummyCycles |
bool QSPI_StigCmd_TypeDef::modeBitEnable |
Mode Bit Configuration register are sent following the address bytes.
Definition at line 179
of file em_qspi.h
.
Referenced by QSPI_ExecStigCmd().
void* QSPI_StigCmd_TypeDef::readBuffer |
uint16_t QSPI_StigCmd_TypeDef::readDataSize |
Number of Read Data Bytes.
Definition at line 171
of file em_qspi.h
.
Referenced by QSPI_ExecStigCmd().
void* QSPI_StigCmd_TypeDef::writeBuffer |
Buffer with data to write.
Definition at line 185
of file em_qspi.h
.
Referenced by QSPI_ExecStigCmd().
uint8_t QSPI_StigCmd_TypeDef::writeDataSize |
Number of Write Data Bytes.
Definition at line 175
of file em_qspi.h
.
Referenced by QSPI_ExecStigCmd().
The documentation for this struct was generated from the following file:
- C:/repos/embsw_super_h1/platform/emlib/inc/
em_qspi.h