CAN_MIR_TypeDef Struct ReferenceDevicesDevices > | CAN
CAN_MIR CAN MIR Register
.
       Definition at line
       
        47
       
       of file
       
        efm32gg11b_can_mir.h
       
       .
      
      
       #include <
       
     
        efm32gg11b_can_mir.h
       
       >
      
         Data Fields | 
       |
| __IOM uint32_t | ARB | 
| __IOM uint32_t | CMDMASK | 
| __IOM uint32_t | CMDREQ | 
| __IOM uint32_t | CTRL | 
| __IOM uint32_t | DATAH | 
| __IOM uint32_t | DATAL | 
| __IOM uint32_t | MASK | 
| uint32_t | RESERVED0 [1] | 
Field Documentation
| __IOM uint32_t CAN_MIR_TypeDef::ARB | 
Interface Arbitration Register
        Definition at line
        
         50
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_Reset() , CAN_ResetMessages() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| __IOM uint32_t CAN_MIR_TypeDef::CMDMASK | 
Interface Command Mask Register
        Definition at line
        
         48
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_AbortSendMessage() , CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| __IOM uint32_t CAN_MIR_TypeDef::CMDREQ | 
Interface Command Request Register
        Definition at line
        
         54
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_ReadyWait() , CAN_Reset() , and CAN_SendRequest() .
| __IOM uint32_t CAN_MIR_TypeDef::CTRL | 
Interface Message Control Register
        Definition at line
        
         51
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_ConfigureMessageObject() , CAN_MessageLost() , CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , CAN_SendMessage() , and CAN_SetIdAndFilter() .
| __IOM uint32_t CAN_MIR_TypeDef::DATAH | 
Interface Data B Register
        Definition at line
        
         53
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , and CAN_WriteData() .
| __IOM uint32_t CAN_MIR_TypeDef::DATAL | 
Interface Data a Register
        Definition at line
        
         52
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_ReadMessage() , CAN_Reset() , CAN_ResetMessages() , and CAN_WriteData() .
| __IOM uint32_t CAN_MIR_TypeDef::MASK | 
Interface Mask Register
        Definition at line
        
         49
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
Referenced by CAN_Reset() , CAN_ResetMessages() , and CAN_SetIdAndFilter() .
| uint32_t CAN_MIR_TypeDef::RESERVED0[1] | 
Reserved future
        Definition at line
        
         55
        
        of file
        
         efm32gg11b_can_mir.h
        
        .
       
The documentation for this struct was generated from the following file:
- 
       C:/repos/embsw_super_h1/platform/Device/SiliconLabs/EFM32GG11B/Include/
       
efm32gg11b_can_mir.h