LETIMER_Init_TypeDef Struct ReferenceEMLIB > LETIMER

LETIMER initialization structure.

Definition at line 93 of file em_letimer.h .

#include < em_letimer.h >

Data Fields

bool bufTop
bool comp0Top
bool debugRun
bool enable
uint8_t out0Pol
uint8_t out1Pol
LETIMER_RepeatMode_TypeDef repMode
LETIMER_UFOA_TypeDef ufoa0
LETIMER_UFOA_TypeDef ufoa1

Field Documentation

bool LETIMER_Init_TypeDef::bufTop

Load COMP1 into COMP0 when REP0 reaches 0.

Definition at line 101 of file em_letimer.h .

Referenced by LETIMER_Init() .

bool LETIMER_Init_TypeDef::comp0Top

Load COMP0 register into CNT when counter underflows.

Definition at line 100 of file em_letimer.h .

Referenced by LETIMER_Init() , and MIC_init() .

bool LETIMER_Init_TypeDef::debugRun

Counter shall keep running during debug halt.

Definition at line 95 of file em_letimer.h .

Referenced by LETIMER_Init() .

bool LETIMER_Init_TypeDef::enable

Start counting when initialization completes.

Definition at line 94 of file em_letimer.h .

Referenced by LETIMER_Init() , and MIC_init() .

uint8_t LETIMER_Init_TypeDef::out0Pol

Idle value for output 0.

Definition at line 102 of file em_letimer.h .

Referenced by LETIMER_Init() .

uint8_t LETIMER_Init_TypeDef::out1Pol

Idle value for output 1.

Definition at line 103 of file em_letimer.h .

Referenced by LETIMER_Init() .

LETIMER_RepeatMode_TypeDef LETIMER_Init_TypeDef::repMode

Repeat mode.

Definition at line 106 of file em_letimer.h .

Referenced by LETIMER_Init() .

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa0

Underflow output 0 action.

Definition at line 104 of file em_letimer.h .

Referenced by LETIMER_Init() , and MIC_init() .

LETIMER_UFOA_TypeDef LETIMER_Init_TypeDef::ufoa1

Underflow output 1 action.

Definition at line 105 of file em_letimer.h .

Referenced by LETIMER_Init() .


The documentation for this struct was generated from the following file:
  • C:/repos/embsw_super_h1/platform/emlib/inc/ em_letimer.h