COMM_LayerEMDRV > EZRADIODRV
Detailed Description
EzRadio Communication Layer
.
| Functions | |
| void | ezradio_comm_ClearCTS (void) | 
| uint8_t | ezradio_comm_GetResp (uint8_t byteCount, uint8_t *pData) | 
| uint8_t | ezradio_comm_PollCTS (void) | 
| void | ezradio_comm_ReadData (uint8_t cmd, uint8_t pollCts, uint8_t byteCount, uint8_t *pData) | 
| void | ezradio_comm_SendCmd (uint8_t byteCount, uint8_t *pData) | 
| uint8_t | ezradio_comm_SendCmdGetResp (uint8_t cmdByteCount, uint8_t *pCmdData, uint8_t respByteCount, uint8_t *pRespData) | 
| void | ezradio_comm_WriteData (uint8_t cmd, uint8_t pollCts, uint8_t byteCount, uint8_t *pData) | 
| Variables | |
| uint8_t | ezradio_comm_CtsWentHigh | 
Function Documentation
| void ezradio_comm_ClearCTS | ( | void | 
            | ) | 
Clears the CTS state variable.
        Definition at line
        
         248
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_CtsWentHigh .
Referenced by ezradio_reset() .
| uint8_t ezradio_comm_GetResp | ( | uint8_t | 
            byteCount,
            | 
| uint8_t * | 
            pData
            | ||
| ) | 
Gets a command response from the radio chip
- Parameters
- 
         byteCountNumber of bytes to get from the radio chip pDataPointer to where to put the data 
- Returns
- CTS value
        Definition at line
        
         39
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_CtsWentHigh , ezradio_hal_ClearNsel() , ezradio_hal_SetNsel() , ezradio_hal_SpiReadByte() , ezradio_hal_SpiReadData() , ezradio_hal_SpiWriteByte() , ezradio_hal_SpiWriteReadData() , and EZRADIODRV_COMM_CTS_RETRY .
Referenced by ezradio_comm_PollCTS() , and ezradio_comm_SendCmdGetResp() .
| uint8_t ezradio_comm_PollCTS | ( | void | 
            | ) | 
Waits for CTS to be high
- Returns
- CTS value
        Definition at line
        
         219
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_CtsWentHigh , ezradio_comm_GetResp() , EZRADIODRV_COMM_CTS_RETRY , USTIMER_DeInit() , USTIMER_Delay() , and USTIMER_Init() .
Referenced by ezradio_comm_ReadData() , ezradio_comm_SendCmd() , and ezradio_comm_WriteData() .
| void ezradio_comm_ReadData | ( | uint8_t | 
            cmd,
            | 
| uint8_t | 
            pollCts,
            | ||
| uint8_t | 
            byteCount,
            | ||
| uint8_t * | 
            pData
            | ||
| ) | 
Gets a command response from the radio chip
- Parameters
- 
         cmdCommand ID pollCtsSet to poll CTS byteCountNumber of bytes to get from the radio chip. pDataPointer to where to put the data. 
        Definition at line
        
         143
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_CtsWentHigh , ezradio_comm_PollCTS() , ezradio_hal_ClearNsel() , ezradio_hal_SetNsel() , ezradio_hal_SpiReadData() , ezradio_hal_SpiWriteByte() , and ezradio_hal_SpiWriteReadData() .
Referenced by ezradio_frr_a_read() , ezradio_frr_b_read() , ezradio_frr_c_read() , ezradio_frr_d_read() , and ezradio_read_rx_fifo() .
| void ezradio_comm_SendCmd | ( | uint8_t | 
            byteCount,
            | 
| uint8_t * | 
            pData
            | ||
| ) | 
Sends a command to the radio chip
- Parameters
- 
         byteCountNumber of bytes in the command to send to the radio device pDataPointer to the command to send. 
        Definition at line
        
         120
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_CtsWentHigh , ezradio_comm_PollCTS() , ezradio_hal_ClearNsel() , ezradio_hal_SetNsel() , and ezradio_hal_SpiWriteData() .
Referenced by ezradio_change_state() , ezradio_comm_SendCmdGetResp() , ezradio_fifo_info_fast_reset() , ezradio_get_chip_status_fast_clear() , ezradio_get_int_status_fast_clear() , ezradio_get_modem_status_fast_clear() , ezradio_get_ph_status_fast_clear() , ezradio_ircal() , ezradio_nop() , ezradio_power_up() , ezradio_rx_hop() , ezradio_set_property() , ezradio_start_rx() , ezradio_start_rx_fast() , ezradio_start_tx() , ezradio_start_tx_fast() , and ezradio_tx_hop() .
| uint8_t ezradio_comm_SendCmdGetResp | ( | uint8_t | 
            cmdByteCount,
            | 
| uint8_t * | 
            pCmdData,
            | ||
| uint8_t | 
            respByteCount,
            | ||
| uint8_t * | 
            pRespData
            | ||
| ) | 
Sends a command to the radio chip and gets a response
- Parameters
- 
         cmdByteCountNumber of bytes in the command to send to the radio device pCmdDataPointer to the command data respByteCountNumber of bytes in the response to fetch pRespDataPointer to where to put the response data 
- Returns
- CTS value
        Definition at line
        
         263
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_GetResp() , and ezradio_comm_SendCmd() .
Referenced by ezradio_configuration_init() , ezradio_ezconfig_check() , ezradio_fifo_info() , ezradio_fifo_info_fast_read() , ezradio_func_info() , ezradio_get_adc_reading() , ezradio_get_chip_status() , ezradio_get_chip_status_fast_clear_read() , ezradio_get_int_status() , ezradio_get_int_status_fast_clear_read() , ezradio_get_modem_status() , ezradio_get_modem_status_fast_clear_read() , ezradio_get_packet_info() , ezradio_get_ph_status() , ezradio_get_ph_status_fast_clear_read() , ezradio_get_property() , ezradio_gpio_pin_cfg() , ezradio_gpio_pin_cfg_fast() , ezradio_ircal_manual() , ezradio_part_info() , ezradio_read_cmd_buff() , and ezradio_request_device_state() .
| void ezradio_comm_WriteData | ( | uint8_t | 
            cmd,
            | 
| uint8_t | 
            pollCts,
            | ||
| uint8_t | 
            byteCount,
            | ||
| uint8_t * | 
            pData
            | ||
| ) | 
Gets a command response from the radio chip
- Parameters
- 
         cmdCommand ID pollCtsSet to poll CTS byteCountNumber of bytes to get from the radio chip pDataPointer to where to put the data 
        Definition at line
        
         182
        
        of file
        
         ezradio_comm.c
        
        .
       
References ezradio_comm_CtsWentHigh , ezradio_comm_PollCTS() , ezradio_hal_ClearNsel() , ezradio_hal_SetNsel() , ezradio_hal_SpiWriteByte() , and ezradio_hal_SpiWriteData() .
Referenced by ezradio_write_ezconfig_array() , and ezradio_write_tx_fifo() .
Variable Documentation
| uint8_t ezradio_comm_CtsWentHigh | 
Can be used to prevent CTS check before any communication command.
        Definition at line
        
         29
        
        of file
        
         ezradio_comm.c
        
        .
       
Referenced by ezradio_comm_ClearCTS() , ezradio_comm_GetResp() , ezradio_comm_PollCTS() , ezradio_comm_ReadData() , ezradio_comm_SendCmd() , ezradio_comm_WriteData() , and ezradio_ezconfig_check() .