MSC_EccConfig_TypeDef Struct ReferenceEMLIB > MSC
ECC configuration.
       Definition at line
       
        232
       
       of file
       
        em_msc.h
       
       .
      
      
       #include <
       
     
        em_msc.h
       
       >
      
| Data Fields | |
| uint32_t | dmaChannels [2] | 
| bool | enableEccBank [ MSC_ECC_BANKS ] | 
Field Documentation
| uint32_t MSC_EccConfig_TypeDef::dmaChannels[2] | 
Array of 2 DMA channel numbers to use for ECC initialization.
        Definition at line
        
         237
        
        of file
        
         em_msc.h
        
        .
       
Referenced by MSC_EccConfigSet() .
| bool MSC_EccConfig_TypeDef::enableEccBank[ MSC_ECC_BANKS ] | 
Array of bools to enable/disable Error Correcting Code (ECC) for each RAM bank that supports ECC on the device.
        Definition at line
        
         233
        
        of file
        
         em_msc.h
        
        .
       
Referenced by MSC_EccConfigSet() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_msc.h