TouchKit Drivers
Detailed Description
Touch panel driver for DK3650, DK3750 and DK3850 Development Kits.
| Data Structures | |
| struct | TOUCH_Config_TypeDef | 
| struct | TOUCH_Pos_TypeDef | 
| Macros | |
| #define | ADC_X adcSingleInpCh1 | 
| #define | ADC_Y adcSingleInpCh4 | 
| #define | TOUCH_INIT_DEFAULT | 
| #define | TOUCH_X1_PIN 5 | 
| #define | TOUCH_X1_PORT gpioPortD | 
| #define | TOUCH_X2_PIN 4 | 
| #define | TOUCH_X2_PORT gpioPortD | 
| #define | TOUCH_Y1_PIN 3 | 
| #define | TOUCH_Y1_PORT gpioPortD | 
| #define | TOUCH_Y2_PIN 1 | 
| #define | TOUCH_Y2_PORT gpioPortD | 
| Typedefs | |
| typedef void( | TOUCH_Upcall_TypeDef ) ( TOUCH_Pos_TypeDef *) | 
| Enumerations | |
| enum | TOUCH_State_TypeDef
         
         { TOUCH_INIT , TOUCH_CHECK_PRESS , TOUCH_MEASURE_X , TOUCH_MEASURE_Y } | 
| Functions | |
| void | ADC0_IRQHandler (void) | 
| Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second. | |
| int | TOUCH_CalibrationTable (POINT *displayPtr, POINT *screenPtr) | 
| Set calibration table. | |
| void | TOUCH_CallUpcall (void) | 
| Function that calls registered upcall. | |
| TOUCH_Pos_TypeDef * | TOUCH_GetPos (void) | 
| Returns current touch position and state. | |
| void | TOUCH_Init ( TOUCH_Config_TypeDef *config) | 
| Initialize touch panel driver. | |
| int | TOUCH_IsBusy (void) | 
| Check status of the touch panel. | |
| void | TOUCH_RecalculatePosition (volatile TOUCH_Pos_TypeDef *pos) | 
| Convert ADC readings into XY position. | |
| void | TOUCH_RegisterUpcall ( TOUCH_Upcall_TypeDef *new_upcall) | 
| Register upcall which will be call every position or state change. | |
| int | TOUCH_StateChanged (void) | 
| Check if cursor state changed (down or move) | |
| Variables | |
| MATRIX | calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } | 
Macro Definition Documentation
| #define ADC_X adcSingleInpCh1 | 
| #define ADC_Y adcSingleInpCh4 | 
Input channel 4
        Definition at line
        
         51
        
        of file
        
         touch.c
        
        .
       
Referenced by ADC0_IRQHandler() , and TOUCH_Init() .
| #define TOUCH_INIT_DEFAULT | 
Initializes Touch default values
        Definition at line
        
         63
        
        of file
        
         touch.h
        
        .
       
| #define TOUCH_X1_PIN 5 | 
| #define TOUCH_X1_PORT gpioPortD | 
| #define TOUCH_X2_PIN 4 | 
Pin 4
        Definition at line
        
         57
        
        of file
        
         touch.c
        
        .
       
Referenced by ADC0_IRQHandler() , and TOUCH_IsBusy() .
| #define TOUCH_X2_PORT gpioPortD | 
Port D
        Definition at line
        
         56
        
        of file
        
         touch.c
        
        .
       
Referenced by ADC0_IRQHandler() , and TOUCH_IsBusy() .
| #define TOUCH_Y1_PIN 3 | 
| #define TOUCH_Y1_PORT gpioPortD | 
| #define TOUCH_Y2_PIN 1 | 
| #define TOUCH_Y2_PORT gpioPortD | 
Typedef Documentation
| typedef void( TOUCH_Upcall_TypeDef) ( TOUCH_Pos_TypeDef *) | 
touch panel upcall type definition
        Definition at line
        
         70
        
        of file
        
         touch.h
        
        .
       
Enumeration Type Documentation
| enum TOUCH_State_TypeDef | 
touch driver states
        Definition at line
        
         64
        
        of file
        
         touch.c
        
        .
       
Function Documentation
| void ADC0_IRQHandler | ( | void | 
            | ) | 
Interrupt handler is executed with frequency ~28Hz when panel is not pressed and with frequency ~140Hz when panel is pressed - this will give ~50 readings per second.
ADC0 IRQ Handler
        Definition at line
        
         242
        
        of file
        
         touch.c
        
        .
       
References ADC_InitSingle_TypeDef::acqTime , ADC_DataSingleGet() , ADC_InitSingle() , ADC_IntClear() , ADC_Start() , ADC_X , ADC_Y , adcAcqTime128 , adcAcqTime16 , adcRefVDD , adcResOVS , adcStartSingle , TOUCH_Pos_TypeDef::adcx , TOUCH_Pos_TypeDef::adcy , GPIO_PinInGet() , GPIO_PinModeSet() , gpioModeInput , gpioModeInputPullFilter , gpioModePushPull , TOUCH_Pos_TypeDef::pen , ADC_InitSingle_TypeDef::reference , ADC_InitSingle_TypeDef::resolution , TOUCH_CallUpcall() , TOUCH_RecalculatePosition() , TOUCH_StateChanged() , TOUCH_X1_PIN , TOUCH_X1_PORT , TOUCH_X2_PIN , TOUCH_X2_PORT , TOUCH_Y1_PIN , TOUCH_Y1_PORT , TOUCH_Y2_PIN , TOUCH_Y2_PORT , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
| int TOUCH_CalibrationTable | ( | POINT * | 
            displayPtr,
            | 
| POINT * | 
            screenPtr
            | ||
| ) | 
Set calibration table.
- Parameters
- 
         [in] displayPtrTable of display points [in] screenPtrTable of adc values reflecting display points 
- Returns
- Returns OK if calibration table is set.
        Definition at line
        
         420
        
        of file
        
         touch.c
        
        .
       
References calibrationMatrix .
| TOUCH_Pos_TypeDef * TOUCH_GetPos | ( | void | 
            | ) | 
Returns current touch position and state.
- Returns
- Current touch position and state
        Definition at line
        
         383
        
        of file
        
         touch.c
        
        .
       
References ADC_IntDisable() , ADC_IntEnable() , TOUCH_Pos_TypeDef::adcx , TOUCH_Pos_TypeDef::adcy , TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
| void TOUCH_Init | ( | TOUCH_Config_TypeDef * | 
            config
            | ) | 
Initialize touch panel driver.
- Parameters
- 
         configDriver configuration data. 
        Definition at line
        
         351
        
        of file
        
         touch.c
        
        .
       
References ADC_Init() , ADC_INIT_DEFAULT , ADC_InitSingle() , ADC_IntClear() , ADC_IntDisable() , ADC_IntEnable() , ADC_PrescaleCalc() , ADC_Start() , ADC_Y , adcRefVDD , adcResOVS , adcStartSingle , BSP_PeripheralAccess() , BSP_TOUCH , CMU_ClockEnable() , cmuClock_ADC0 , TOUCH_Config_TypeDef::frequency , TOUCH_Config_TypeDef::ignore , TOUCH_Config_TypeDef::oversampling , ADC_Init_TypeDef::ovsRateSel , ADC_Init_TypeDef::prescale , ADC_InitSingle_TypeDef::reference , and ADC_InitSingle_TypeDef::resolution .
| int TOUCH_IsBusy | ( | void | 
            | ) | 
Check status of the touch panel.
- Returns
- 0 if panel is idle (not touched).
        Definition at line
        
         331
        
        of file
        
         touch.c
        
        .
       
References GPIO_PinInGet() , TOUCH_X2_PIN , and TOUCH_X2_PORT .
| void TOUCH_RecalculatePosition | ( | volatile TOUCH_Pos_TypeDef * | 
            pos
            | ) | 
Convert ADC readings into XY position.
- Parameters
- 
         [in] posPointer to position structure 
        Definition at line
        
         172
        
        of file
        
         touch.c
        
        .
       
References TOUCH_Pos_TypeDef::adcx , TOUCH_Pos_TypeDef::adcy , calibrationMatrix , TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
Referenced by ADC0_IRQHandler() .
| void TOUCH_RegisterUpcall | ( | TOUCH_Upcall_TypeDef * | 
            new_upcall
            | ) | 
Register upcall which will be call every position or state change.
- Parameters
- 
         [in] new_upcallPointer to upcall function 
        Definition at line
        
         403
        
        of file
        
         touch.c
        
        .
       
| int TOUCH_StateChanged | ( | void | 
            | ) | 
Check if cursor state changed (down or move)
- Returns
- 1 if the cursor state has changed
        Definition at line
        
         215
        
        of file
        
         touch.c
        
        .
       
References TOUCH_Pos_TypeDef::pen , TOUCH_Pos_TypeDef::x , and TOUCH_Pos_TypeDef::y .
Referenced by ADC0_IRQHandler() .
Variable Documentation
| MATRIX calibrationMatrix = { 103800, 2048, -8184704, -384, 102144, -16424640, 287650 } | 
Calibration table
        Definition at line
        
         84
        
        of file
        
         touch.c
        
        .
       
Referenced by TOUCH_CalibrationTable() , and TOUCH_RecalculatePosition() .