LESENSE_PerCtrlDesc_TypeDef Struct ReferenceEMLIB > LESENSE
LESENSE peripheral control descriptor structure.
       Definition at line
       
        566
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
Field Documentation
| LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp0Mode | 
Configure how LESENSE controls ACMP 0.
        Definition at line
        
         606
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlACMP_TypeDef LESENSE_PerCtrlDesc_TypeDef::acmp1Mode | 
Configure how LESENSE controls ACMP 1.
        Definition at line
        
         609
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh0Data | 
Configure DAC channel 0 data control.
        Definition at line
        
         568
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_PerCtrlDesc_TypeDef::dacCh0En | 
When set to true, LESENSE controls DAC channel 0.
        Definition at line
        
         628
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_ControlDACData_TypeDef LESENSE_PerCtrlDesc_TypeDef::dacCh1Data | 
Configure DAC channel 1 data control.
        Definition at line
        
         581
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_PerCtrlDesc_TypeDef::dacCh1En | 
When set to true, LESENSE controls DAC channel 1.
        Definition at line
        
         633
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_PerCtrlDesc_TypeDef::dacScan | 
When set to true the DAC is only enabled once for each scan. When set to false the DAC is enabled before every channel measurement.
        Definition at line
        
         617
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| bool LESENSE_PerCtrlDesc_TypeDef::dacStartupHalf | 
When set to true the DAC is started a half clock cycle before sensor interaction starts. When set to false, a full clock cycle is used.
        Definition at line
        
         623
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
| LESENSE_WarmupMode_TypeDef LESENSE_PerCtrlDesc_TypeDef::warmupMode | 
Configure how LESENSE controls ACMPs and DAC in idle mode.
        Definition at line
        
         612
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_Init() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_lesense.h