QSPI_StigCmd_TypeDef Struct ReferenceEMLIB > QSPI
Defines command to be executed using STIG mechanism.
       Definition at line
       
        166
       
       of file
       
        em_qspi.h
       
       .
      
      
       #include <
       
     
        em_qspi.h
       
       >
      
| Data Fields | |
| uint32_t | address | 
| uint8_t | addrSize | 
| uint8_t | cmdOpcode | 
| uint8_t | dummyCycles | 
| bool | modeBitEnable | 
| void * | readBuffer | 
| uint16_t | readDataSize | 
| void * | writeBuffer | 
| uint8_t | writeDataSize | 
Field Documentation
| uint32_t QSPI_StigCmd_TypeDef::address | 
Flash command address.
        Definition at line
        
         180
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| uint8_t QSPI_StigCmd_TypeDef::addrSize | 
Number of Address Bytes.
        Definition at line
        
         172
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| uint8_t QSPI_StigCmd_TypeDef::cmdOpcode | 
| uint8_t QSPI_StigCmd_TypeDef::dummyCycles | 
Number of dummy cycles.
        Definition at line
        
         176
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| bool QSPI_StigCmd_TypeDef::modeBitEnable | 
Mode Bit Configuration register are sent following the address bytes.
        Definition at line
        
         178
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| void* QSPI_StigCmd_TypeDef::readBuffer | 
| uint16_t QSPI_StigCmd_TypeDef::readDataSize | 
Number of Read Data Bytes.
        Definition at line
        
         170
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| void* QSPI_StigCmd_TypeDef::writeBuffer | 
Buffer with data to write.
        Definition at line
        
         184
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
| uint8_t QSPI_StigCmd_TypeDef::writeDataSize | 
Number of Write Data Bytes.
        Definition at line
        
         174
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ExecStigCmd() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_qspi.h