EMU_VmonInit_TypeDef Struct ReferenceEMLIB > EMU
VMON initialization structure.
       Definition at line
       
        855
       
       of file
       
        em_emu.h
       
       .
      
      
       #include <
       
     
        em_emu.h
       
       >
      
| Data Fields | |
| EMU_VmonChannel_TypeDef | channel | 
| bool | enable | 
| bool | fallWakeup | 
| bool | retDisable | 
| bool | riseWakeup | 
| int | threshold | 
Field Documentation
| EMU_VmonChannel_TypeDef EMU_VmonInit_TypeDef::channel | 
| bool EMU_VmonInit_TypeDef::enable | 
| bool EMU_VmonInit_TypeDef::fallWakeup | 
Wake up from EM4H on falling edge.
        Definition at line
        
         859
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonInit() .
| bool EMU_VmonInit_TypeDef::retDisable | 
Disable IO0 retention when voltage drops below threshold (IOVDD only).
        Definition at line
        
         861
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonInit() .
| bool EMU_VmonInit_TypeDef::riseWakeup | 
Wake up from EM4H on rising edge.
        Definition at line
        
         858
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonInit() .
| int EMU_VmonInit_TypeDef::threshold | 
Trigger threshold (mV). Supported range is 1620 mV to 3400 mV.
        Definition at line
        
         857
        
        of file
        
         em_emu.h
        
        .
       
Referenced by EMU_VmonInit() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_emu.h