LESENSE_ChDesc_TypeDef Struct ReferenceEMLIB > LESENSE
Channel descriptor structure.
       Definition at line
       
        760
       
       of file
       
        em_lesense.h
       
       .
      
      
       #include <
       
     
        em_lesense.h
       
       >
      
| Data Fields | |
| uint16_t | acmpThres | 
| LESENSE_ChPinExMode_TypeDef | chPinExMode | 
| LESENSE_ChPinIdleMode_TypeDef | chPinIdleMode | 
| uint16_t | cntThres | 
| LESENSE_ChCompMode_TypeDef | compMode | 
| bool | enaInt | 
| bool | enaPin | 
| bool | enaScanCh | 
| LESENSE_ChEvalMode_TypeDef | evalMode | 
| LESENSE_ChClk_TypeDef | exClk | 
| uint8_t | exTime | 
| LESENSE_ChIntMode_TypeDef | intMode | 
| bool | invRes | 
| uint16_t | measDelay | 
| LESENSE_ChClk_TypeDef | sampleClk | 
| uint8_t | sampleDelay | 
| LESENSE_ChSampleMode_TypeDef | sampleMode | 
| bool | shiftRes | 
| bool | storeCntRes | 
| bool | useAltEx | 
Field Documentation
| uint16_t LESENSE_ChDesc_TypeDef::acmpThres | 
Configure the ACMP threshold or the DAC data. If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to lesenseDACIfData , acmpThres defines the 12-bit DAC data in the corresponding data register of DAC interface (DACn_CH0DATA and DACn_CH1DATA). In this case, the valid range is: 0-4095 (12 bits). If perCtrl.dacCh0Data or perCtrl.dacCh1Data is set to #lesenseACMPThres, acmpThres defines the 6-bit Vdd scaling factor of ACMP negative input (VDDLEVEL in ACMP_INPUTSEL register). In this case, the valid range is: 0-63 (6 bits).
        Definition at line
        
         821
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChPinExMode_TypeDef LESENSE_ChDesc_TypeDef::chPinExMode | 
Configure channel pin mode for the excitation phase of the scan sequence. Note: OPAOUT is only available on channels 2, 3, 4, and 5.
        Definition at line
        
         773
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChPinIdleMode_TypeDef LESENSE_ChDesc_TypeDef::chPinIdleMode | 
Configure channel pin idle setup in LESENSE idle phase.
        Definition at line
        
         776
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| uint16_t LESENSE_ChDesc_TypeDef::cntThres | 
Configure the decision threshold for the sensor data comparison. Valid range: 0-65535 (16 bits).
        Definition at line
        
         832
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChCompMode_TypeDef LESENSE_ChDesc_TypeDef::compMode | 
Select the mode for counter comparison.
        Definition at line
        
         835
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::enaInt | 
Enable/disable channel interrupts after configuring all the sensor channel parameters.
        Definition at line
        
         769
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::enaPin | 
Set to enable CHx pin.
        Definition at line
        
         765
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::enaScanCh | 
Set to enable scan channel CHx.
        Definition at line
        
         762
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChEvalMode_TypeDef LESENSE_ChDesc_TypeDef::evalMode | 
Select the sensor evaluation mode.
        Definition at line
        
         839
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChClk_TypeDef LESENSE_ChDesc_TypeDef::exClk | 
Select clock used for the excitation timing.
        Definition at line
        
         793
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| uint8_t LESENSE_ChDesc_TypeDef::exTime | 
Configure the excitation time. Excitation will last exTime+1 excitation clock cycles. Valid range: 0-63 (6 bits).
        Definition at line
        
         800
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChIntMode_TypeDef LESENSE_ChDesc_TypeDef::intMode | 
Configure the interrupt generation mode for the CHx interrupt flag.
        Definition at line
        
         828
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::invRes | 
Set to invert result bit stored in the SCANRES register.
        Definition at line
        
         786
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| uint16_t LESENSE_ChDesc_TypeDef::measDelay | 
Configure the measure delay. Sensor measuring is delayed for measDelay excitation clock cycles. Valid range: 0-127 (7 bits) or 0-1023 (10 bits) depending on device.
        Definition at line
        
         810
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChClk_TypeDef LESENSE_ChDesc_TypeDef::sampleClk | 
Select clock used for the sample delay timing.
        Definition at line
        
         796
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| uint8_t LESENSE_ChDesc_TypeDef::sampleDelay | 
Configure the sample delay. Sampling will occur after sampleDelay+1 sample clock cycles. Valid range: 0-127 (7 bits) or 0-255 (8 bits) depending on device.
        Definition at line
        
         805
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| LESENSE_ChSampleMode_TypeDef LESENSE_ChDesc_TypeDef::sampleMode | 
Select if the ACMP output, the ADC output or the counter output should be used in comparison.
        Definition at line
        
         825
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::shiftRes | 
Set to enable result from this channel being shifted into the decoder register.
        Definition at line
        
         783
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::storeCntRes | 
Set to store counter value in the RAM (accessible via RESDATA) and make the comparison result available in the SCANRES register.
        Definition at line
        
         790
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
| bool LESENSE_ChDesc_TypeDef::useAltEx | 
Set to use alternate excite pin for excitation.
        Definition at line
        
         779
        
        of file
        
         em_lesense.h
        
        .
       
Referenced by LESENSE_ChannelConfig() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_lesense.h