QSPI_DelayConfig_TypeDef Struct ReferenceEMLIB > QSPI
QSPI Device Delay Configuration Structure.
Definition at line 149
of file em_qspi.h
.
#include <
em_qspi.h
>
Data Fields | |
uint8_t | deassert |
uint8_t | deviceSwitch |
uint8_t | firstBit |
uint8_t | lastBit |
Field Documentation
uint8_t QSPI_DelayConfig_TypeDef::deassert |
The minimal delay to keep the chip select line de-asserted between two transactions.
Definition at line 152
of file em_qspi.h
.
uint8_t QSPI_DelayConfig_TypeDef::deviceSwitch |
Delay between one chip select being de-activated and the activation of another.
Definition at line 156
of file em_qspi.h
.
uint8_t QSPI_DelayConfig_TypeDef::firstBit |
Delay chip select assert and first bit in a transaction.
Definition at line 162
of file em_qspi.h
.
uint8_t QSPI_DelayConfig_TypeDef::lastBit |
Delay between last bit and chip select de-assert.
Definition at line 159
of file em_qspi.h
.
The documentation for this struct was generated from the following file:
- C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
em_qspi.h