LCD_Init_TypeDef Struct ReferenceEMLIB > LCD
LCD Controller Initialization structure.
       Definition at line
       
        272
       
       of file
       
        em_lcd.h
       
       .
      
      
       #include <
       
     
        em_lcd.h
       
       >
      
| Data Fields | |
| LCD_Bias_TypeDef | bias | 
| LCD_ChargeRedistribution_TypeDef | chargeRedistribution | 
| int | contrastLevel | 
| bool | enable | 
| uint8_t | frameRateDivider | 
| LCD_Mode_Typedef | mode | 
| LCD_Mux_TypeDef | mux | 
| LCD_Wave_TypeDef | wave | 
Field Documentation
| LCD_Bias_TypeDef LCD_Init_TypeDef::bias | 
| bool LCD_Init_TypeDef::enable | 
Enable controller at end of initialization.
        Definition at line
        
         274
        
        of file
        
         em_lcd.h
        
        .
       
Referenced by LCD_Init() .
| LCD_Mode_Typedef LCD_Init_TypeDef::mode | 
| LCD_Mux_TypeDef LCD_Init_TypeDef::mux | 
| LCD_Wave_TypeDef LCD_Init_TypeDef::wave | 
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_lcd.h