QSPI_ReadConfig_TypeDef Struct ReferenceEMLIB > QSPI
QSPI Device Read Instruction Configuration Structure.
       Definition at line
       
        83
       
       of file
       
        em_qspi.h
       
       .
      
      
       #include <
       
     
        em_qspi.h
       
       >
      
| Data Fields | |
| QSPI_TransferType_TypeDef | addrTransfer | 
| QSPI_TransferType_TypeDef | dataTransfer | 
| uint8_t | dummyCycles | 
| QSPI_TransferType_TypeDef | instTransfer | 
| uint8_t | opCode | 
Field Documentation
| QSPI_TransferType_TypeDef QSPI_ReadConfig_TypeDef::addrTransfer | 
Transfer type used for address.
        Definition at line
        
         91
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ReadConfig() .
| QSPI_TransferType_TypeDef QSPI_ReadConfig_TypeDef::dataTransfer | 
Transfer type used for data.
        Definition at line
        
         94
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ReadConfig() .
| uint8_t QSPI_ReadConfig_TypeDef::dummyCycles | 
Number of dummy read clock cycles.
        Definition at line
        
         88
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ReadConfig() .
| QSPI_TransferType_TypeDef QSPI_ReadConfig_TypeDef::instTransfer | 
Transfer type used for instruction.
        Definition at line
        
         97
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ReadConfig() .
| uint8_t QSPI_ReadConfig_TypeDef::opCode | 
Read opcode in non-xip mode.
        Definition at line
        
         85
        
        of file
        
         em_qspi.h
        
        .
       
Referenced by QSPI_ReadConfig() .
The documentation for this struct was generated from the following file:
- 
       C:/cygwin/home/caamunds/work/super/platform/emlib/inc/
       em_qspi.h