PCNT_TCC_TypeDef Struct Reference

TCC initialization structure.

Definition at line 326 of file em_pcnt.h.

#include <em_pcnt.h>

Data Fields

PCNT_TCCComp_Typedef compare
 
PCNT_TCCMode_TypeDef mode
 
PCNT_TCCPresc_Typedef prescaler
 
bool prsGateEnable
 
bool prsPolarity
 
PCNT_PRSSel_TypeDef tccPRS
 

Field Documentation

PCNT_TCCComp_Typedef PCNT_TCC_TypeDef::compare

Choose the event that will trigger a clear.

Definition at line 334 of file em_pcnt.h.

Referenced by PCNT_TCCConfiguration().

PCNT_TCCMode_TypeDef PCNT_TCC_TypeDef::mode

Mode to operate in.

Definition at line 328 of file em_pcnt.h.

Referenced by PCNT_TCCConfiguration().

PCNT_TCCPresc_Typedef PCNT_TCC_TypeDef::prescaler

Prescaler value for LFACLK in LFA mode.

Definition at line 331 of file em_pcnt.h.

Referenced by PCNT_TCCConfiguration().

bool PCNT_TCC_TypeDef::prsGateEnable

Enable gating PCNT input clock through TCC PRS signal. Polarity selection is done through prsPolarity.

Definition at line 346 of file em_pcnt.h.

Referenced by PCNT_TCCConfiguration().

bool PCNT_TCC_TypeDef::prsPolarity

TCC PRS input polarity.
False = Rising edge for comparison trigger, and PCNT clock gated when PRS signal is high.
True = Falling edge for comparison trigger, and PCNT clock gated when PRS signal is low.

Definition at line 342 of file em_pcnt.h.

Referenced by PCNT_TCCConfiguration().

PCNT_PRSSel_TypeDef PCNT_TCC_TypeDef::tccPRS

PRS input to TCC module, either for gating the PCNT clock, triggering the TCC comparison, or both.

Definition at line 337 of file em_pcnt.h.

Referenced by PCNT_TCCConfiguration().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/platform/emlib/inc/em_pcnt.h