TEXTDISPLAY_Config_t Struct Reference

Initialization data structure for text display devices.

Definition at line 82 of file textdisplay.h.

#include <textdisplay.h>

Data Fields

int displayDeviceNo
 
bool lfToCrLf
 
bool scrollEnable
 

Field Documentation

int TEXTDISPLAY_Config_t::displayDeviceNo

Display device number to initialize test display on.

Definition at line 83 of file textdisplay.h.

Referenced by RETARGET_TextDisplayInit(), and TEXTDISPLAY_New().

bool TEXTDISPLAY_Config_t::lfToCrLf

Enable or disable LF to CR+LF conversion.

Definition at line 90 of file textdisplay.h.

Referenced by RETARGET_TextDisplayInit(), and TEXTDISPLAY_New().

bool TEXTDISPLAY_Config_t::scrollEnable

Enable/disable scrolling mode on the text display. Scrolling mode will consume more memory because the lines will have to be stored in memory.

Definition at line 85 of file textdisplay.h.

Referenced by RETARGET_TextDisplayInit(), and TEXTDISPLAY_New().


The documentation for this struct was generated from the following file:
  • C:/HandsOn/super/hardware/kit/common/drivers/textdisplay.h