This module includes functions that allow a Host processor to execute remote procedure calls on a co-processor over spinel.
Functions |
|
| void | otCliAppendResult ( otError aError) |
|
Append an error code to the output buffer.
|
|
| otError | otCRPCHandleCommand (void *aContext, uint8_t aArgsLength, char *aArgs[], uint8_t aCommandsLength, const otCliCommand aCommands[]) |
|
Call the corresponding handler for a command.
|
|
| void | otCliOutputBytes (const uint8_t *aBytes, uint8_t aLength) |
|
Output a byte array as hex to the output buffer.
|
|
| void | otCliOutputCommands (const otCliCommand aCommands[], size_t aCommandsLength) |
Write all command names in
aCommands
to the output buffer.
|
|
| int | otCliOutputFormatV (const char *aFormat, va_list aArguments) |
|
Write formatted output to the output buffer.
|
|
| void | otCliOutputFormat (const char *aFmt,...) |
|
Write formatted string to the output buffer.
|
|
| int | otCliOutputIp6Address (const otIp6Address *aAddress) |
|
Write an IPv6 address to the output buffer.
|
|
| otError | otCRPCProcessCmd (uint8_t aArgsLength, char *aArgs[], char *aOutput, size_t aOutputMaxLen) |
|
Process a command line.
|
|
| void | otCRPCProcessCmdLine (const char *aString, char *aOutput, size_t aOutputMaxLen) |
|
Process a command-line string.
|
|
| void | otCRPCProcessHelp (void *aContext, uint8_t aArgsLength, char *aArgs[]) |
|
Output all available CRPC built-in commands and user commands.
|
|
| void | otCRPCSetUserCommands (const otCliCommand *aUserCommands, uint8_t aLength, void *aContext) |
|
Set a user command table.
|
|
Detailed Description
This module includes functions that allow a Host processor to execute remote procedure calls on a co-processor over spinel.
Function Documentation
◆ otCliAppendResult()
| void otCliAppendResult | ( | otError |
aError
|
) |
Append an error code to the output buffer.
- Parameters
-
[in] aError
◆ otCliOutputBytes()
| void otCliOutputBytes | ( | const uint8_t * |
aBytes,
|
| uint8_t |
aLength
|
||
| ) |
Output a byte array as hex to the output buffer.
- Parameters
-
[in] aBytesBytes to output [in] aLengthNumber of bytes
◆ otCliOutputCommands()
| void otCliOutputCommands | ( | const otCliCommand |
aCommands[],
|
| size_t |
aCommandsLength
|
||
| ) |
Write all command names in
aCommands
to the output buffer.
- Parameters
-
[in] aCommandsan array of commands [in] aCommandsLengthlength of aCommands
◆ otCliOutputFormat()
| void otCliOutputFormat | ( | const char * |
aFmt,
|
...
|
|||
| ) |
Write formatted string to the output buffer.
- Parameters
-
[in] aFmtA pointer to the format string. [in] ...A matching list of arguments.
◆ otCliOutputFormatV()
| int otCliOutputFormatV | ( | const char * |
aFormat,
|
| va_list |
aArguments
|
||
| ) |
Write formatted output to the output buffer.
- Parameters
-
[in] aFormatA pointer to the format string. [in] aArgumentsA variable list of arguments for format.
- Returns
- The number of bytes placed in the output buffer.
◆ otCliOutputIp6Address()
| int otCliOutputIp6Address | ( | const otIp6Address * |
aAddress
|
) |
Write an IPv6 address to the output buffer.
- Parameters
-
[in] aAddressA pointer to the IPv6 address.
- Returns
- The number of bytes placed in the output queue.
- Return values
-
-1Driver is broken.
◆ otCRPCHandleCommand()
| otError otCRPCHandleCommand | ( | void * |
aContext,
|
| uint8_t |
aArgsLength,
|
||
| char * |
aArgs[],
|
||
| uint8_t |
aCommandsLength,
|
||
| const otCliCommand |
aCommands[]
|
||
| ) |
Call the corresponding handler for a command.
This function will look through
aCommands
to find a command that matches
aArgs
[0]. If found, the handler function for the command will be called with the remaining args passed to it.
- Parameters
-
[in] aContexta context [in] aArgsLengthnumber of args [in] aArgslist of args [in] aCommandsLengthnumber of commands in aCommands[in] aCommandslist of commands
- Return values
-
◆ otCRPCProcessCmd()
| otError otCRPCProcessCmd | ( | uint8_t |
aArgsLength,
|
| char * |
aArgs[],
|
||
| char * |
aOutput,
|
||
| size_t |
aOutputMaxLen
|
||
| ) |
Process a command line.
- Parameters
-
[in] aArgsLengthThe number of elements in aArgs.[in] aArgsAn array of arguments. [out] aOutputThe execution result. [in] aOutputMaxLenThe output buffer size.
- Return values
-
OT_ERROR_INVALID_ARGSThe command is supported but invalid arguments provided. OT_ERROR_NONEThe command is successfully process. OT_ERROR_NOT_IMPLEMENTEDThe command is not supported.
◆ otCRPCProcessCmdLine()
| void otCRPCProcessCmdLine | ( | const char * |
aString,
|
| char * |
aOutput,
|
||
| size_t |
aOutputMaxLen
|
||
| ) |
Process a command-line string.
- Parameters
-
[in] aStringA NULL-terminated input string. [out] aOutputThe execution result. [in] aOutputMaxLenThe output buffer size.
◆ otCRPCProcessHelp()
| void otCRPCProcessHelp | ( | void * |
aContext,
|
| uint8_t |
aArgsLength,
|
||
| char * |
aArgs[]
|
||
| ) |
Output all available CRPC built-in commands and user commands.
- Parameters
-
aContextaArgsLengthaArgs
◆ otCRPCSetUserCommands()
| void otCRPCSetUserCommands | ( | const otCliCommand * |
aUserCommands,
|
| uint8_t |
aLength,
|
||
| void * |
aContext
|
||
| ) |
Set a user command table.
- Parameters
-
[in] aUserCommandsA pointer to an array with user commands. [in] aLengthaUserCommandslength.[in] aContextThecontext passed to the handler.