Instance

This module includes functions that control the OpenThread Instance.

Typedefs

typedef struct otInstance otInstance
 This structure represents the OpenThread instance structure.
 
typedef uint32_t otChangedFlags
 This type represents a bit-field indicating specific state/configuration that has changed.
 
typedef void(* otStateChangedCallback) (otChangedFlags aFlags, void *aContext)
 This function pointer is called to notify certain configuration or state changes within OpenThread.

Enumerations

enum  {
  OT_CHANGED_IP6_ADDRESS_ADDED = 1 << 0,
  OT_CHANGED_IP6_ADDRESS_REMOVED = 1 << 1,
  OT_CHANGED_THREAD_ROLE = 1 << 2,
  OT_CHANGED_THREAD_LL_ADDR = 1 << 3,
  OT_CHANGED_THREAD_ML_ADDR = 1 << 4,
  OT_CHANGED_THREAD_RLOC_ADDED = 1 << 5,
  OT_CHANGED_THREAD_RLOC_REMOVED = 1 << 6,
  OT_CHANGED_THREAD_PARTITION_ID = 1 << 7,
  OT_CHANGED_THREAD_KEY_SEQUENCE_COUNTER = 1 << 8,
  OT_CHANGED_THREAD_NETDATA = 1 << 9,
  OT_CHANGED_THREAD_CHILD_ADDED = 1 << 10,
  OT_CHANGED_THREAD_CHILD_REMOVED = 1 << 11,
  OT_CHANGED_IP6_MULTICAST_SUBSCRIBED = 1 << 12,
  OT_CHANGED_IP6_MULTICAST_UNSUBSCRIBED = 1 << 13,
  OT_CHANGED_THREAD_CHANNEL = 1 << 14,
  OT_CHANGED_THREAD_PANID = 1 << 15,
  OT_CHANGED_THREAD_NETWORK_NAME = 1 << 16,
  OT_CHANGED_THREAD_EXT_PANID = 1 << 17,
  OT_CHANGED_MASTER_KEY = 1 << 18,
  OT_CHANGED_PSKC = 1 << 19,
  OT_CHANGED_SECURITY_POLICY = 1 << 20,
  OT_CHANGED_CHANNEL_MANAGER_NEW_CHANNEL = 1 << 21,
  OT_CHANGED_SUPPORTED_CHANNEL_MASK = 1 << 22,
  OT_CHANGED_COMMISSIONER_STATE = 1 << 23,
  OT_CHANGED_THREAD_NETIF_STATE = 1 << 24,
  OT_CHANGED_THREAD_BACKBONE_ROUTER_STATE = 1 << 25,
  OT_CHANGED_THREAD_BACKBONE_ROUTER_LOCAL = 1 << 26,
  OT_CHANGED_JOINER_STATE = 1 << 27,
  OT_CHANGED_ACTIVE_DATASET = 1 << 28,
  OT_CHANGED_PENDING_DATASET = 1 << 29
}
 This enumeration defines flags that are passed as part of otStateChangedCallback.

Functions

otInstanceotInstanceInit (void *aInstanceBuffer, size_t *aInstanceBufferSize)
 This function initializes the OpenThread library.
 
otInstanceotInstanceInitSingle (void)
 This function initializes the static single instance of the OpenThread library.
 
bool otInstanceIsInitialized (otInstance *aInstance)
 This function indicates whether or not the instance is valid/initialized.
 
void otInstanceFinalize (otInstance *aInstance)
 This function disables the OpenThread library.
 
otError otSetStateChangedCallback (otInstance *aInstance, otStateChangedCallback aCallback, void *aContext)
 This function registers a callback to indicate when certain configuration or state changes within OpenThread.
 
void otRemoveStateChangeCallback (otInstance *aInstance, otStateChangedCallback aCallback, void *aContext)
 This function removes a callback to indicate when certain configuration or state changes within OpenThread.
 
void otInstanceReset (otInstance *aInstance)
 This method triggers a platform reset.
 
void otInstanceFactoryReset (otInstance *aInstance)
 This method deletes all the settings stored on non-volatile memory, and then triggers platform reset.
 
otError otInstanceErasePersistentInfo (otInstance *aInstance)
 This function erases all the OpenThread persistent info (network settings) stored on non-volatile memory.
 
const char * otGetVersionString (void)
 This function gets the OpenThread version string.
 
const char * otGetRadioVersionString (otInstance *aInstance)
 This function gets the OpenThread radio version string.

Detailed Description

This module includes functions that control the OpenThread Instance.

Typedef Documentation

◆ otChangedFlags

typedef uint32_t otChangedFlags

This type represents a bit-field indicating specific state/configuration that has changed.

See OT_CHANGED_* definitions.

◆ otStateChangedCallback

typedef void(* otStateChangedCallback) (otChangedFlags aFlags, void *aContext)

This function pointer is called to notify certain configuration or state changes within OpenThread.

Parameters
[in]aFlagsA bit-field indicating specific state that has changed. See OT_CHANGED_* definitions.
[in]aContextA pointer to application-specific context.

Enumeration Type Documentation

◆ anonymous enum

anonymous enum

This enumeration defines flags that are passed as part of otStateChangedCallback.

Enumerator
OT_CHANGED_IP6_ADDRESS_ADDED 

IPv6 address was added.

OT_CHANGED_IP6_ADDRESS_REMOVED 

IPv6 address was removed.

OT_CHANGED_THREAD_ROLE 

Role (disabled, detached, child, router, leader) changed.

OT_CHANGED_THREAD_LL_ADDR 

The link-local address changed.

OT_CHANGED_THREAD_ML_ADDR 

The mesh-local address changed.

OT_CHANGED_THREAD_RLOC_ADDED 

RLOC was added.

OT_CHANGED_THREAD_RLOC_REMOVED 

RLOC was removed.

OT_CHANGED_THREAD_PARTITION_ID 

Partition ID changed.

OT_CHANGED_THREAD_KEY_SEQUENCE_COUNTER 

Thread Key Sequence changed.

OT_CHANGED_THREAD_NETDATA 

Thread Network Data changed.

OT_CHANGED_THREAD_CHILD_ADDED 

Child was added.

OT_CHANGED_THREAD_CHILD_REMOVED 

Child was removed.

OT_CHANGED_IP6_MULTICAST_SUBSCRIBED 

Subscribed to a IPv6 multicast address.

OT_CHANGED_IP6_MULTICAST_UNSUBSCRIBED 

Unsubscribed from a IPv6 multicast address.

OT_CHANGED_THREAD_CHANNEL 

Thread network channel changed.

OT_CHANGED_THREAD_PANID 

Thread network PAN Id changed.

OT_CHANGED_THREAD_NETWORK_NAME 

Thread network name changed.

OT_CHANGED_THREAD_EXT_PANID 

Thread network extended PAN ID changed.

OT_CHANGED_MASTER_KEY 

Master key changed.

OT_CHANGED_PSKC 

PSKc changed.

OT_CHANGED_SECURITY_POLICY 

Security Policy changed.

OT_CHANGED_CHANNEL_MANAGER_NEW_CHANNEL 

Channel Manager new pending Thread channel changed.

OT_CHANGED_SUPPORTED_CHANNEL_MASK 

Supported channel mask changed.

OT_CHANGED_COMMISSIONER_STATE 

Commissioner state changed.

OT_CHANGED_THREAD_NETIF_STATE 

Thread network interface state changed.

OT_CHANGED_THREAD_BACKBONE_ROUTER_STATE 

Backbone Router state changed.

OT_CHANGED_THREAD_BACKBONE_ROUTER_LOCAL 

Local Backbone Router configuration changed.

OT_CHANGED_JOINER_STATE 

Joiner state changed.

OT_CHANGED_ACTIVE_DATASET 

Active Operational Dataset changed.

OT_CHANGED_PENDING_DATASET 

Pending Operational Dataset changed.

Function Documentation

◆ otGetRadioVersionString()

const char* otGetRadioVersionString ( otInstance aInstance)

This function gets the OpenThread radio version string.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
Returns
A pointer to the OpenThread radio version.

◆ otGetVersionString()

const char* otGetVersionString ( void  )

This function gets the OpenThread version string.

Returns
A pointer to the OpenThread version.

◆ otInstanceErasePersistentInfo()

otError otInstanceErasePersistentInfo ( otInstance aInstance)

This function erases all the OpenThread persistent info (network settings) stored on non-volatile memory.

Erase is successful only if the device is in disabled state/role.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
Return values
OT_ERROR_NONEAll persistent info/state was erased successfully.
OT_ERROR_INVALID_STATEDevice is not in disabled state/role.

◆ otInstanceFactoryReset()

void otInstanceFactoryReset ( otInstance aInstance)

This method deletes all the settings stored on non-volatile memory, and then triggers platform reset.

Parameters
[in]aInstanceA pointer to an OpenThread instance.

◆ otInstanceFinalize()

void otInstanceFinalize ( otInstance aInstance)

This function disables the OpenThread library.

Call this function when OpenThread is no longer in use.

Parameters
[in]aInstanceA pointer to an OpenThread instance.

◆ otInstanceInit()

otInstance* otInstanceInit ( void *  aInstanceBuffer,
size_t *  aInstanceBufferSize 
)

This function initializes the OpenThread library.

This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.

This function is available and can only be used when support for multiple OpenThread instances is enabled.

Parameters
[in]aInstanceBufferThe buffer for OpenThread to use for allocating the otInstance structure.
[in,out]aInstanceBufferSizeOn input, the size of aInstanceBuffer. On output, if not enough space for otInstance, the number of bytes required for otInstance.
Returns
A pointer to the new OpenThread instance.
See also
otInstanceFinalize

◆ otInstanceInitSingle()

otInstance* otInstanceInitSingle ( void  )

This function initializes the static single instance of the OpenThread library.

This function initializes OpenThread and prepares it for subsequent OpenThread API calls. This function must be called before any other calls to OpenThread.

This function is available and can only be used when support for multiple OpenThread instances is disabled.

Returns
A pointer to the single OpenThread instance.

◆ otInstanceIsInitialized()

bool otInstanceIsInitialized ( otInstance aInstance)

This function indicates whether or not the instance is valid/initialized.

The instance is considered valid if it is acquired and initialized using either otInstanceInitSingle() (in single instance case) or otInstanceInit() (in multi instance case). A subsequent call to otInstanceFinalize() causes the instance to be considered as uninitialized.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
Returns
TRUE if the given instance is valid/initialized, FALSE otherwise.

◆ otInstanceReset()

void otInstanceReset ( otInstance aInstance)

This method triggers a platform reset.

The reset process ensures that all the OpenThread state/info (stored in volatile memory) is erased. Note that the otPlatformReset does not erase any persistent state/info saved in non-volatile memory.

Parameters
[in]aInstanceA pointer to an OpenThread instance.

◆ otRemoveStateChangeCallback()

void otRemoveStateChangeCallback ( otInstance aInstance,
otStateChangedCallback  aCallback,
void *  aContext 
)

This function removes a callback to indicate when certain configuration or state changes within OpenThread.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aCallbackA pointer to a function that is called with certain configuration or state changes.
[in]aContextA pointer to application-specific context.

◆ otSetStateChangedCallback()

otError otSetStateChangedCallback ( otInstance aInstance,
otStateChangedCallback  aCallback,
void *  aContext 
)

This function registers a callback to indicate when certain configuration or state changes within OpenThread.

Parameters
[in]aInstanceA pointer to an OpenThread instance.
[in]aCallbackA pointer to a function that is called with certain configuration or state changes.
[in]aContextA pointer to application-specific context.
Return values
OT_ERROR_NONEAdded the callback to the list of callbacks.
OT_ERROR_ALREADYThe callback was already registered.
OT_ERROR_NO_BUFSCould not add the callback due to resource constraints.