otBackboneRouterConfig Struct Reference

This structure represents Backbone Router configuration.

#include < include/openthread/backbone_router.h >

Public Attributes

uint16_t mServer16
Only used when get Primary Backbone Router information in the Thread Network.
uint16_t mReregistrationDelay
Reregistration Delay (in seconds)
uint32_t mMlrTimeout
Multicast Listener Registration Timeout (in seconds)
uint8_t mSequenceNumber
Sequence Number.

This structure represents Backbone Router configuration.


The documentation for this struct was generated from the following file:
  • include/openthread/ backbone_router.h