otServerConfig Struct Reference

This structure represents a Server configuration.

#include < include/openthread/netdata.h >

Public Attributes

bool mStable : 1
TRUE, if this configuration is considered Stable Network Data. FALSE, otherwise.
uint8_t mServerDataLength
Length of server data.
uint8_t mServerData [ OT_SERVER_DATA_MAX_SIZE ]
Server data bytes.
uint16_t mRloc16
The Server RLOC16.

This structure represents a Server configuration.


The documentation for this struct was generated from the following file:
  • include/openthread/ netdata.h