UDP Forward
This module includes functions for UDP forward feature.
Typedefs | |
typedef void(* | otUdpForwarder) (otMessage *aMessage, uint16_t aPeerPort, otIp6Address *aPeerAddr, uint16_t aSockPort, void *aContext) |
This function pointer delivers the UDP packet to host and host should send the packet through its own network stack. |
Functions | |
void | otUdpForwardSetForwarder (otInstance *aInstance, otUdpForwarder aForwarder, void *aContext) |
Set UDP forward callback to deliver UDP packets to host. | |
void | otUdpForwardReceive (otInstance *aInstance, otMessage *aMessage, uint16_t aPeerPort, const otIp6Address *aPeerAddr, uint16_t aSockPort) |
Handle a UDP packet received from host. |
Detailed Description
This module includes functions for UDP forward feature.
The functions in this module are available when udp-forward feature (OPENTHREAD_CONFIG_UDP_FORWARD_ENABLE
) is enabled.
Typedef Documentation
◆ otUdpForwarder
typedef void(* otUdpForwarder) (otMessage *aMessage, uint16_t aPeerPort, otIp6Address *aPeerAddr, uint16_t aSockPort, void *aContext) |
This function pointer delivers the UDP packet to host and host should send the packet through its own network stack.
- Parameters
-
[in] aMessage
A pointer to the UDP Message. [in] aPeerPort
The destination UDP port. [in] aPeerAddr
A pointer to the destination IPv6 address. [in] aSockPort
The source UDP port. [in] aContext
A pointer to application-specific context.
Function Documentation
◆ otUdpForwardReceive()
void otUdpForwardReceive | ( | otInstance * | aInstance, |
otMessage * | aMessage, |
||
uint16_t | aPeerPort, |
||
const otIp6Address * | aPeerAddr, |
||
uint16_t | aSockPort |
||
) |
Handle a UDP packet received from host.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aMessage
A pointer to the UDP Message. [in] aPeerPort
The source UDP port. [in] aPeerAddr
A pointer to the source address. [in] aSockPort
The destination UDP port.
- Warning
- No matter the call success or fail, the message is freed.
◆ otUdpForwardSetForwarder()
void otUdpForwardSetForwarder | ( | otInstance * | aInstance, |
otUdpForwarder | aForwarder, |
||
void * | aContext |
||
) |
Set UDP forward callback to deliver UDP packets to host.
- Parameters
-
[in] aInstance
A pointer to an OpenThread instance. [in] aForwarder
A pointer to a function called to forward UDP packet to host. [in] aContext
A pointer to application-specific context.