otSrpClientService Struct Reference
This structure represents an SRP client service.
#include <
include/openthread/srp_client.h
>
Public Attributes |
|
| const char * | mName |
|
The service name labels (e.g., "_chip._udp", not the full domain name).
|
|
| const char * | mInstanceName |
|
The service instance name label (not the full name).
|
|
| const otDnsTxtEntry * | mTxtEntries |
Array of TXT entries (number of entries is given by
mNumTxtEntries
).
|
|
| uint16_t | mPort |
|
The service port number.
|
|
| uint16_t | mPriority |
|
The service priority.
|
|
| uint16_t | mWeight |
|
The service weight.
|
|
| uint8_t | mNumTxtEntries |
Number of entries in the
mTxtEntries
array.
|
|
| otSrpClientItemState | mState |
| uint32_t | mData |
|
Internal data (used by OT core).
|
|
| struct otSrpClientService * | mNext |
|
Pointer to next entry in a linked-list (managed by OT core).
|
|
This structure represents an SRP client service.
The values in this structure, including the string buffers for the names and the TXT record entries, MUST persist and stay constant after an instance of this structure is passed to OpenThread from
otSrpClientAddService()
or
otSrpClientRemoveService()
.
Member Data Documentation
◆ mState
| otSrpClientItemState otSrpClientService::mState |
- Note
-
The following fields are used/managed by OT core only. Their values do not matter and are ignored when an instance of
otSrpClientServiceis passed inotSrpClientAddService()orotSrpClientRemoveService(). The user should not modify these fields.Service state (managed by OT core).
The documentation for this struct was generated from the following file:
-
include/openthread/
srp_client.h