This structure represents the message buffer information.
#include <
include/openthread/message.h
>
Public Attributes |
|
| uint16_t | mTotalBuffers |
|
The number of buffers in the pool.
|
|
| uint16_t | mFreeBuffers |
|
The number of free message buffers.
|
|
| uint16_t | m6loSendMessages |
|
The number of messages in the 6lo send queue.
|
|
| uint16_t | m6loSendBuffers |
|
The number of buffers in the 6lo send queue.
|
|
| uint16_t | m6loReassemblyMessages |
|
The number of messages in the 6LoWPAN reassembly queue.
|
|
| uint16_t | m6loReassemblyBuffers |
|
The number of buffers in the 6LoWPAN reassembly queue.
|
|
| uint16_t | mIp6Messages |
|
The number of messages in the IPv6 send queue.
|
|
| uint16_t | mIp6Buffers |
|
The number of buffers in the IPv6 send queue.
|
|
| uint16_t | mMplMessages |
|
The number of messages in the MPL send queue.
|
|
| uint16_t | mMplBuffers |
|
The number of buffers in the MPL send queue.
|
|
| uint16_t | mMleMessages |
|
The number of messages in the MLE send queue.
|
|
| uint16_t | mMleBuffers |
|
The number of buffers in the MLE send queue.
|
|
| uint16_t | mArpMessages |
|
The number of messages in the ARP send queue.
|
|
| uint16_t | mArpBuffers |
|
The number of buffers in the ARP send queue.
|
|
| uint16_t | mCoapMessages |
|
The number of messages in the CoAP send queue.
|
|
| uint16_t | mCoapBuffers |
|
The number of buffers in the CoAP send queue.
|
|
| uint16_t | mCoapSecureMessages |
|
The number of messages in the CoAP secure send queue.
|
|
| uint16_t | mCoapSecureBuffers |
|
The number of buffers in the CoAP secure send queue.
|
|
| uint16_t | mApplicationCoapMessages |
|
The number of messages in the application CoAP send queue.
|
|
| uint16_t | mApplicationCoapBuffers |
|
The number of buffers in the application CoAP send queue.
|
|
This structure represents the message buffer information.
The documentation for this struct was generated from the following file:
-
include/openthread/
message.h