Logging
This module includes the platform abstraction for the debug log service.
Macros | |
#define | OT_LOG_LEVEL_NONE 0 |
Log level None. | |
#define | OT_LOG_LEVEL_CRIT 1 |
Log level Critical. | |
#define | OT_LOG_LEVEL_WARN 2 |
Log level Warning. | |
#define | OT_LOG_LEVEL_NOTE 3 |
Log level Notice. | |
#define | OT_LOG_LEVEL_INFO 4 |
Log level Informational. | |
#define | OT_LOG_LEVEL_DEBG 5 |
Log level Debug. |
Typedefs | |
typedef int | otLogLevel |
This type represents the log level. | |
typedef enum otLogRegion | otLogRegion |
This enumeration represents log regions. |
Enumerations | |
enum | otLogRegion { OT_LOG_REGION_API = 1, OT_LOG_REGION_MLE = 2, OT_LOG_REGION_ARP = 3, OT_LOG_REGION_NET_DATA = 4, OT_LOG_REGION_ICMP = 5, OT_LOG_REGION_IP6 = 6, OT_LOG_REGION_MAC = 7, OT_LOG_REGION_MEM = 8, OT_LOG_REGION_NCP = 9, OT_LOG_REGION_MESH_COP = 10, OT_LOG_REGION_NET_DIAG = 11, OT_LOG_REGION_PLATFORM = 12, OT_LOG_REGION_COAP = 13, OT_LOG_REGION_CLI = 14, OT_LOG_REGION_CORE = 15, OT_LOG_REGION_UTIL = 16, OT_LOG_REGION_BBR = 17, OT_LOG_REGION_MLR = 18, OT_LOG_REGION_DUA = 19, OT_LOG_REGION_BR = 20, OT_LOG_REGION_SRP = 21, OT_LOG_REGION_DNS = 22 } |
This enumeration represents log regions. |
Functions | |
void | otPlatLog (otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aFormat,...) |
This function outputs logs. | |
void | otPlatLogLine (otLogLevel aLogLevel, otLogRegion aLogRegion, const char *aLogLine) |
This (optional) platform function outputs a prepared log line. |
Detailed Description
This module includes the platform abstraction for the debug log service.
Macro Definition Documentation
◆ OT_LOG_LEVEL_CRIT
#define OT_LOG_LEVEL_CRIT 1 |
Log level Critical.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_DEBG
#define OT_LOG_LEVEL_DEBG 5 |
Log level Debug.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_INFO
#define OT_LOG_LEVEL_INFO 4 |
Log level Informational.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_NONE
#define OT_LOG_LEVEL_NONE 0 |
Log level None.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_NOTE
#define OT_LOG_LEVEL_NOTE 3 |
Log level Notice.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
◆ OT_LOG_LEVEL_WARN
#define OT_LOG_LEVEL_WARN 2 |
Log level Warning.
- Note
- Log Levels are defines so that embedded implementations can eliminate code at compile time via #if/#else/#endif.
Enumeration Type Documentation
◆ otLogRegion
enum otLogRegion |
This enumeration represents log regions.
Function Documentation
◆ otPlatLog()
void otPlatLog | ( | otLogLevel | aLogLevel, |
otLogRegion | aLogRegion, |
||
const char * | aFormat, |
||
... |
|||
) |
This function outputs logs.
- Parameters
-
[in] aLogLevel
The log level. [in] aLogRegion
The log region. [in] aFormat
A pointer to the format string. [in] ...
Arguments for the format specification.
◆ otPlatLogLine()
void otPlatLogLine | ( | otLogLevel | aLogLevel, |
otLogRegion | aLogRegion, |
||
const char * | aLogLine |
||
) |
This (optional) platform function outputs a prepared log line.
This platform function is used by OpenThread core when OPENTHREAD_CONFIG_LOG_DEFINE_AS_MACRO_ONLY
is not enabled (in this case, the OT core itself will prepare a full log line).
Note that this function is optional and if not provided by platform layer, a default (weak) implementation is provided and used by OpenThread core as otPlatLog(aLogLevel, aLogResion, "%s", aLogLine)
.
- Parameters
-
[in] aLogLevel
The log level. [in] aLogRegion
The log region. [in] aLogLine
A pointer to a log line string.