Operation
This module includes the platform abstraction for radio operations.
Functions |
|
| otRadioState | otPlatRadioGetState ( otInstance *aInstance) |
|
Get current state of the radio.
|
|
| otError | otPlatRadioEnable ( otInstance *aInstance) |
|
Enable the radio.
|
|
| otError | otPlatRadioDisable ( otInstance *aInstance) |
|
Disable the radio.
|
|
| bool | otPlatRadioIsEnabled ( otInstance *aInstance) |
|
Check whether radio is enabled or not.
|
|
| otError | otPlatRadioSleep ( otInstance *aInstance) |
|
Transition the radio from Receive to Sleep (turn off the radio).
|
|
| otError | otPlatRadioReceive ( otInstance *aInstance, uint8_t aChannel) |
|
Transition the radio from Sleep to Receive (turn on the radio).
|
|
| otError | otPlatRadioReceiveAt ( otInstance *aInstance, uint8_t aChannel, uint32_t aStart, uint32_t aDuration) |
|
Schedule a radio reception window at a specific time and duration.
|
|
| void | otPlatRadioReceiveDone ( otInstance *aInstance, otRadioFrame *aFrame, otError aError) |
|
The radio driver calls this method to notify OpenThread of a received frame.
|
|
| void | otPlatDiagRadioReceiveDone ( otInstance *aInstance, otRadioFrame *aFrame, otError aError) |
|
The radio driver calls this method to notify OpenThread diagnostics module of a received frame.
|
|
| otRadioFrame * | otPlatRadioGetTransmitBuffer ( otInstance *aInstance) |
|
Get the radio transmit frame buffer.
|
|
| otError | otPlatRadioTransmit ( otInstance *aInstance, otRadioFrame *aFrame) |
|
Begin the transmit sequence on the radio.
|
|
| void | otPlatRadioTxStarted ( otInstance *aInstance, otRadioFrame *aFrame) |
|
The radio driver calls this method to notify OpenThread that the transmission has started.
|
|
| void | otPlatRadioTxDone ( otInstance *aInstance, otRadioFrame *aFrame, otRadioFrame *aAckFrame, otError aError) |
|
The radio driver calls this function to notify OpenThread that the transmit operation has completed, providing both the transmitted frame and, if applicable, the received ack frame.
|
|
| void | otPlatDiagRadioTransmitDone ( otInstance *aInstance, otRadioFrame *aFrame, otError aError) |
|
The radio driver calls this method to notify OpenThread diagnostics module that the transmission has completed.
|
|
| int8_t | otPlatRadioGetRssi ( otInstance *aInstance) |
|
Get the most recent RSSI measurement.
|
|
| otError | otPlatRadioEnergyScan ( otInstance *aInstance, uint8_t aScanChannel, uint16_t aScanDuration) |
|
Begin the energy scan sequence on the radio.
|
|
| void | otPlatRadioEnergyScanDone ( otInstance *aInstance, int8_t aEnergyScanMaxRssi) |
|
The radio driver calls this method to notify OpenThread that the energy scan is complete.
|
|
| void | otPlatRadioEnableSrcMatch ( otInstance *aInstance, bool aEnable) |
|
Enable/Disable source address match feature.
|
|
| otError | otPlatRadioAddSrcMatchShortEntry ( otInstance *aInstance, otShortAddress aShortAddress) |
|
Add a short address to the source address match table.
|
|
| otError | otPlatRadioAddSrcMatchExtEntry ( otInstance *aInstance, const otExtAddress *aExtAddress) |
|
Add an extended address to the source address match table.
|
|
| otError | otPlatRadioClearSrcMatchShortEntry ( otInstance *aInstance, otShortAddress aShortAddress) |
|
Remove a short address from the source address match table.
|
|
| otError | otPlatRadioClearSrcMatchExtEntry ( otInstance *aInstance, const otExtAddress *aExtAddress) |
|
Remove an extended address from the source address match table.
|
|
| void | otPlatRadioClearSrcMatchShortEntries ( otInstance *aInstance) |
|
Clear all short addresses from the source address match table.
|
|
| void | otPlatRadioClearSrcMatchExtEntries ( otInstance *aInstance) |
|
Clear all the extended/long addresses from source address match table.
|
|
| uint32_t | otPlatRadioGetSupportedChannelMask ( otInstance *aInstance) |
|
Get the radio supported channel mask that the device is allowed to be on.
|
|
| uint32_t | otPlatRadioGetPreferredChannelMask ( otInstance *aInstance) |
|
Get the radio preferred channel mask that the device prefers to form on.
|
|
| otError | otPlatRadioSetCoexEnabled ( otInstance *aInstance, bool aEnabled) |
|
Enable the radio coex.
|
|
| bool | otPlatRadioIsCoexEnabled ( otInstance *aInstance) |
|
Check whether radio coex is enabled or not.
|
|
| otError | otPlatRadioGetCoexMetrics ( otInstance *aInstance, otRadioCoexMetrics *aCoexMetrics) |
|
Get the radio coexistence metrics.
|
|
| otError | otPlatRadioEnableCsl ( otInstance *aInstance, uint32_t aCslPeriod, const otExtAddress *aExtAddr) |
|
Enable or disable CSL receiver.
|
|
| void | otPlatRadioUpdateCslSampleTime ( otInstance *aInstance, uint32_t aCslSampleTime) |
|
Update CSL sample time in radio driver.
|
|
| uint8_t | otPlatRadioGetCslAccuracy ( otInstance *aInstance) |
|
Get the current accuracy, in units of ± ppm, of the clock used for scheduling CSL operations.
|
|
| otError | otPlatRadioSetChannelMaxTransmitPower ( otInstance *aInstance, uint8_t aChannel, int8_t aMaxPower) |
|
Set the max transmit power for a specific channel.
|
|
| otError | otPlatRadioSetRegion ( otInstance *aInstance, uint16_t aRegionCode) |
|
Set the region code.
|
|
| otError | otPlatRadioGetRegion ( otInstance *aInstance, uint16_t *aRegionCode) |
|
Get the region code.
|
|
| otError | otPlatRadioConfigureEnhAckProbing ( otInstance *aInstance, otLinkMetrics aLinkMetrics, otShortAddress aShortAddress, const otExtAddress *aExtAddress) |
|
Enable/disable or update Enhanced-ACK Based Probing in radio for a specific Initiator.
|
|
Detailed Description
This module includes the platform abstraction for radio operations.
Function Documentation
◆ otPlatDiagRadioReceiveDone()
| void otPlatDiagRadioReceiveDone | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame,
|
||
| otError |
aError
|
||
| ) |
The radio driver calls this method to notify OpenThread diagnostics module of a received frame.
This function is used when diagnostics is enabled.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aFrameA pointer to the received frame or NULL if the receive operation failed. [in] aErrorOT_ERROR_NONE when successfully received a frame, OT_ERROR_ABORT when reception was aborted and a frame was not received, OT_ERROR_NO_BUFS when a frame could not be received due to lack of rx buffer space.
◆ otPlatDiagRadioTransmitDone()
| void otPlatDiagRadioTransmitDone | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame,
|
||
| otError |
aError
|
||
| ) |
The radio driver calls this method to notify OpenThread diagnostics module that the transmission has completed.
This function is used when diagnostics is enabled.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aFrameA pointer to the frame that was transmitted. [in] aErrorOT_ERROR_NONE when the frame was transmitted, OT_ERROR_CHANNEL_ACCESS_FAILURE tx could not take place due to activity on the channel, OT_ERROR_ABORT when transmission was aborted for other reasons.
◆ otPlatRadioAddSrcMatchExtEntry()
| otError otPlatRadioAddSrcMatchExtEntry | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress
|
||
| ) |
Add an extended address to the source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aExtAddressThe extended address to be added stored in little-endian byte order.
- Return values
-
OT_ERROR_NONESuccessfully added extended address to the source match table. OT_ERROR_NO_BUFSNo available entry in the source match table.
◆ otPlatRadioAddSrcMatchShortEntry()
| otError otPlatRadioAddSrcMatchShortEntry | ( | otInstance * |
aInstance,
|
| otShortAddress |
aShortAddress
|
||
| ) |
Add a short address to the source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aShortAddressThe short address to be added.
- Return values
-
OT_ERROR_NONESuccessfully added short address to the source match table. OT_ERROR_NO_BUFSNo available entry in the source match table.
◆ otPlatRadioClearSrcMatchExtEntries()
| void otPlatRadioClearSrcMatchExtEntries | ( | otInstance * |
aInstance
|
) |
Clear all the extended/long addresses from source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
◆ otPlatRadioClearSrcMatchExtEntry()
| otError otPlatRadioClearSrcMatchExtEntry | ( | otInstance * |
aInstance,
|
| const otExtAddress * |
aExtAddress
|
||
| ) |
Remove an extended address from the source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aExtAddressThe extended address to be removed stored in little-endian byte order.
- Return values
-
OT_ERROR_NONESuccessfully removed the extended address from the source match table. OT_ERROR_NO_ADDRESSThe extended address is not in source address match table.
◆ otPlatRadioClearSrcMatchShortEntries()
| void otPlatRadioClearSrcMatchShortEntries | ( | otInstance * |
aInstance
|
) |
Clear all short addresses from the source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
◆ otPlatRadioClearSrcMatchShortEntry()
| otError otPlatRadioClearSrcMatchShortEntry | ( | otInstance * |
aInstance,
|
| otShortAddress |
aShortAddress
|
||
| ) |
Remove a short address from the source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aShortAddressThe short address to be removed.
- Return values
-
OT_ERROR_NONESuccessfully removed short address from the source match table. OT_ERROR_NO_ADDRESSThe short address is not in source address match table.
◆ otPlatRadioConfigureEnhAckProbing()
| otError otPlatRadioConfigureEnhAckProbing | ( | otInstance * |
aInstance,
|
| otLinkMetrics |
aLinkMetrics,
|
||
| otShortAddress |
aShortAddress,
|
||
| const otExtAddress * |
aExtAddress
|
||
| ) |
Enable/disable or update Enhanced-ACK Based Probing in radio for a specific Initiator.
After Enhanced-ACK Based Probing is configured by a specific Probing Initiator, the Enhanced-ACK sent to that node should include Vendor-Specific IE containing Link Metrics data. This method informs the radio to start/stop to collect Link Metrics data and include Vendor-Specific IE that containing the data in Enhanced-ACK sent to that Probing Initiator.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aLinkMetricsThis parameter specifies what metrics to query. Per spec 4.11.3.4.4.6, at most 2 metrics can be specified. The probing would be disabled if is bitwise 0.aLinkMetrics[in] aShortAddrThe short address of the Probing Initiator. [in] aExtAddrThe extended source address of the Probing Initiator. aExtAddrMUST NOT beNULL.
- Return values
-
OT_ERROR_NONESuccessfully configured the Enhanced-ACK Based Probing. OT_ERROR_INVALID_ARGSaExtAddressisNULL.OT_ERROR_NOT_FOUNDThe Initiator indicated by aShortAddressis not found when trying to clear.OT_ERROR_NO_BUFSNo more Initiator can be supported.
◆ otPlatRadioDisable()
| otError otPlatRadioDisable | ( | otInstance * |
aInstance
|
) |
Disable the radio.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Return values
-
OT_ERROR_NONESuccessfully transitioned to Disabled. OT_ERROR_INVALID_STATEThe radio was not in sleep state.
◆ otPlatRadioEnable()
| otError otPlatRadioEnable | ( | otInstance * |
aInstance
|
) |
Enable the radio.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Return values
-
OT_ERROR_NONESuccessfully enabled. OT_ERROR_FAILEDThe radio could not be enabled.
◆ otPlatRadioEnableCsl()
| otError otPlatRadioEnableCsl | ( | otInstance * |
aInstance,
|
| uint32_t |
aCslPeriod,
|
||
| const otExtAddress * |
aExtAddr
|
||
| ) |
Enable or disable CSL receiver.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aCslPeriodCSL period, 0 for disabling CSL. [in] aExtAddrThe extended source address of CSL receiver's parent device (when the platforms generate enhanced ack, platforms may need to know acks to which address should include CSL IE).
- Return values
-
OT_ERROR_NOT_SUPPORTEDRadio driver doesn't support CSL. OT_ERROR_FAILEDOther platform specific errors. OT_ERROR_NONESuccessfully enabled or disabled CSL.
◆ otPlatRadioEnableSrcMatch()
| void otPlatRadioEnableSrcMatch | ( | otInstance * |
aInstance,
|
| bool |
aEnable
|
||
| ) |
Enable/Disable source address match feature.
The source address match feature controls how the radio layer decides the "frame pending" bit for acks sent in response to data request commands from children.
If disabled, the radio layer must set the "frame pending" on all acks to data request commands.
If enabled, the radio layer uses the source address match table to determine whether to set or clear the "frame pending" bit in an ack to a data request command.
The source address match table provides the list of children for which there is a pending frame. Either a short address or an extended/long address can be added to the source address match table.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aEnableEnable/disable source address match feature.
◆ otPlatRadioEnergyScan()
| otError otPlatRadioEnergyScan | ( | otInstance * |
aInstance,
|
| uint8_t |
aScanChannel,
|
||
| uint16_t |
aScanDuration
|
||
| ) |
Begin the energy scan sequence on the radio.
This function is used when radio provides OT_RADIO_CAPS_ENERGY_SCAN capability.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aScanChannelThe channel to perform the energy scan on. [in] aScanDurationThe duration, in milliseconds, for the channel to be scanned.
- Return values
-
OT_ERROR_NONESuccessfully started scanning the channel. OT_ERROR_NOT_IMPLEMENTEDThe radio doesn't support energy scanning.
◆ otPlatRadioEnergyScanDone()
| void otPlatRadioEnergyScanDone | ( | otInstance * |
aInstance,
|
| int8_t |
aEnergyScanMaxRssi
|
||
| ) |
The radio driver calls this method to notify OpenThread that the energy scan is complete.
This function is used when radio provides OT_RADIO_CAPS_ENERGY_SCAN capability.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aEnergyScanMaxRssiThe maximum RSSI encountered on the scanned channel.
◆ otPlatRadioGetCoexMetrics()
| otError otPlatRadioGetCoexMetrics | ( | otInstance * |
aInstance,
|
| otRadioCoexMetrics * |
aCoexMetrics
|
||
| ) |
Get the radio coexistence metrics.
This function is used when feature OPENTHREAD_CONFIG_PLATFORM_RADIO_COEX_ENABLE is enabled.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [out] aCoexMetricsA pointer to the coexistence metrics structure.
- Return values
-
OT_ERROR_NONESuccessfully retrieved the coex metrics. OT_ERROR_INVALID_ARGSaCoexMetricswas NULL.
◆ otPlatRadioGetCslAccuracy()
| uint8_t otPlatRadioGetCslAccuracy | ( | otInstance * |
aInstance
|
) |
Get the current accuracy, in units of ± ppm, of the clock used for scheduling CSL operations.
- Note
- Platforms may optimize this value based on operational conditions (i.e.: temperature).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- The current CSL rx/tx scheduling drift, in units of ± ppm.
◆ otPlatRadioGetPreferredChannelMask()
| uint32_t otPlatRadioGetPreferredChannelMask | ( | otInstance * |
aInstance
|
) |
Get the radio preferred channel mask that the device prefers to form on.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- The radio preferred channel mask.
◆ otPlatRadioGetRegion()
| otError otPlatRadioGetRegion | ( | otInstance * |
aInstance,
|
| uint16_t * |
aRegionCode
|
||
| ) |
Get the region code.
The radio region format is the 2-bytes ascii representation of the ISO 3166 alpha-2 code.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [out] aRegionCodeThe radio region.
- Return values
-
OT_ERROR_INVALID_ARGSaRegionCodeis nullptr.OT_ERROR_FAILEDOther platform specific errors. OT_ERROR_NONESuccessfully got region code.
◆ otPlatRadioGetRssi()
| int8_t otPlatRadioGetRssi | ( | otInstance * |
aInstance
|
) |
Get the most recent RSSI measurement.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- The RSSI in dBm when it is valid. 127 when RSSI is invalid.
◆ otPlatRadioGetState()
| otRadioState otPlatRadioGetState | ( | otInstance * |
aInstance
|
) |
Get current state of the radio.
This function is not required by OpenThread. It may be used for debugging and/or application-specific purposes.
- Note
- This function may be not implemented. It does not affect OpenThread.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- Current state of the radio.
◆ otPlatRadioGetSupportedChannelMask()
| uint32_t otPlatRadioGetSupportedChannelMask | ( | otInstance * |
aInstance
|
) |
Get the radio supported channel mask that the device is allowed to be on.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- The radio supported channel mask.
◆ otPlatRadioGetTransmitBuffer()
| otRadioFrame * otPlatRadioGetTransmitBuffer | ( | otInstance * |
aInstance
|
) |
Get the radio transmit frame buffer.
OpenThread forms the IEEE 802.15.4 frame in this buffer then calls
otPlatRadioTransmit()
to request transmission.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- A pointer to the transmit frame buffer.
◆ otPlatRadioIsCoexEnabled()
| bool otPlatRadioIsCoexEnabled | ( | otInstance * |
aInstance
|
) |
Check whether radio coex is enabled or not.
This function is used when feature OPENTHREAD_CONFIG_PLATFORM_RADIO_COEX_ENABLE is enabled.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- TRUE if the radio coex is enabled, FALSE otherwise.
◆ otPlatRadioIsEnabled()
| bool otPlatRadioIsEnabled | ( | otInstance * |
aInstance
|
) |
Check whether radio is enabled or not.
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Returns
- TRUE if the radio is enabled, FALSE otherwise.
◆ otPlatRadioReceive()
| otError otPlatRadioReceive | ( | otInstance * |
aInstance,
|
| uint8_t |
aChannel
|
||
| ) |
Transition the radio from Sleep to Receive (turn on the radio).
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aChannelThe channel to use for receiving.
- Return values
-
OT_ERROR_NONESuccessfully transitioned to Receive. OT_ERROR_INVALID_STATEThe radio was disabled or transmitting.
◆ otPlatRadioReceiveAt()
| otError otPlatRadioReceiveAt | ( | otInstance * |
aInstance,
|
| uint8_t |
aChannel,
|
||
| uint32_t |
aStart,
|
||
| uint32_t |
aDuration
|
||
| ) |
Schedule a radio reception window at a specific time and duration.
- Parameters
-
[in] aChannelThe radio channel on which to receive. [in] aStartThe receive window start time, in microseconds. [in] aDurationThe receive window duration, in microseconds
- Return values
-
OT_ERROR_NONESuccessfully scheduled receive window. OT_ERROR_FAILEDThe receive window could not be scheduled.
◆ otPlatRadioReceiveDone()
| void otPlatRadioReceiveDone | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame,
|
||
| otError |
aError
|
||
| ) |
The radio driver calls this method to notify OpenThread of a received frame.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aFrameA pointer to the received frame or NULL if the receive operation failed. [in] aErrorOT_ERROR_NONE when successfully received a frame, OT_ERROR_ABORT when reception was aborted and a frame was not received, OT_ERROR_NO_BUFS when a frame could not be received due to lack of rx buffer space.
◆ otPlatRadioSetChannelMaxTransmitPower()
| otError otPlatRadioSetChannelMaxTransmitPower | ( | otInstance * |
aInstance,
|
| uint8_t |
aChannel,
|
||
| int8_t |
aMaxPower
|
||
| ) |
Set the max transmit power for a specific channel.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aChannelThe radio channel. [in] aMaxPowerThe max power in dBm, passing OT_RADIO_RSSI_INVALID will disable this channel.
- Return values
-
OT_ERROR_NOT_IMPLEMENTEDThe feature is not implemented OT_ERROR_INVALID_ARGSThe specified channel is not valid. OT_ERROR_FAILEDOther platform specific errors. OT_ERROR_NONESuccessfully set max transmit poewr.
◆ otPlatRadioSetCoexEnabled()
| otError otPlatRadioSetCoexEnabled | ( | otInstance * |
aInstance,
|
| bool |
aEnabled
|
||
| ) |
Enable the radio coex.
This function is used when feature OPENTHREAD_CONFIG_PLATFORM_RADIO_COEX_ENABLE is enabled.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aEnabledTRUE to enable the radio coex, FALSE otherwise.
- Return values
-
OT_ERROR_NONESuccessfully enabled. OT_ERROR_FAILEDThe radio coex could not be enabled.
◆ otPlatRadioSetRegion()
| otError otPlatRadioSetRegion | ( | otInstance * |
aInstance,
|
| uint16_t |
aRegionCode
|
||
| ) |
Set the region code.
The radio region format is the 2-bytes ascii representation of the ISO 3166 alpha-2 code.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aRegionCodeThe radio region.
- Return values
-
OT_ERROR_FAILEDOther platform specific errors. OT_ERROR_NONESuccessfully set region code.
◆ otPlatRadioSleep()
| otError otPlatRadioSleep | ( | otInstance * |
aInstance
|
) |
Transition the radio from Receive to Sleep (turn off the radio).
- Parameters
-
[in] aInstanceThe OpenThread instance structure.
- Return values
-
OT_ERROR_NONESuccessfully transitioned to Sleep. OT_ERROR_BUSYThe radio was transmitting. OT_ERROR_INVALID_STATEThe radio was disabled.
◆ otPlatRadioTransmit()
| otError otPlatRadioTransmit | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame
|
||
| ) |
Begin the transmit sequence on the radio.
The caller must form the IEEE 802.15.4 frame in the buffer provided by
otPlatRadioGetTransmitBuffer()
before requesting transmission. The channel and transmit power are also included in the
otRadioFrame
structure.
The transmit sequence consists of:
-
Transitioning the radio to Transmit from one of the following states:
- Receive if RX is on when the device is idle or OT_RADIO_CAPS_SLEEP_TO_TX is not supported
- Sleep if RX is off when the device is idle and OT_RADIO_CAPS_SLEEP_TO_TX is supported.
- Transmits the psdu on the given channel and at the given transmit power.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aFrameA pointer to the frame to be transmitted.
- Return values
-
OT_ERROR_NONESuccessfully transitioned to Transmit. OT_ERROR_INVALID_STATEThe radio was not in the Receive state.
◆ otPlatRadioTxDone()
| void otPlatRadioTxDone | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame,
|
||
| otRadioFrame * |
aAckFrame,
|
||
| otError |
aError
|
||
| ) |
The radio driver calls this function to notify OpenThread that the transmit operation has completed, providing both the transmitted frame and, if applicable, the received ack frame.
When radio provides
OT_RADIO_CAPS_TRANSMIT_SEC
capability, radio platform layer updates
aFrame
with the security frame counter and key index values maintained by the radio.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aFrameA pointer to the frame that was transmitted. [in] aAckFrameA pointer to the ACK frame, NULL if no ACK was received. [in] aErrorOT_ERROR_NONE when the frame was transmitted, OT_ERROR_NO_ACK when the frame was transmitted but no ACK was received, OT_ERROR_CHANNEL_ACCESS_FAILURE tx could not take place due to activity on the channel, OT_ERROR_ABORT when transmission was aborted for other reasons.
◆ otPlatRadioTxStarted()
| void otPlatRadioTxStarted | ( | otInstance * |
aInstance,
|
| otRadioFrame * |
aFrame
|
||
| ) |
The radio driver calls this method to notify OpenThread that the transmission has started.
- Note
- This function should be called by the same thread that executes all of the other OpenThread code. It should not be called by ISR or any other task.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance structure. [in] aFrameA pointer to the frame that is being transmitted.
◆ otPlatRadioUpdateCslSampleTime()
| void otPlatRadioUpdateCslSampleTime | ( | otInstance * |
aInstance,
|
| uint32_t |
aCslSampleTime
|
||
| ) |
Update CSL sample time in radio driver.
Sample time is stored in radio driver as a copy to calculate phase when sending ACK with CSL IE.
- Parameters
-
[in] aInstanceThe OpenThread instance structure. [in] aCslSampleTimeThe latest sample time.