otNeighborInfo Struct Reference

This structure holds diagnostic information for a neighboring Thread node.

#include < include/openthread/thread.h >

Public Attributes

otExtAddress mExtAddress
IEEE 802.15.4 Extended Address.
uint32_t mAge
Time last heard.
uint16_t mRloc16
RLOC16.
uint32_t mLinkFrameCounter
Link Frame Counter.
uint32_t mMleFrameCounter
MLE Frame Counter.
uint8_t mLinkQualityIn
Link Quality In.
int8_t mAverageRssi
Average RSSI.
int8_t mLastRssi
Last observed RSSI.
uint16_t mFrameErrorRate
Frame error rate (0xffff->100%). Requires error tracking feature.
uint16_t mMessageErrorRate
(IPv6) msg error rate (0xffff->100%). Requires error tracking feature.
bool mRxOnWhenIdle : 1
rx-on-when-idle
bool mFullThreadDevice : 1
Full Thread Device.
bool mFullNetworkData : 1
Full Network Data.
bool mIsChild : 1
Is the neighbor a child.

This structure holds diagnostic information for a neighboring Thread node.


The documentation for this struct was generated from the following file:
  • include/openthread/ thread.h