DNSv6
This module includes functions that control DNS communication.
Classes |
|
| struct | otDnsTxtEntry |
|
This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).
|
|
| struct | otDnsTxtEntryIterator |
|
This structure represents an iterator for TXT record entires (key/value pairs).
|
|
| struct | otDnsQueryConfig |
|
This structure represents a DNS query configuration.
|
|
| struct | otDnsServiceInfo |
|
This structure provides info for a DNS service instance.
|
|
Macros |
|
| #define | OT_DNS_MAX_NAME_SIZE 255 |
|
Maximum name string size (includes null char at the end of string).
|
|
| #define | OT_DNS_MAX_LABEL_SIZE 64 |
|
Maximum label string size (include null char at the end of string).
|
|
| #define | OT_DNS_TXT_KEY_MIN_LENGTH 1 |
|
Minimum length of TXT record key string (RFC 6763 - section 6.4).
|
|
| #define | OT_DNS_TXT_KEY_MAX_LENGTH 9 |
|
Recommended maximum length of TXT record key string (RFC 6763 - section 6.4).
|
|
Typedefs |
|
| typedef struct otDnsTxtEntry | otDnsTxtEntry |
|
This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).
|
|
| typedef struct otDnsTxtEntryIterator | otDnsTxtEntryIterator |
|
This structure represents an iterator for TXT record entires (key/value pairs).
|
|
| typedef struct otDnsQueryConfig | otDnsQueryConfig |
|
This structure represents a DNS query configuration.
|
|
| typedef struct otDnsAddressResponse | otDnsAddressResponse |
|
This type is an opaque representation of a response to an address resolution DNS query.
|
|
| typedef void(* | otDnsAddressCallback ) ( otError aError, const otDnsAddressResponse *aResponse, void *aContext) |
|
This function pointer is called when a DNS response is received for an address resolution query.
|
|
| typedef struct otDnsBrowseResponse | otDnsBrowseResponse |
|
This type is an opaque representation of a response to a browse (service instance enumeration) DNS query.
|
|
| typedef void(* | otDnsBrowseCallback ) ( otError aError, const otDnsBrowseResponse *aResponse, void *aContext) |
|
This function pointer is called when a DNS response is received for a browse (service instance enumeration) query.
|
|
| typedef struct otDnsServiceInfo | otDnsServiceInfo |
|
This structure provides info for a DNS service instance.
|
|
| typedef struct otDnsServiceResponse | otDnsServiceResponse |
|
This type is an opaque representation of a response to a service instance resolution DNS query.
|
|
| typedef void(* | otDnsServiceCallback ) ( otError aError, const otDnsServiceResponse *aResponse, void *aContext) |
|
This function pointer is called when a DNS response is received for a service instance resolution query.
|
|
Enumerations |
|
| enum |
otDnsRecursionFlag
{
OT_DNS_FLAG_UNSPECIFIED = 0, OT_DNS_FLAG_RECURSION_DESIRED = 1, OT_DNS_FLAG_NO_RECURSION = 2 } |
This enumeration type represents the "Recursion Desired" (RD) flag in an
otDnsQueryConfig
.
|
|
| enum |
otDnsNat64Mode
{
OT_DNS_NAT64_UNSPECIFIED = 0, OT_DNS_NAT64_ALLOW = 1, OT_DNS_NAT64_DISALLOW = 2 } |
This enumeration type represents the NAT64 mode in an
otDnsQueryConfig
.
|
|
Functions |
|
| void | otDnsInitTxtEntryIterator ( otDnsTxtEntryIterator *aIterator, const uint8_t *aTxtData, uint16_t aTxtDataLength) |
|
This function initializes a TXT record iterator.
|
|
| otError | otDnsGetNextTxtEntry ( otDnsTxtEntryIterator *aIterator, otDnsTxtEntry *aEntry) |
|
This function parses the TXT data from an iterator and gets the next TXT record entry (key/value pair).
|
|
| void | otDnsSetNameCompressionEnabled (bool aEnabled) |
|
This function enables/disables the "DNS name compression" mode.
|
|
| bool | otDnsIsNameCompressionEnabled (void) |
|
This function indicates whether the "DNS name compression" mode is enabled or not.
|
|
| const otDnsQueryConfig * | otDnsClientGetDefaultConfig ( otInstance *aInstance) |
|
This function gets the current default query config used by DNS client.
|
|
| void | otDnsClientSetDefaultConfig ( otInstance *aInstance, const otDnsQueryConfig *aConfig) |
|
This function sets the default query config on DNS client.
|
|
| otError | otDnsClientResolveAddress ( otInstance *aInstance, const char *aHostName, otDnsAddressCallback aCallback, void *aContext, const otDnsQueryConfig *aConfig) |
|
This function sends an address resolution DNS query for AAAA (IPv6) record(s) for a given host name.
|
|
| otError | otDnsAddressResponseGetHostName (const otDnsAddressResponse *aResponse, char *aNameBuffer, uint16_t aNameBufferSize) |
|
This function gets the full host name associated with an address resolution DNS response.
|
|
| otError | otDnsAddressResponseGetAddress (const otDnsAddressResponse *aResponse, uint16_t aIndex, otIp6Address *aAddress, uint32_t *aTtl) |
|
This function gets an IPv6 address associated with an address resolution DNS response.
|
|
| otError | otDnsClientBrowse ( otInstance *aInstance, const char *aServiceName, otDnsBrowseCallback aCallback, void *aContext, const otDnsQueryConfig *aConfig) |
|
This function sends a DNS browse (service instance enumeration) query for a given service name.
|
|
| otError | otDnsBrowseResponseGetServiceName (const otDnsBrowseResponse *aResponse, char *aNameBuffer, uint16_t aNameBufferSize) |
|
This function gets the service name associated with a DNS browse (service instance enumeration) response.
|
|
| otError | otDnsBrowseResponseGetServiceInstance (const otDnsBrowseResponse *aResponse, uint16_t aIndex, char *aLabelBuffer, uint8_t aLabelBufferSize) |
|
This function gets a service instance associated with a DNS browse (service instance enumeration) response.
|
|
| otError | otDnsBrowseResponseGetServiceInfo (const otDnsBrowseResponse *aResponse, const char *aInstanceLabel, otDnsServiceInfo *aServiceInfo) |
|
This function gets info for a service instance from a DNS browse (service instance enumeration) response.
|
|
| otError | otDnsBrowseResponseGetHostAddress (const otDnsBrowseResponse *aResponse, const char *aHostName, uint16_t aIndex, otIp6Address *aAddress, uint32_t *aTtl) |
|
This function gets the host IPv6 address from a DNS browse (service instance enumeration) response.
|
|
| otError | otDnsClientResolveService ( otInstance *aInstance, const char *aInstanceLabel, const char *aServiceName, otDnsServiceCallback aCallback, void *aContext, const otDnsQueryConfig *aConfig) |
|
This function sends a DNS service instance resolution query for a given service instance.
|
|
| otError | otDnsServiceResponseGetServiceName (const otDnsServiceResponse *aResponse, char *aLabelBuffer, uint8_t aLabelBufferSize, char *aNameBuffer, uint16_t aNameBufferSize) |
|
This function gets the service instance name associated with a DNS service instance resolution response.
|
|
| otError | otDnsServiceResponseGetServiceInfo (const otDnsServiceResponse *aResponse, otDnsServiceInfo *aServiceInfo) |
|
This function gets info for a service instance from a DNS service instance resolution response.
|
|
| otError | otDnsServiceResponseGetHostAddress (const otDnsServiceResponse *aResponse, const char *aHostName, uint16_t aIndex, otIp6Address *aAddress, uint32_t *aTtl) |
|
This function gets the host IPv6 address from a DNS service instance resolution response.
|
|
Detailed Description
This module includes functions that control DNS communication.
The functions in this module are available only if feature
OPENTHREAD_CONFIG_DNS_CLIENT_ENABLE
is enabled.
Typedef Documentation
◆ otDnsAddressCallback
| typedef void(* otDnsAddressCallback) ( otError aError, const otDnsAddressResponse *aResponse, void *aContext) |
This function pointer is called when a DNS response is received for an address resolution query.
Within this callback the user can use
otDnsAddressResponseGet{Item}()
functions along with the
aResponse
pointer to get more info about the response.
The
aResponse
pointer can only be used within this callback and after returning from this function it will not stay valid, so the user MUST NOT retain the
aResponse
pointer for later use.
- Parameters
-
[in] aErrorThe result of the DNS transaction. [in] aResponseA pointer to the response (it is always non-NULL). [in] aContextA pointer to application-specific context.
The
aError
can have the following:
- OT_ERROR_NONE A response was received successfully.
- OT_ERROR_ABORT A DNS transaction was aborted by stack.
- OT_ERROR_RESPONSE_TIMEOUT No DNS response has been received within timeout.
If the server rejects the address resolution request the error code from server is mapped as follow:
- (0) NOERROR Success (no error condition) -> OT_ERROR_NONE
- (1) FORMERR Server unable to interpret due to format error -> OT_ERROR_PARSE
- (2) SERVFAIL Server encountered an internal failure -> OT_ERROR_FAILED
- (3) NXDOMAIN Name that ought to exist, does not exist -> OT_ERROR_NOT_FOUND
- (4) NOTIMP Server does not support the query type (OpCode) -> OT_ERROR_NOT_IMPLEMENTED
- (5) REFUSED Server refused for policy/security reasons -> OT_ERROR_SECURITY
- (6) YXDOMAIN Some name that ought not to exist, does exist -> OT_ERROR_DUPLICATED
- (7) YXRRSET Some RRset that ought not to exist, does exist -> OT_ERROR_DUPLICATED
- (8) NXRRSET Some RRset that ought to exist, does not exist -> OT_ERROR_NOT_FOUND
- (9) NOTAUTH Service is not authoritative for zone -> OT_ERROR_SECURITY
- (10) NOTZONE A name is not in the zone -> OT_ERROR_PARSE
- (20) BADNAME Bad name -> OT_ERROR_PARSE
- (21) BADALG Bad algorithm -> OT_ERROR_SECURITY
- (22) BADTRUN Bad truncation -> OT_ERROR_PARSE
- Other response codes -> OT_ERROR_FAILED
◆ otDnsAddressResponse
| typedef struct otDnsAddressResponse otDnsAddressResponse |
This type is an opaque representation of a response to an address resolution DNS query.
Pointers to instance of this type are provided from callback
otDnsAddressCallback
.
◆ otDnsBrowseCallback
| typedef void(* otDnsBrowseCallback) ( otError aError, const otDnsBrowseResponse *aResponse, void *aContext) |
This function pointer is called when a DNS response is received for a browse (service instance enumeration) query.
Within this callback the user can use
otDnsBrowseResponseGet{Item}()
functions along with the
aResponse
pointer to get more info about the response.
The
aResponse
pointer can only be used within this callback and after returning from this function it will not stay valid, so the user MUST NOT retain the
aResponse
pointer for later use.
- Parameters
-
[in] aErrorThe result of the DNS transaction. [in] aResponseA pointer to the response (it is always non-NULL). [in] aContextA pointer to application-specific context.
For the full list of possible values for
aError
, please see
otDnsAddressCallback()
.
◆ otDnsBrowseResponse
| typedef struct otDnsBrowseResponse otDnsBrowseResponse |
This type is an opaque representation of a response to a browse (service instance enumeration) DNS query.
Pointers to instance of this type are provided from callback
otDnsBrowseCallback
.
◆ otDnsQueryConfig
| typedef struct otDnsQueryConfig otDnsQueryConfig |
This structure represents a DNS query configuration.
Any of the fields in this structure can be set to zero to indicate that it is not specified. How the unspecified fields are treated is determined by the function which uses the instance of
otDnsQueryConfig
.
◆ otDnsServiceCallback
| typedef void(* otDnsServiceCallback) ( otError aError, const otDnsServiceResponse *aResponse, void *aContext) |
This function pointer is called when a DNS response is received for a service instance resolution query.
Within this callback the user can use
otDnsServiceResponseGet{Item}()
functions along with the
aResponse
pointer to get more info about the response.
The
aResponse
pointer can only be used within this callback and after returning from this function it will not stay valid, so the user MUST NOT retain the
aResponse
pointer for later use.
- Parameters
-
[in] aErrorThe result of the DNS transaction. [in] aResponseA pointer to the response (it is always non-NULL). [in] aContextA pointer to application-specific context.
For the full list of possible values for
aError
, please see
otDnsAddressCallback()
.
◆ otDnsServiceResponse
| typedef struct otDnsServiceResponse otDnsServiceResponse |
This type is an opaque representation of a response to a service instance resolution DNS query.
Pointers to instance of this type are provided from callback
otDnsAddressCallback
.
◆ otDnsTxtEntry
| typedef struct otDnsTxtEntry otDnsTxtEntry |
This structure represents a TXT record entry representing a key/value pair (RFC 6763 - section 6.3).
The string buffers pointed to by
mKey
and
mValue
MUST persist and remain unchanged after an instance of such structure is passed to OpenThread (as part of
otSrpClientService
instance).
An array of
otDnsTxtEntry
entries are used in
otSrpClientService
to specify the full TXT record (a list of entries).
◆ otDnsTxtEntryIterator
| typedef struct otDnsTxtEntryIterator otDnsTxtEntryIterator |
This structure represents an iterator for TXT record entires (key/value pairs).
The data fields in this structure are intended for use by OpenThread core and caller should not read or change them.
Enumeration Type Documentation
◆ otDnsNat64Mode
| enum otDnsNat64Mode |
This enumeration type represents the NAT64 mode in an
otDnsQueryConfig
.
The NAT64 mode indicates whether to allow or disallow NAT64 address translation during DNS client address resolution. This mode is only used when
OPENTHREAD_CONFIG_DNS_CLIENT_NAT64_ENABLE
is enabled.
◆ otDnsRecursionFlag
| enum otDnsRecursionFlag |
This enumeration type represents the "Recursion Desired" (RD) flag in an
otDnsQueryConfig
.
Function Documentation
◆ otDnsAddressResponseGetAddress()
| otError otDnsAddressResponseGetAddress | ( | const otDnsAddressResponse * |
aResponse,
|
| uint16_t |
aIndex,
|
||
| otIp6Address * |
aAddress,
|
||
| uint32_t * |
aTtl
|
||
| ) |
This function gets an IPv6 address associated with an address resolution DNS response.
This function MUST only be used from
otDnsAddressCallback
.
The response may include multiple IPv6 address records.
aIndex
can be used to iterate through the list of addresses. Index zero gets the first address and so on. When we reach end of the list,
OT_ERROR_NOT_FOUND
is returned.
- Parameters
-
[in] aResponseA pointer to the response. [in] aIndexThe address record index to retrieve. [out] aAddressA pointer to a IPv6 address to output the address (MUST NOT be NULL). [out] aTtlA pointer to an uint32_tto output TTL for the address. It can be NULL if caller does not want to get the TTL.
- Return values
-
OT_ERROR_NONEThe address was read successfully. OT_ERROR_NOT_FOUNDNo address record in aResponseataIndex.OT_ERROR_PARSECould not parse the records in the aResponse.
◆ otDnsAddressResponseGetHostName()
| otError otDnsAddressResponseGetHostName | ( | const otDnsAddressResponse * |
aResponse,
|
| char * |
aNameBuffer,
|
||
| uint16_t |
aNameBufferSize
|
||
| ) |
This function gets the full host name associated with an address resolution DNS response.
This function MUST only be used from
otDnsAddressCallback
.
- Parameters
-
[in] aResponseA pointer to the response. [out] aNameBufferA buffer to char array to output the full host name (MUST NOT be NULL). [in] aNameBufferSizeThe size of aNameBuffer.
- Return values
-
OT_ERROR_NONEThe full host name was read successfully. OT_ERROR_NO_BUFSThe name does not fit in aNameBuffer.
◆ otDnsBrowseResponseGetHostAddress()
| otError otDnsBrowseResponseGetHostAddress | ( | const otDnsBrowseResponse * |
aResponse,
|
| const char * |
aHostName,
|
||
| uint16_t |
aIndex,
|
||
| otIp6Address * |
aAddress,
|
||
| uint32_t * |
aTtl
|
||
| ) |
This function gets the host IPv6 address from a DNS browse (service instance enumeration) response.
This function MUST only be used from
otDnsBrowseCallback
.
The response can include zero or more IPv6 address records.
aIndex
can be used to iterate through the list of addresses. Index zero gets the first address and so on. When we reach end of the list,
OT_ERROR_NOT_FOUND
is returned.
- Parameters
-
[in] aResponseA pointer to the response. [in] aHostNameThe host name to get the address (MUST NOT be NULL). [in] aIndexThe address record index to retrieve. [out] aAddressA pointer to a IPv6 address to output the address (MUST NOT be NULL). [out] aTtlA pointer to an uint32_tto output TTL for the address. It can be NULL if caller does not want to get the TTL.
- Return values
-
OT_ERROR_NONEThe address was read successfully. OT_ERROR_NOT_FOUNDNo address record for aHostnameinaResponseataIndex.OT_ERROR_PARSECould not parse the records in the aResponse.
◆ otDnsBrowseResponseGetServiceInfo()
| otError otDnsBrowseResponseGetServiceInfo | ( | const otDnsBrowseResponse * |
aResponse,
|
| const char * |
aInstanceLabel,
|
||
| otDnsServiceInfo * |
aServiceInfo
|
||
| ) |
This function gets info for a service instance from a DNS browse (service instance enumeration) response.
This function MUST only be used from
otDnsBrowseCallback
.
A browse DNS response should include the SRV, TXT, and AAAA records for the service instances that are enumerated (note that it is a SHOULD and not a MUST requirement). This function tries to retrieve this info for a given service instance when available.
-
If no matching SRV record is found in
aResponse,OT_ERROR_NOT_FOUNDis returned. -
If a matching SRV record is found in
aResponse,aServiceInfois updated andOT_ERROR_NONEis returned. -
If no matching TXT record is found in
aResponse,mTxtDataSizeinaServiceInfois set to zero. -
If no matching AAAA record is found in
aResponse,mHostAddress is set to all zero or unspecified address. -
If there are multiple AAAA records for the host name in @p aResponse,mHostAddressis set to the first one. The other addresses can be retrieved usingotDnsBrowseResponseGetHostAddress() `.
- Parameters
-
[in] aResponseA pointer to the response. [in] aInstanceLabelThe service instance label (MUST NOT be NULL). [out] aServiceInfoA ServiceInfoto output the service instance information (MUST NOT be NULL).
- Return values
-
OT_ERROR_NONEThe service instance info was read. aServiceInfois updated.OT_ERROR_NOT_FOUNDCould not find a matching SRV record for aInstanceLabel.OT_ERROR_NO_BUFSThe host name and/or TXT data could not fit in the given buffers. OT_ERROR_PARSECould not parse the records in the aResponse.
◆ otDnsBrowseResponseGetServiceInstance()
| otError otDnsBrowseResponseGetServiceInstance | ( | const otDnsBrowseResponse * |
aResponse,
|
| uint16_t |
aIndex,
|
||
| char * |
aLabelBuffer,
|
||
| uint8_t |
aLabelBufferSize
|
||
| ) |
This function gets a service instance associated with a DNS browse (service instance enumeration) response.
This function MUST only be used from
otDnsBrowseCallback
.
The response may include multiple service instance records.
aIndex
can be used to iterate through the list. Index zero gives the the first record. When we reach end of the list,
OT_ERROR_NOT_FOUND
is returned.
Note that this function gets the service instance label and not the full service instance name which is of the form
<Instance>.<Service>.<Domain>
.
- Parameters
-
[in] aResponseA pointer to the response. [in] aIndexThe service instance record index to retrieve. [out] aLabelBufferA buffer to char array to output the service instance label (MUST NOT be NULL). [in] aLabelBufferSizeThe size of aLabelBuffer.
- Return values
-
OT_ERROR_NONEThe service instance was read successfully. OT_ERROR_NO_BUFSThe name does not fit in aNameBuffer.OT_ERROR_NOT_FOUNDNo service instance record in aResponseataIndex.OT_ERROR_PARSECould not parse the records in the aResponse.
◆ otDnsBrowseResponseGetServiceName()
| otError otDnsBrowseResponseGetServiceName | ( | const otDnsBrowseResponse * |
aResponse,
|
| char * |
aNameBuffer,
|
||
| uint16_t |
aNameBufferSize
|
||
| ) |
This function gets the service name associated with a DNS browse (service instance enumeration) response.
This function MUST only be used from
otDnsBrowseCallback
.
- Parameters
-
[in] aResponseA pointer to the response. [out] aNameBufferA buffer to char array to output the service name (MUST NOT be NULL). [in] aNameBufferSizeThe size of aNameBuffer.
- Return values
-
OT_ERROR_NONEThe service name was read successfully. OT_ERROR_NO_BUFSThe name does not fit in aNameBuffer.
◆ otDnsClientBrowse()
| otError otDnsClientBrowse | ( | otInstance * |
aInstance,
|
| const char * |
aServiceName,
|
||
| otDnsBrowseCallback |
aCallback,
|
||
| void * |
aContext,
|
||
| const otDnsQueryConfig * |
aConfig
|
||
| ) |
This function sends a DNS browse (service instance enumeration) query for a given service name.
This function is available when
OPENTHREAD_CONFIG_DNS_CLIENT_SERVICE_DISCOVERY_ENABLE
is enabled.
The
aConfig
can be NULL. In this case the default config (from
otDnsClientGetDefaultConfig()
) will be used as the config for this query. In a non-NULL
aConfig
, some of the fields can be left unspecified (value zero). The unspecified fields are then replaced by the values from the default config.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aServiceNameThe service name to query for (MUST NOT be NULL). [in] aCallbackA function pointer that shall be called on response reception or time-out. [in] aContextA pointer to arbitrary context information. [in] aConfigA pointer to the config to use for this query.
- Return values
-
OT_ERROR_NONEQuery sent successfully. aCallbackwill be invoked to report the status.OT_ERROR_NO_BUFSInsufficient buffer to prepare and send query.
◆ otDnsClientGetDefaultConfig()
| const otDnsQueryConfig * otDnsClientGetDefaultConfig | ( | otInstance * |
aInstance
|
) |
This function gets the current default query config used by DNS client.
When OpenThread stack starts, the default DNS query config is determined from a set of OT config options such as
OPENTHREAD_CONFIG_DNS_CLIENT_DEFAULT_SERVER_IP6_ADDRESS
,
_DEFAULT_SERVER_PORT
,
_DEFAULT_RESPONSE_TIMEOUT
, etc. (see
config/dns_client.h
for all related config options).
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- A pointer to the current default config being used by DNS client.
◆ otDnsClientResolveAddress()
| otError otDnsClientResolveAddress | ( | otInstance * |
aInstance,
|
| const char * |
aHostName,
|
||
| otDnsAddressCallback |
aCallback,
|
||
| void * |
aContext,
|
||
| const otDnsQueryConfig * |
aConfig
|
||
| ) |
This function sends an address resolution DNS query for AAAA (IPv6) record(s) for a given host name.
The
aConfig
can be NULL. In this case the default config (from
otDnsClientGetDefaultConfig()
) will be used as the config for this query. In a non-NULL
aConfig
, some of the fields can be left unspecified (value zero). The unspecified fields are then replaced by the values from the default config.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aHostNameThe host name for which to query the address (MUST NOT be NULL). [in] aCallbackA function pointer that shall be called on response reception or time-out. [in] aContextA pointer to arbitrary context information. [in] aConfigA pointer to the config to use for this query.
- Return values
-
OT_ERROR_NONEQuery sent successfully. aCallbackwill be invoked to report the status.OT_ERROR_NO_BUFSInsufficient buffer to prepare and send query.
◆ otDnsClientResolveService()
| otError otDnsClientResolveService | ( | otInstance * |
aInstance,
|
| const char * |
aInstanceLabel,
|
||
| const char * |
aServiceName,
|
||
| otDnsServiceCallback |
aCallback,
|
||
| void * |
aContext,
|
||
| const otDnsQueryConfig * |
aConfig
|
||
| ) |
This function sends a DNS service instance resolution query for a given service instance.
This function is available when
OPENTHREAD_CONFIG_DNS_CLIENT_SERVICE_DISCOVERY_ENABLE
is enabled.
The
aConfig
can be NULL. In this case the default config (from
otDnsClientGetDefaultConfig()
) will be used as the config for this query. In a non-NULL
aConfig
, some of the fields can be left unspecified (value zero). The unspecified fields are then replaced by the values from the default config.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aInstanceLabelThe service instance label. [in] aServiceNameThe service name (together with aInstanceLabelform full instance name).[in] aCallbackA function pointer that shall be called on response reception or time-out. [in] aContextA pointer to arbitrary context information. [in] aConfigA pointer to the config to use for this query.
- Return values
-
OT_ERROR_NONEQuery sent successfully. aCallbackwill be invoked to report the status.OT_ERROR_NO_BUFSInsufficient buffer to prepare and send query. OT_ERROR_INVALID_ARGSaInstanceLabelis NULL.
◆ otDnsClientSetDefaultConfig()
| void otDnsClientSetDefaultConfig | ( | otInstance * |
aInstance,
|
| const otDnsQueryConfig * |
aConfig
|
||
| ) |
This function sets the default query config on DNS client.
- Note
- Any ongoing query will continue to use the config from when it was started. The new default config will be used for any future DNS queries.
The
aConfig
can be NULL. In this case the default config will be set to the defaults from OT config options
OPENTHREAD_CONFIG_DNS_CLIENT_DEFAULT_{}
. This resets the default query config back to to the config when the OpenThread stack starts.
In a non-NULL
aConfig
, caller can choose to leave some of the fields in
otDnsQueryConfig
instance unspecified (value zero). The unspecified fields are replaced by the corresponding OT config option definitions
OPENTHREAD_CONFIG_DNS_CLIENT_DEFAULT_{}
to form the default query config.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aConfigA pointer to the new query config to use as default.
◆ otDnsGetNextTxtEntry()
| otError otDnsGetNextTxtEntry | ( | otDnsTxtEntryIterator * |
aIterator,
|
| otDnsTxtEntry * |
aEntry
|
||
| ) |
This function parses the TXT data from an iterator and gets the next TXT record entry (key/value pair).
The
aIterator
MUST be initialized using
otDnsInitTxtEntryIterator()
before calling this function and the TXT data buffer used to initialize the iterator MUST persist and remain unchanged. Otherwise the behavior of this function is undefined.
If the parsed key string length is smaller than or equal to
OT_DNS_TXT_KEY_MAX_LENGTH
(recommended max key length) the key string is returned in
mKey
in
aEntry
. But if the key is longer, then
mKey
is set to NULL and the entire encoded TXT entry string is returned in
mValue
and
mValueLength
.
- Parameters
-
[in] aIteratorA pointer to the iterator (MUST NOT be NULL). [out] aEntryA pointer to a otDnsTxtEntrystructure to output the parsed/read entry (MUST NOT be NULL).
- Return values
-
OT_ERROR_NONEThe next entry was parsed successfully. aEntryis updated.OT_ERROR_NOT_FOUNDNo more entries in the TXT data. OT_ERROR_PARSEThe TXT data from aIteratoris not well-formed.
◆ otDnsInitTxtEntryIterator()
| void otDnsInitTxtEntryIterator | ( | otDnsTxtEntryIterator * |
aIterator,
|
| const uint8_t * |
aTxtData,
|
||
| uint16_t |
aTxtDataLength
|
||
| ) |
This function initializes a TXT record iterator.
The buffer pointer
aTxtData
and its content MUST persist and remain unchanged while
aIterator
object is being used.
- Parameters
-
[in] aIteratorA pointer to the iterator to initialize (MUST NOT be NULL). [in] aTxtDataA pointer to buffer containing the encoded TXT data. [in] aTxtDataLengthThe length (number of bytes) of aTxtData.
◆ otDnsIsNameCompressionEnabled()
| bool otDnsIsNameCompressionEnabled | ( | void |
|
) |
This function indicates whether the "DNS name compression" mode is enabled or not.
This is intended for testing only and available when
OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
config is enabled.
- Returns
- TRUE if the "DNS name compression" mode is enabled, FALSE otherwise.
◆ otDnsServiceResponseGetHostAddress()
| otError otDnsServiceResponseGetHostAddress | ( | const otDnsServiceResponse * |
aResponse,
|
| const char * |
aHostName,
|
||
| uint16_t |
aIndex,
|
||
| otIp6Address * |
aAddress,
|
||
| uint32_t * |
aTtl
|
||
| ) |
This function gets the host IPv6 address from a DNS service instance resolution response.
This function MUST only be used from
otDnsServiceCallback
.
The response can include zero or more IPv6 address records.
aIndex
can be used to iterate through the list of addresses. Index zero gets the first address and so on. When we reach end of the list,
OT_ERROR_NOT_FOUND
is returned.
- Parameters
-
[in] aResponseA pointer to the response. [in] aHostNameThe host name to get the address (MUST NOT be NULL). [in] aIndexThe address record index to retrieve. [out] aAddressA pointer to a IPv6 address to output the address (MUST NOT be NULL). [out] aTtlA pointer to an uint32_tto output TTL for the address. It can be NULL if caller does not want to get the TTL.
- Return values
-
OT_ERROR_NONEThe address was read successfully. OT_ERROR_NOT_FOUNDNo address record for aHostnameinaResponseataIndex.OT_ERROR_PARSECould not parse the records in the aResponse.
◆ otDnsServiceResponseGetServiceInfo()
| otError otDnsServiceResponseGetServiceInfo | ( | const otDnsServiceResponse * |
aResponse,
|
| otDnsServiceInfo * |
aServiceInfo
|
||
| ) |
This function gets info for a service instance from a DNS service instance resolution response.
This function MUST only be used from
otDnsServiceCallback
.
-
If no matching SRV record is found in
aResponse,OT_ERROR_NOT_FOUNDis returned. -
If a matching SRV record is found in
aResponse,aServiceInfois updated andOT_ERROR_NONEis returned. -
If no matching TXT record is found in
aResponse,mTxtDataSizeinaServiceInfois set to zero. -
If no matching AAAA record is found in
aResponse,mHostAddress is set to all zero or unspecified address. -
If there are multiple AAAA records for the host name in @p aResponse,mHostAddressis set to the first one. The other addresses can be retrieved usingotDnsServiceResponseGetHostAddress() `.
- Parameters
-
[in] aResponseA pointer to the response. [out] aServiceInfoA ServiceInfoto output the service instance information (MUST NOT be NULL).
- Return values
-
OT_ERROR_NONEThe service instance info was read. aServiceInfois updated.OT_ERROR_NOT_FOUNDCould not find a matching SRV record in aResponse.OT_ERROR_NO_BUFSThe host name and/or TXT data could not fit in the given buffers. OT_ERROR_PARSECould not parse the records in the aResponse.
◆ otDnsServiceResponseGetServiceName()
| otError otDnsServiceResponseGetServiceName | ( | const otDnsServiceResponse * |
aResponse,
|
| char * |
aLabelBuffer,
|
||
| uint8_t |
aLabelBufferSize,
|
||
| char * |
aNameBuffer,
|
||
| uint16_t |
aNameBufferSize
|
||
| ) |
This function gets the service instance name associated with a DNS service instance resolution response.
This function MUST only be used from
otDnsServiceCallback
.
- Parameters
-
[in] aResponseA pointer to the response. [out] aLabelBufferA buffer to char array to output the service instance label (MUST NOT be NULL). [in] aLabelBufferSizeThe size of aLabelBuffer.[out] aNameBufferA buffer to char array to output the rest of service name (can be NULL if user is not interested in getting the name. [in] aNameBufferSizeThe size of aNameBuffer.
- Return values
-
OT_ERROR_NONEThe service name was read successfully. OT_ERROR_NO_BUFSEither the label or name does not fit in the given buffers.
◆ otDnsSetNameCompressionEnabled()
| void otDnsSetNameCompressionEnabled | ( | bool |
aEnabled
|
) |
This function enables/disables the "DNS name compression" mode.
By default DNS name compression is enabled. When disabled, DNS names are appended as full and never compressed. This is applicable to OpenThread's DNS and SRP client/server modules.
This is intended for testing only and available when
OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
config is enabled.
Note that in the case
OPENTHREAD_CONFIG_MULTIPLE_INSTANCE_ENABLE
is used, this mode applies to all OpenThread instances (i.e., calling this function enables/disables the compression mode on all OpenThread instances).
- Parameters
-
[in] aEnabledTRUE to enable the "DNS name compression" mode, FALSE to disable.