SRP
This module includes functions that control SRP client behavior.
Classes |
|
| struct | otSrpClientHostInfo |
|
This structure represents an SRP client host info.
|
|
| struct | otSrpClientService |
|
This structure represents an SRP client service.
|
|
| struct | otSrpClientBuffersServiceEntry |
|
This struct represents a SRP client service pool entry.
|
|
| struct | otSrpServerLeaseConfig |
|
This structure includes SRP server LEASE and KEY-LEASE configurations.
|
|
Typedefs |
|
| typedef struct otSrpClientHostInfo | otSrpClientHostInfo |
|
This structure represents an SRP client host info.
|
|
| typedef struct otSrpClientService | otSrpClientService |
|
This structure represents an SRP client service.
|
|
| typedef void(* | otSrpClientCallback ) ( otError aError, const otSrpClientHostInfo *aHostInfo, const otSrpClientService *aServices, const otSrpClientService *aRemovedServices, void *aContext) |
|
This function pointer type defines the callback used by SRP client to notify user of changes/events/errors.
|
|
| typedef void(* | otSrpClientAutoStartCallback ) (const otSockAddr *aServerSockAddr, void *aContext) |
|
This function pointer type defines the callback used by SRP client to notify user when it is auto-started or stopped.
|
|
| typedef struct otSrpClientBuffersServiceEntry | otSrpClientBuffersServiceEntry |
|
This struct represents a SRP client service pool entry.
|
|
| typedef void | otSrpServerHost |
|
This opaque type represents a SRP service host.
|
|
| typedef void | otSrpServerService |
|
This opaque type represents a SRP service.
|
|
| typedef uint32_t | otSrpServerServiceUpdateId |
|
The ID of a SRP service update transaction on the SRP Server.
|
|
| typedef struct otSrpServerLeaseConfig | otSrpServerLeaseConfig |
|
This structure includes SRP server LEASE and KEY-LEASE configurations.
|
|
| typedef void(* | otSrpServerServiceUpdateHandler ) ( otSrpServerServiceUpdateId aId, const otSrpServerHost *aHost, uint32_t aTimeout, void *aContext) |
|
This function handles SRP service updates.
|
|
Enumerations |
|
| enum |
otSrpClientItemState
{
OT_SRP_CLIENT_ITEM_STATE_TO_ADD , OT_SRP_CLIENT_ITEM_STATE_ADDING , OT_SRP_CLIENT_ITEM_STATE_TO_REFRESH , OT_SRP_CLIENT_ITEM_STATE_REFRESHING , OT_SRP_CLIENT_ITEM_STATE_TO_REMOVE , OT_SRP_CLIENT_ITEM_STATE_REMOVING , OT_SRP_CLIENT_ITEM_STATE_REGISTERED , OT_SRP_CLIENT_ITEM_STATE_REMOVED } |
|
This enumeration specifies an SRP client item (service or host info) state.
|
|
Functions |
|
| otError | otSrpClientStart ( otInstance *aInstance, const otSockAddr *aServerSockAddr) |
|
This function starts the SRP client operation.
|
|
| void | otSrpClientStop ( otInstance *aInstance) |
|
This function stops the SRP client operation.
|
|
| bool | otSrpClientIsRunning ( otInstance *aInstance) |
|
This function indicates whether the SRP client is running or not.
|
|
| const otSockAddr * | otSrpClientGetServerAddress ( otInstance *aInstance) |
|
This function gets the socket address (IPv6 address and port number) of the SRP server which is being used by SRP client.
|
|
| void | otSrpClientSetCallback ( otInstance *aInstance, otSrpClientCallback aCallback, void *aContext) |
|
This function sets the callback to notify caller of events/changes from SRP client.
|
|
| void | otSrpClientEnableAutoStartMode ( otInstance *aInstance, otSrpClientAutoStartCallback aCallback, void *aContext) |
|
This function enables the auto-start mode.
|
|
| void | otSrpClientDisableAutoStartMode ( otInstance *aInstance) |
|
This function disables the auto-start mode.
|
|
| bool | otSrpClientIsAutoStartModeEnabled ( otInstance *aInstance) |
|
This function indicates the current state of auto-start mode (enabled or disabled).
|
|
| uint32_t | otSrpClientGetLeaseInterval ( otInstance *aInstance) |
|
This function gets the lease interval used in SRP update requests.
|
|
| void | otSrpClientSetLeaseInterval ( otInstance *aInstance, uint32_t aInterval) |
|
This function sets the lease interval used in SRP update requests.
|
|
| uint32_t | otSrpClientGetKeyLeaseInterval ( otInstance *aInstance) |
|
This function gets the key lease interval used in SRP update requests.
|
|
| void | otSrpClientSetKeyLeaseInterval ( otInstance *aInstance, uint32_t aInterval) |
|
This function sets the key lease interval used in SRP update requests.
|
|
| const otSrpClientHostInfo * | otSrpClientGetHostInfo ( otInstance *aInstance) |
|
This function gets the host info.
|
|
| otError | otSrpClientSetHostName ( otInstance *aInstance, const char *aName) |
|
This function sets the host name label.
|
|
| otError | otSrpClientSetHostAddresses ( otInstance *aInstance, const otIp6Address *aIp6Addresses, uint8_t aNumAddresses) |
|
This function sets/updates the list of host IPv6 address.
|
|
| otError | otSrpClientAddService ( otInstance *aInstance, otSrpClientService *aService) |
|
This function adds a service to be registered with server.
|
|
| otError | otSrpClientRemoveService ( otInstance *aInstance, otSrpClientService *aService) |
|
This function requests a service to be unregistered with server.
|
|
| const otSrpClientService * | otSrpClientGetServices ( otInstance *aInstance) |
|
This function gets the list of services being managed by client.
|
|
| otError | otSrpClientRemoveHostAndServices ( otInstance *aInstance, bool aRemoveKeyLease) |
|
This function starts the remove process of the host info and all services.
|
|
| void | otSrpClientClearHostAndServices ( otInstance *aInstance) |
|
This function clears all host info and all the services.
|
|
| const char * | otSrpClientGetDomainName ( otInstance *aInstance) |
|
This function gets the domain name being used by SRP client.
|
|
| otError | otSrpClientSetDomainName ( otInstance *aInstance, const char *aName) |
|
This function sets the domain name to be used by SRP client.
|
|
| const char * | otSrpClientItemStateToString ( otSrpClientItemState aItemState) |
This function converts a
otSrpClientItemState
to a string.
|
|
| void | otSrpClientSetServiceKeyRecordEnabled ( otInstance *aInstance, bool aEnabled) |
|
This function enables/disables "service key record inclusion" mode.
|
|
| bool | otSrpClientIsServiceKeyRecordEnabled ( otInstance *aInstance) |
|
This method indicates whether the "service key record inclusion" mode is enabled or disabled.
|
|
| char * | otSrpClientBuffersGetHostNameString ( otInstance *aInstance, uint16_t *aSize) |
|
This function gets the string buffer to use for SRP client host name.
|
|
| otIp6Address * | otSrpClientBuffersGetHostAddressesArray ( otInstance *aInstance, uint8_t *aArrayLength) |
|
This function gets the array of IPv6 address entries to use as SRP client host address list.
|
|
| otSrpClientBuffersServiceEntry * | otSrpClientBuffersAllocateService ( otInstance *aInstance) |
|
This function allocates a new service entry from the pool.
|
|
| void | otSrpClientBuffersFreeService ( otInstance *aInstance, otSrpClientBuffersServiceEntry *aService) |
|
This function frees a previously allocated service entry.
|
|
| void | otSrpClientBuffersFreeAllServices ( otInstance *aInstance) |
|
This function frees all previously allocated service entries.
|
|
| char * | otSrpClientBuffersGetServiceEntryServiceNameString ( otSrpClientBuffersServiceEntry *aEntry, uint16_t *aSize) |
|
This function gets the string buffer for service name from a service entry.
|
|
| char * | otSrpClientBuffersGetServiceEntryInstanceNameString ( otSrpClientBuffersServiceEntry *aEntry, uint16_t *aSize) |
|
This function gets the string buffer for service instance name from a service entry.
|
|
| uint8_t * | otSrpClientBuffersGetServiceEntryTxtBuffer ( otSrpClientBuffersServiceEntry *aEntry, uint16_t *aSize) |
|
This function gets the buffer for TXT record from a service entry.
|
|
| const char * | otSrpServerGetDomain ( otInstance *aInstance) |
|
This function returns the domain authorized to the SRP server.
|
|
| otError | otSrpServerSetDomain ( otInstance *aInstance, const char *aDomain) |
|
This function sets the domain on the SRP server.
|
|
| void | otSrpServerSetEnabled ( otInstance *aInstance, bool aEnabled) |
|
This function enables/disables the SRP server.
|
|
| void | otSrpServerGetLeaseConfig ( otInstance *aInstance, otSrpServerLeaseConfig *aLeaseConfig) |
|
This function returns SRP server LEASE and KEY-LEASE configurations.
|
|
| otError | otSrpServerSetLeaseConfig ( otInstance *aInstance, const otSrpServerLeaseConfig *aLeaseConfig) |
|
This function sets SRP server LEASE and KEY-LEASE configurations.
|
|
| void | otSrpServerSetServiceUpdateHandler ( otInstance *aInstance, otSrpServerServiceUpdateHandler aServiceHandler, void *aContext) |
|
This function sets the SRP service updates handler on SRP server.
|
|
| void | otSrpServerHandleServiceUpdateResult ( otInstance *aInstance, otSrpServerServiceUpdateId aId, otError aError) |
|
This function reports the result of processing a SRP update to the SRP server.
|
|
| const otSrpServerHost * | otSrpServerGetNextHost ( otInstance *aInstance, const otSrpServerHost *aHost) |
|
This function returns the next registered host on the SRP server.
|
|
| bool | otSrpServerHostIsDeleted (const otSrpServerHost *aHost) |
|
This function tells if the SRP service host has been deleted.
|
|
| const char * | otSrpServerHostGetFullName (const otSrpServerHost *aHost) |
|
This function returns the full name of the host.
|
|
| const otIp6Address * | otSrpServerHostGetAddresses (const otSrpServerHost *aHost, uint8_t *aAddressesNum) |
|
This function returns the addresses of given host.
|
|
| const otSrpServerService * | otSrpServerHostGetNextService (const otSrpServerHost *aHost, const otSrpServerService *aService) |
|
This function returns the next service of given host.
|
|
| bool | otSrpServerServiceIsDeleted (const otSrpServerService *aService) |
|
This function tells if the SRP service has been deleted.
|
|
| const char * | otSrpServerServiceGetFullName (const otSrpServerService *aService) |
|
This function returns the full name of the service.
|
|
| uint16_t | otSrpServerServiceGetPort (const otSrpServerService *aService) |
|
This function returns the port of the service instance.
|
|
| uint16_t | otSrpServerServiceGetWeight (const otSrpServerService *aService) |
|
This function returns the weight of the service instance.
|
|
| uint16_t | otSrpServerServiceGetPriority (const otSrpServerService *aService) |
|
This function returns the priority of the service instance.
|
|
| const uint8_t * | otSrpServerServiceGetTxtData (const otSrpServerService *aService, uint16_t *aDataLength) |
|
This function returns the TXT record data of the service instance.
|
|
| const otSrpServerHost * | otSrpServerServiceGetHost (const otSrpServerService *aService) |
|
This function returns the host which the service instance reside on.
|
|
Detailed Description
This module includes functions that control SRP client behavior.
This module includes functions of the Service Registration Protocol.
This module includes functions for SRP client buffers and service pool.
Functions in this module are only available when feature OPENTHREAD_CONFIG_SRP_CLIENT_BUFFERS_ENABLE is enabled.
Typedef Documentation
◆ otSrpClientAutoStartCallback
| typedef void(* otSrpClientAutoStartCallback) (const otSockAddr *aServerSockAddr, void *aContext) |
This function pointer type defines the callback used by SRP client to notify user when it is auto-started or stopped.
This is only used when auto-start feature
OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
This callback is invoked when auto-start mode is enabled and the SRP client is either automatically started or stopped.
- Parameters
-
[in] aSeverSockAddressA non-NULL pointer indicates SRP sever was started and pointer will give the selected server socket address. A NULL pointer indicates SRP sever was stopped. [in] aContextA pointer to an arbitrary context (provided when callback was registered).
◆ otSrpClientCallback
| typedef void(* otSrpClientCallback) ( otError aError, const otSrpClientHostInfo *aHostInfo, const otSrpClientService *aServices, const otSrpClientService *aRemovedServices, void *aContext) |
This function pointer type defines the callback used by SRP client to notify user of changes/events/errors.
This callback is invoked on a successful registration of an update (i.e., add/remove of host-info and/or some service(s)) with the SRP server, or if there is a failure or error (e.g., server rejects a update request or client times out waiting for response, etc).
In case of a successful reregistration of an update,
aError
parameter would be
OT_ERROR_NONE
and the host info and the full list of services is provided as input parameters to the callback. Note that host info and services each track its own state in the corresponding
mState
member variable of the related data structure (the state indicating whether the host-info/service is registered or removed or still being added/removed, etc).
The list of removed services is passed as its own linked-list
aRemovedServices
in the callback. Note that when the callback is invoked, the SRP client (OpenThread implementation) is done with the removed service instances listed in
aRemovedServices
and no longer tracks/stores them (i.e., if from the callback we call
otSrpClientGetServices()
the removed services will not be present in the returned list). Providing a separate list of removed services in the callback helps indicate to user which items are now removed and allow user to re-claim/reuse the instances.
If the server rejects an SRP update request, the DNS response code (RFC 2136) is mapped to the following errors:
- (0) NOERROR Success (no error condition) -> OT_ERROR_NONE
- (1) FORMERR Server unable to interpret due to format error -> OT_ERROR_PARSE
- (2) SERVFAIL Server encountered an internal failure -> OT_ERROR_FAILED
- (3) NXDOMAIN Name that ought to exist, does not exist -> OT_ERROR_NOT_FOUND
- (4) NOTIMP Server does not support the query type (OpCode) -> OT_ERROR_NOT_IMPLEMENTED
- (5) REFUSED Server refused for policy/security reasons -> OT_ERROR_SECURITY
- (6) YXDOMAIN Some name that ought not to exist, does exist -> OT_ERROR_DUPLICATED
- (7) YXRRSET Some RRset that ought not to exist, does exist -> OT_ERROR_DUPLICATED
- (8) NXRRSET Some RRset that ought to exist, does not exist -> OT_ERROR_NOT_FOUND
- (9) NOTAUTH Service is not authoritative for zone -> OT_ERROR_SECURITY
- (10) NOTZONE A name is not in the zone -> OT_ERROR_PARSE
- (20) BADNAME Bad name -> OT_ERROR_PARSE
- (21) BADALG Bad algorithm -> OT_ERROR_SECURITY
- (22) BADTRUN Bad truncation -> OT_ERROR_PARSE
- Other response codes -> OT_ERROR_FAILED
The following errors are also possible:
- OT_ERROR_RESPONSE_TIMEOUT : Timed out waiting for response from server (client would continue to retry).
-
OT_ERROR_INVALID_ARGS : The provided service structure is invalid (e.g., bad service name or
otDnsTxtEntry). - OT_ERROR_NO_BUFS : Insufficient buffer to prepare or send the update message.
Note that in case of any failure, the client continues the operation, i.e. it prepares and (re)transmits the SRP update message to the server, after some wait interval. The retry wait interval starts from the minimum value and is increased by the growth factor every failure up to the max value (please see configuration parameter
OPENTHREAD_CONFIG_SRP_CLIENT_MIN_RETRY_WAIT_INTERVAL
and the related ones for more details).
- Parameters
-
[in] aErrorThe error (see above). [in] aHostInfoA pointer to host info. [in] aServiceThe head of linked-list containing all services (excluding the ones removed). NULL if the list is empty. [in] aRemovedServicesThe head of linked-list containing all removed services. NULL if the list is empty. [in] aContextA pointer to an arbitrary context (provided when callback was registered).
◆ otSrpClientService
| typedef struct otSrpClientService otSrpClientService |
This structure represents an SRP client service.
The values in this structure, including the string buffers for the names and the TXT record entries, MUST persist and stay constant after an instance of this structure is passed to OpenThread from
otSrpClientAddService()
or
otSrpClientRemoveService()
.
◆ otSrpServerServiceUpdateHandler
| typedef void(* otSrpServerServiceUpdateHandler) ( otSrpServerServiceUpdateId aId, const otSrpServerHost *aHost, uint32_t aTimeout, void *aContext) |
This function handles SRP service updates.
This function is called by the SRP server to notify that a SRP host and possibly SRP services are being updated. It is important that the SRP updates are not committed until the handler returns the result by calling otSrpServerHandleServiceUpdateResult or times out after
aTimeout
.
A SRP service observer should always call otSrpServerHandleServiceUpdateResult with error code OT_ERROR_NONE immediately after receiving the update events.
A more generic handler may perform validations on the SRP host/services and rejects the SRP updates if any validation fails. For example, an Advertising Proxy should advertise (or remove) the host and services on a multicast-capable link and returns specific error code if any failure occurs.
- Parameters
-
[in] aIdThe service update transaction ID. This ID must be passed back with otSrpServerHandleServiceUpdateResult.[in] aHostA pointer to the otSrpServerHost object which contains the SRP updates. The handler should publish/un-publish the host and each service points to this host with below rules: -
If the host is not deleted (indicated by
otSrpServerHostIsDeleted), then it should be published or updated with mDNS. Otherwise, the host should be un-published (remove AAAA RRs). -
For each service points to this host, it must be un-published if the host is to be un-published. Otherwise, the handler should publish or update the service when it is not deleted (indicated by
otSrpServerServiceIsDeleted) and un-publish it when deleted.
[in] aTimeoutThe maximum time in milliseconds for the handler to process the service event. [in] aContextA pointer to application-specific context. -
If the host is not deleted (indicated by
Enumeration Type Documentation
◆ otSrpClientItemState
| enum otSrpClientItemState |
This enumeration specifies an SRP client item (service or host info) state.
Function Documentation
◆ otSrpClientAddService()
| otError otSrpClientAddService | ( | otInstance * |
aInstance,
|
| otSrpClientService * |
aService
|
||
| ) |
This function adds a service to be registered with server.
After a successful call to this function,
otSrpClientCallback
will be called to report the status of the service addition/registration with SRP server.
The
otSrpClientService
instance being pointed to by
aService
MUST persist and remain unchanged after returning from this function (with
OT_ERROR_NONE
). OpenThread will save the pointer to the service instance.
The
otSrpClientService
instance is not longer tracked by OpenThread and can be reclaimed only when
-
It is removed explicitly by a call to
otSrpClientRemoveService()or removed along with other services by a call tootSrpClientRemoveHostAndServices() and only after theotSrpClientCallback` is called indicating the service was removed. Or, -
A call to
otSrpClientClearHostAndServices()which removes the host and all related services immediately.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aServiceA pointer to a otSrpClientServiceinstance to add.
- Return values
-
OT_ERROR_NONEThe addition of service started successfully. The otSrpClientCallbackwill be called to report the status.OT_ERROR_ALREADYA service with the same service and instance names is already in the list. OT_ERROR_INVALID_ARGSThe service structure is invalid (e.g., bad service name or otDnsTxtEntry).
◆ otSrpClientBuffersAllocateService()
| otSrpClientBuffersServiceEntry * otSrpClientBuffersAllocateService | ( | otInstance * |
aInstance
|
) |
This function allocates a new service entry from the pool.
The returned service entry instance will be initialized as follows:
-
mService.mNamewill point to an allocated string buffer which can be retrieved using the functionotSrpClientBuffersGetServiceEntryServiceNameString(). -
mService.mInstanceNamewill point to an allocated string buffer which can be retrieved using the functionotSrpClientBuffersGetServiceEntryInstanceNameString(). -
mService.mTxtEntrieswill point tomTxtEntry. -
mService.mNumTxtEntrieswill be set to one. -
Other
mServicefields (port, priority, weight) are set to zero. -
mTxtEntry.mKeyis set to NULL (value is treated as already encoded). -
mTxtEntry.mValuewill point to an allocated buffer which can be retrieved using the functionotSrpClientBuffersGetServiceEntryTxtBuffer(). -
mTxtEntry.mValueLengthis set to zero.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- A pointer to the newly allocated service entry or NULL if not more entry available in the pool.
◆ otSrpClientBuffersFreeAllServices()
| void otSrpClientBuffersFreeAllServices | ( | otInstance * |
aInstance
|
) |
This function frees all previously allocated service entries.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
◆ otSrpClientBuffersFreeService()
| void otSrpClientBuffersFreeService | ( | otInstance * |
aInstance,
|
| otSrpClientBuffersServiceEntry * |
aService
|
||
| ) |
This function frees a previously allocated service entry.
The
aService
MUST be previously allocated using
otSrpClientBuffersAllocateService()
and not yet freed. Otherwise the behavior of this function is undefined.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aSeviceA pointer to the service entry to free (MUST NOT be NULL).
◆ otSrpClientBuffersGetHostAddressesArray()
| otIp6Address * otSrpClientBuffersGetHostAddressesArray | ( | otInstance * |
aInstance,
|
| uint8_t * |
aArrayLength
|
||
| ) |
This function gets the array of IPv6 address entries to use as SRP client host address list.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [out] aArrayLengthPointer to a variable to return the array length i.e., number of IPv6 address entries in the array (MUST NOT be NULL).
- Returns
-
A pointer to an array of
otIp6Addressentries (number of entries is returned inaArrayLength).
◆ otSrpClientBuffersGetHostNameString()
| char* otSrpClientBuffersGetHostNameString | ( | otInstance * |
aInstance,
|
| uint16_t * |
aSize
|
||
| ) |
This function gets the string buffer to use for SRP client host name.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [out] aSizePointer to a variable to return the size (number of bytes) of the string buffer (MUST NOT be NULL).
- Returns
- A pointer to char buffer to use for SRP client host name.
◆ otSrpClientBuffersGetServiceEntryInstanceNameString()
| char* otSrpClientBuffersGetServiceEntryInstanceNameString | ( | otSrpClientBuffersServiceEntry * |
aEntry,
|
| uint16_t * |
aSize
|
||
| ) |
This function gets the string buffer for service instance name from a service entry.
- Parameters
-
[in] aEntryA pointer to a previously allocated service entry (MUST NOT be NULL). [out] aSizeA pointer to a variable to return the size (number of bytes) of the string buffer (MUST NOT be NULL).
- Returns
- A pointer to the string buffer.
◆ otSrpClientBuffersGetServiceEntryServiceNameString()
| char* otSrpClientBuffersGetServiceEntryServiceNameString | ( | otSrpClientBuffersServiceEntry * |
aEntry,
|
| uint16_t * |
aSize
|
||
| ) |
This function gets the string buffer for service name from a service entry.
- Parameters
-
[in] aEntryA pointer to a previously allocated service entry (MUST NOT be NULL). [out] aSizeA pointer to a variable to return the size (number of bytes) of the string buffer (MUST NOT be NULL).
- Returns
- A pointer to the string buffer.
◆ otSrpClientBuffersGetServiceEntryTxtBuffer()
| uint8_t* otSrpClientBuffersGetServiceEntryTxtBuffer | ( | otSrpClientBuffersServiceEntry * |
aEntry,
|
| uint16_t * |
aSize
|
||
| ) |
This function gets the buffer for TXT record from a service entry.
- Parameters
-
[in] aEntryA pointer to a previously allocated service entry (MUST NOT be NULL). [out] aSizeA pointer to a variable to return the size (number of bytes) of the buffer (MUST NOT be NULL).
- Returns
- A pointer to the buffer.
◆ otSrpClientClearHostAndServices()
| void otSrpClientClearHostAndServices | ( | otInstance * |
aInstance
|
) |
This function clears all host info and all the services.
Unlike
otSrpClientRemoveHostAndServices()
which sends an update message to server to remove/unregister all the info, this function clears all the info immediately without any interaction with server.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
◆ otSrpClientDisableAutoStartMode()
| void otSrpClientDisableAutoStartMode | ( | otInstance * |
aInstance
|
) |
This function disables the auto-start mode.
This is only available when auto-start feature
OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
Disabling the auto-start mode will not stop the client if it is already running but the client stops monitoring the Thread Network Data to verify that the selected SRP server is still present in it.
Note that a call to
otSrpClientStop()
will also disable the auto-start mode.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
◆ otSrpClientEnableAutoStartMode()
| void otSrpClientEnableAutoStartMode | ( | otInstance * |
aInstance,
|
| otSrpClientAutoStartCallback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
This function enables the auto-start mode.
This is only available when auto-start feature
OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
Config option
OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_DEFAULT_MODE
specifies the default auto-start mode (whether it is enabled or disabled at the start of OT stack).
When auto-start is enabled, the SRP client will monitor the Thread Network Data for SRP Server Service entries and automatically start and stop the client when an SRP server is detected.
If multiple SRP servers are found, a random one will be selected. If the selected SRP server is no longer detected (not longer present in the Thread Network Data), the SRP client will be stopped and then it may switch to another SRP server (if available).
When the SRP client is explicitly started through a successful call to
otSrpClientStart()
, the given SRP server address in
otSrpClientStart()
will continue to be used regardless of the state of auto-start mode and whether the same SRP server address is discovered or not in the Thread Network Data. In this case, only an explicit
otSrpClientStop()
call will stop the client.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aCallbackA callback to notify when client is auto-started/stopped. Can be NULL if not needed. [in] aContextA context to be passed when invoking aCallback.
◆ otSrpClientGetDomainName()
| const char* otSrpClientGetDomainName | ( | otInstance * |
aInstance
|
) |
This function gets the domain name being used by SRP client.
This function requires
OPENTHREAD_CONFIG_SRP_CLIENT_DOMAIN_NAME_API_ENABLE
to be enabled.
If domain name is not set, "default.service.arpa" will be used.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- The domain name string.
◆ otSrpClientGetHostInfo()
| const otSrpClientHostInfo * otSrpClientGetHostInfo | ( | otInstance * |
aInstance
|
) |
This function gets the host info.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- A pointer to host info structure.
◆ otSrpClientGetKeyLeaseInterval()
| uint32_t otSrpClientGetKeyLeaseInterval | ( | otInstance * |
aInstance
|
) |
This function gets the key lease interval used in SRP update requests.
Note that this is the lease duration requested by the SRP client. The server may choose to accept a different lease interval.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- The key lease interval (in seconds).
◆ otSrpClientGetLeaseInterval()
| uint32_t otSrpClientGetLeaseInterval | ( | otInstance * |
aInstance
|
) |
This function gets the lease interval used in SRP update requests.
Note that this is the lease duration requested by the SRP client. The server may choose to accept a different lease interval.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- The lease interval (in seconds).
◆ otSrpClientGetServerAddress()
| const otSockAddr * otSrpClientGetServerAddress | ( | otInstance * |
aInstance
|
) |
This function gets the socket address (IPv6 address and port number) of the SRP server which is being used by SRP client.
If the client is not running, the address is unspecified (all zero) with zero port number.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- A pointer to the SRP server's socket address (is always non-NULL).
◆ otSrpClientGetServices()
| const otSrpClientService * otSrpClientGetServices | ( | otInstance * |
aInstance
|
) |
This function gets the list of services being managed by client.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- A pointer to the head of linked-list of all services or NULL if the list is empty.
◆ otSrpClientIsAutoStartModeEnabled()
| bool otSrpClientIsAutoStartModeEnabled | ( | otInstance * |
aInstance
|
) |
This function indicates the current state of auto-start mode (enabled or disabled).
This is only available when auto-start feature
OPENTHREAD_CONFIG_SRP_CLIENT_AUTO_START_API_ENABLE
is enabled.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- TRUE if the auto-start mode is enabled, FALSE otherwise.
◆ otSrpClientIsRunning()
| bool otSrpClientIsRunning | ( | otInstance * |
aInstance
|
) |
This function indicates whether the SRP client is running or not.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- TRUE if the SRP client is running, FALSE otherwise.
◆ otSrpClientIsServiceKeyRecordEnabled()
| bool otSrpClientIsServiceKeyRecordEnabled | ( | otInstance * |
aInstance
|
) |
This method indicates whether the "service key record inclusion" mode is enabled or disabled.
This function is available when
OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
configuration is enabled.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
- Returns
- TRUE if "service key record inclusion" mode is enabled, FALSE otherwise.
◆ otSrpClientItemStateToString()
| const char* otSrpClientItemStateToString | ( | otSrpClientItemState |
aItemState
|
) |
This function converts a
otSrpClientItemState
to a string.
- Parameters
-
[in] aItemStateAn item state.
- Returns
-
A string representation of
aItemState.
◆ otSrpClientRemoveHostAndServices()
| otError otSrpClientRemoveHostAndServices | ( | otInstance * |
aInstance,
|
| bool |
aRemoveKeyLease
|
||
| ) |
This function starts the remove process of the host info and all services.
After returning from this function,
otSrpClientCallback
will be called to report the status of remove request with SRP server.
If the host info is to be permanently removed from server,
aRemoveKeyLease
should be set to
true
which removes the key lease associated with host on server. Otherwise, the key lease record is kept as before, which ensures that the server holds the host name in reserve for when the client is once again able to provide and register its service(s).
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aRemoveKeyLeaseA boolean indicating whether or not the host key lease should also be removed.
- Return values
-
OT_ERROR_NONEThe removal of host info and services started successfully. The otSrpClientCallbackwill be called to report the status.OT_ERROR_ALREADYThe host info is already removed.
◆ otSrpClientRemoveService()
| otError otSrpClientRemoveService | ( | otInstance * |
aInstance,
|
| otSrpClientService * |
aService
|
||
| ) |
This function requests a service to be unregistered with server.
After a successful call to this function,
otSrpClientCallback
will be called to report the status of remove request with SRP server.
The
otSrpClientService
instance being pointed to by
aService
MUST persist and remain unchanged after returning from this function (with
OT_ERROR_NONE
). OpenThread will keep the service instance during the remove process. Only after the
otSrpClientCallback
is called indicating the service instance is removed from SRP client service list and can be be freed/reused.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aServiceA pointer to a otSrpClientServiceinstance to remove.
- Return values
-
OT_ERROR_NONEThe removal of service started successfully. The otSrpClientCallbackwill be called to report the status.OT_ERROR_NOT_FOUNDThe service could not be found in the list.
◆ otSrpClientSetCallback()
| void otSrpClientSetCallback | ( | otInstance * |
aInstance,
|
| otSrpClientCallback |
aCallback,
|
||
| void * |
aContext
|
||
| ) |
This function sets the callback to notify caller of events/changes from SRP client.
The SRP client allows a single callback to be registered. So consecutive calls to this function will overwrite any previously set callback functions.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aCallbackThe callback to notify of events and changes. Can be NULL if not needed. [in] aContextAn arbitrary context used with aCallback.
◆ otSrpClientSetDomainName()
| otError otSrpClientSetDomainName | ( | otInstance * |
aInstance,
|
| const char * |
aName
|
||
| ) |
This function sets the domain name to be used by SRP client.
This function requires
OPENTHREAD_CONFIG_SRP_CLIENT_DOMAIN_NAME_API_ENABLE
to be enabled.
If not set "default.service.arpa" will be used.
The name string buffer pointed to by
aName
MUST persist and stay unchanged after returning from this function. OpenThread will keep the pointer to the string.
The domain name can be set before client is started or after start but before host info is registered with server (host info should be in either
STATE_TO_ADD
or
STATE_TO_REMOVE
).
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aNameA pointer to the domain name string. If NULL sets it to default "default.service.arpa".
- Return values
-
OT_ERROR_NONEThe domain name label was set successfully. OT_ERROR_INVALID_STATEThe host info is already registered with server.
◆ otSrpClientSetHostAddresses()
| otError otSrpClientSetHostAddresses | ( | otInstance * |
aInstance,
|
| const otIp6Address * |
aIp6Addresses,
|
||
| uint8_t |
aNumAddresses
|
||
| ) |
This function sets/updates the list of host IPv6 address.
Host IPv6 addresses can be set/changed before start or during operation of SRP client (e.g. to add/remove or change a previously registered host address), except when the host info is being removed (client is busy handling a remove request from an earlier call to
otSrpClientRemoveHostAndServices()
and host info still being in either
STATE_TO_REMOVE
or
STATE_REMOVING
states).
The host IPv6 address array pointed to by
aAddresses
MUST persist and remain unchanged after returning from this function (with
OT_ERROR_NONE
). OpenThread will save the pointer to the array.
After a successful call to this function,
otSrpClientCallback
will be called to report the status of the address registration with SRP server.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aAddressesA pointer to the an array containing the host IPv6 addresses. [in] aNumAddressesThe number of addresses in the aAddressesarray.
- Return values
-
OT_ERROR_NONEThe host IPv6 address list change started successfully. The otSrpClientCallbackwill be called to report the status of registering addresses with server.OT_ERROR_INVALID_ARGSThe address list is invalid (e.g., must contain at least one address). OT_ERROR_INVALID_STATEHost is being removed and therefore cannot change host address.
◆ otSrpClientSetHostName()
| otError otSrpClientSetHostName | ( | otInstance * |
aInstance,
|
| const char * |
aName
|
||
| ) |
This function sets the host name label.
After a successful call to this function,
otSrpClientCallback
will be called to report the status of host info registration with SRP server.
The name string buffer pointed to by
aName
MUST persist and stay unchanged after returning from this function. OpenThread will keep the pointer to the string.
The host name can be set before client is started or after start but before host info is registered with server (host info should be in either
STATE_TO_ADD
or
STATE_REMOVED
).
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aNameA pointer to host name label string (MUST NOT be NULL). Pointer to the string buffer MUST persist and remain valid and constant after return from this function.
- Return values
-
OT_ERROR_NONEThe host name label was set successfully. OT_ERROR_INVALID_ARGSThe aNameis NULL.OT_ERROR_INVALID_STATEThe host name is already set and registered with the server.
◆ otSrpClientSetKeyLeaseInterval()
| void otSrpClientSetKeyLeaseInterval | ( | otInstance * |
aInstance,
|
| uint32_t |
aInterval
|
||
| ) |
This function sets the key lease interval used in SRP update requests.
Changing the lease interval does not impact the accepted lease interval of already registered services/host-info. It only affects any future SRP update messages (i.e., adding new services and/or refreshes of existing services).
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aIntervalThe key lease interval (in seconds). If zero, the default value specified by OPENTHREAD_CONFIG_SRP_CLIENT_DEFAULT_KEY_LEASEwould be used.
◆ otSrpClientSetLeaseInterval()
| void otSrpClientSetLeaseInterval | ( | otInstance * |
aInstance,
|
| uint32_t |
aInterval
|
||
| ) |
This function sets the lease interval used in SRP update requests.
Changing the lease interval does not impact the accepted lease interval of already registered services/host-info. It only affects any future SRP update messages (i.e., adding new services and/or refreshes of the existing services).
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aIntervalThe lease interval (in seconds). If zero, the default value specified by OPENTHREAD_CONFIG_SRP_CLIENT_DEFAULT_LEASEwould be used.
◆ otSrpClientSetServiceKeyRecordEnabled()
| void otSrpClientSetServiceKeyRecordEnabled | ( | otInstance * |
aInstance,
|
| bool |
aEnabled
|
||
| ) |
This function enables/disables "service key record inclusion" mode.
When enabled, SRP client will include KEY record in Service Description Instructions in the SRP update messages that it sends.
This function is available when
OPENTHREAD_CONFIG_REFERENCE_DEVICE_ENABLE
configuration is enabled.
- Note
- KEY record is optional in Service Description Instruction (it is required and always included in the Host Description Instruction). The default behavior of SRP client is to not include it. This function is intended to override the default behavior for testing only.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aEnabledTRUE to enable, FALSE to disable the "service key record inclusion" mode.
◆ otSrpClientStart()
| otError otSrpClientStart | ( | otInstance * |
aInstance,
|
| const otSockAddr * |
aServerSockAddr
|
||
| ) |
This function starts the SRP client operation.
SRP client will prepare and send "SRP Update" message to the SRP server once all the following conditions are met:
-
The SRP client is started -
otSrpClientStart()is called. -
Host name is set -
otSrpClientSetHostName()is called. -
At least one host IPv6 address is set -
otSrpClientSetHostName()is called. -
At least one service is added -
otSrpClientAddService()is called.
It does not matter in which order these functions are called. When all conditions are met, the SRP client will wait for a short delay before preparing an "SRP Update" message and sending it to server. This delay allows for user to add multiple services and/or IPv6 addresses before the first SRP Update message is sent (ensuring a single SRP Update is sent containing all the info). The config
OPENTHREAD_CONFIG_SRP_CLIENT_UPDATE_TX_DELAY
specifies the delay interval.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance. [in] aServerSockAddrThe socket address (IPv6 address and port number) of the SRP server.
- Return values
-
OT_ERROR_NONESRP client operation started successfully or it is already running with same server socket address and callback. OT_ERROR_BUSYSRP client is busy running with a different socket address. OT_ERROR_FAILEDFailed to open/connect the client's UDP socket.
◆ otSrpClientStop()
| void otSrpClientStop | ( | otInstance * |
aInstance
|
) |
This function stops the SRP client operation.
This function stops any further interactions with the SRP server. Note that it does not remove or clear host info and/or list of services. It marks all services to be added/removed again once the client is (re)started.
- Parameters
-
[in] aInstanceA pointer to the OpenThread instance.
◆ otSrpServerGetDomain()
| const char* otSrpServerGetDomain | ( | otInstance * |
aInstance
|
) |
This function returns the domain authorized to the SRP server.
If the domain if not set by SetDomain, "default.service.arpa." will be returned. A trailing dot is always appended even if the domain is set without it.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance.
- Returns
- A pointer to the dot-joined domain string.
◆ otSrpServerGetLeaseConfig()
| void otSrpServerGetLeaseConfig | ( | otInstance * |
aInstance,
|
| otSrpServerLeaseConfig * |
aLeaseConfig
|
||
| ) |
This function returns SRP server LEASE and KEY-LEASE configurations.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [out] aLeaseConfigA pointer to an otSrpServerLeaseConfiginstance.
◆ otSrpServerGetNextHost()
| const otSrpServerHost * otSrpServerGetNextHost | ( | otInstance * |
aInstance,
|
| const otSrpServerHost * |
aHost
|
||
| ) |
This function returns the next registered host on the SRP server.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aHostA pointer to current host; use NULL to get the first host.
- Returns
- A pointer to the registered host. NULL, if no more hosts can be found.
◆ otSrpServerHandleServiceUpdateResult()
| void otSrpServerHandleServiceUpdateResult | ( | otInstance * |
aInstance,
|
| otSrpServerServiceUpdateId |
aId,
|
||
| otError |
aError
|
||
| ) |
This function reports the result of processing a SRP update to the SRP server.
The Service Update Handler should call this function to return the result of its processing of a SRP update.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aIdThe service update transaction ID. This should be the same ID provided via otSrpServerServiceUpdateHandler.[in] aErrorAn error to be returned to the SRP server. Use OT_ERROR_DUPLICATED to represent DNS name conflicts.
◆ otSrpServerHostGetAddresses()
| const otIp6Address * otSrpServerHostGetAddresses | ( | const otSrpServerHost * |
aHost,
|
| uint8_t * |
aAddressesNum
|
||
| ) |
This function returns the addresses of given host.
- Parameters
-
[in] aHostA pointer to the SRP service host. [out] aAddressesNumA pointer to where we should output the number of the addresses to.
- Returns
- A pointer to the array of IPv6 Address.
◆ otSrpServerHostGetFullName()
| const char* otSrpServerHostGetFullName | ( | const otSrpServerHost * |
aHost
|
) |
This function returns the full name of the host.
- Parameters
-
[in] aHostA pointer to the SRP service host.
- Returns
- A pointer to the null-terminated host name string.
◆ otSrpServerHostGetNextService()
| const otSrpServerService * otSrpServerHostGetNextService | ( | const otSrpServerHost * |
aHost,
|
| const otSrpServerService * |
aService
|
||
| ) |
This function returns the next service of given host.
- Parameters
-
[in] aHostA pointer to the SRP service host. [in] aServiceA pointer to current SRP service instance; use NULL to get the first service.
- Returns
- A pointer to the next service or NULL if there is no more services.
◆ otSrpServerHostIsDeleted()
| bool otSrpServerHostIsDeleted | ( | const otSrpServerHost * |
aHost
|
) |
This function tells if the SRP service host has been deleted.
A SRP service host can be deleted but retains its name for future uses. In this case, the host instance is not removed from the SRP server/registry.
- Parameters
-
[in] aHostA pointer to the SRP service host.
- Returns
- TRUE if the host has been deleted, FALSE if not.
◆ otSrpServerServiceGetFullName()
| const char* otSrpServerServiceGetFullName | ( | const otSrpServerService * |
aService
|
) |
This function returns the full name of the service.
- Parameters
-
[in] aServiceA pointer to the SRP service.
- Returns
- A pointer to the null-terminated service name string.
◆ otSrpServerServiceGetHost()
| const otSrpServerHost * otSrpServerServiceGetHost | ( | const otSrpServerService * |
aService
|
) |
This function returns the host which the service instance reside on.
- Parameters
-
[in] aServiceA pointer to the SRP service.
- Returns
- A pointer to the host instance.
◆ otSrpServerServiceGetPort()
| uint16_t otSrpServerServiceGetPort | ( | const otSrpServerService * |
aService
|
) |
This function returns the port of the service instance.
- Parameters
-
[in] aServiceA pointer to the SRP service.
- Returns
- The port of the service.
◆ otSrpServerServiceGetPriority()
| uint16_t otSrpServerServiceGetPriority | ( | const otSrpServerService * |
aService
|
) |
This function returns the priority of the service instance.
- Parameters
-
[in] aServiceA pointer to the SRP service.
- Returns
- The priority of the service.
◆ otSrpServerServiceGetTxtData()
| const uint8_t* otSrpServerServiceGetTxtData | ( | const otSrpServerService * |
aService,
|
| uint16_t * |
aDataLength
|
||
| ) |
This function returns the TXT record data of the service instance.
- Parameters
-
[in] aServiceA pointer to the SRP service. [out] aDataLengthA pointer to return the TXT record data length. MUST NOT be NULL.
- Returns
-
A pointer to the buffer containing the TXT record data (the TXT data length is returned in
aDataLength).
◆ otSrpServerServiceGetWeight()
| uint16_t otSrpServerServiceGetWeight | ( | const otSrpServerService * |
aService
|
) |
This function returns the weight of the service instance.
- Parameters
-
[in] aServiceA pointer to the SRP service.
- Returns
- The weight of the service.
◆ otSrpServerServiceIsDeleted()
| bool otSrpServerServiceIsDeleted | ( | const otSrpServerService * |
aService
|
) |
This function tells if the SRP service has been deleted.
A SRP service can be deleted but retains its name for future uses. In this case, the service instance is not removed from the SRP server/registry. It is guaranteed that all services are deleted if the host is deleted.
- Parameters
-
[in] aServiceA pointer to the SRP service.
- Returns
- TRUE if the service has been deleted, FALSE if not.
◆ otSrpServerSetDomain()
| otError otSrpServerSetDomain | ( | otInstance * |
aInstance,
|
| const char * |
aDomain
|
||
| ) |
This function sets the domain on the SRP server.
A trailing dot will be appended to
aDomain
if it is not already there. This function should only be called before the SRP server is enabled.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aDomainThe domain to be set. MUST NOT be NULL.
- Return values
-
OT_ERROR_NONESuccessfully set the domain to aDomain.OT_ERROR_INVALID_STATEThe SRP server is already enabled and the Domain cannot be changed. OT_ERROR_INVALID_ARGSThe argument aDomainis not a valid DNS domain name.OT_ERROR_NO_BUFSThere is no memory to store content of aDomain.
◆ otSrpServerSetEnabled()
| void otSrpServerSetEnabled | ( | otInstance * |
aInstance,
|
| bool |
aEnabled
|
||
| ) |
This function enables/disables the SRP server.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aEnabledA boolean to enable/disable the SRP server.
◆ otSrpServerSetLeaseConfig()
| otError otSrpServerSetLeaseConfig | ( | otInstance * |
aInstance,
|
| const otSrpServerLeaseConfig * |
aLeaseConfig
|
||
| ) |
This function sets SRP server LEASE and KEY-LEASE configurations.
When a non-zero LEASE time is requested from a client, the granted value will be limited in range [aMinLease, aMaxLease]; and a non-zero KEY-LEASE will be granted in range [aMinKeyLease, aMaxKeyLease]. For zero LEASE or KEY-LEASE time, zero will be granted.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aLeaseConfigA pointer to an otSrpServerLeaseConfiginstance.
- Return values
-
OT_ERROR_NONESuccessfully set the LEASE and KEY-LEASE ranges. OT_ERROR_INVALID_ARGSThe LEASE or KEY-LEASE range is not valid.
◆ otSrpServerSetServiceUpdateHandler()
| void otSrpServerSetServiceUpdateHandler | ( | otInstance * |
aInstance,
|
| otSrpServerServiceUpdateHandler |
aServiceHandler,
|
||
| void * |
aContext
|
||
| ) |
This function sets the SRP service updates handler on SRP server.
- Parameters
-
[in] aInstanceA pointer to an OpenThread instance. [in] aServiceHandlerA pointer to a service handler. Use NULL to remove the handler. [in] aContextA pointer to arbitrary context information. May be NULL if not used.