otUdpSocket Struct Reference

This structure represents a UDP socket.

#include < include/openthread/udp.h >

Public Attributes

otSockAddr mSockName
The local IPv6 socket address.
otSockAddr mPeerName
The peer IPv6 socket address.
otUdpReceive mHandler
A function pointer to the application callback.
void * mContext
A pointer to application-specific context.
void * mHandle
A handle to platform's UDP.
struct otUdpSocket * mNext
A pointer to the next UDP socket (internal use only).

This structure represents a UDP socket.


The documentation for this struct was generated from the following file:
  • include/openthread/ udp.h