otDnssdServiceInstanceInfo Struct Reference

This structure represents information of a discovered service instance for a DNS-SD query.

#include < include/openthread/dnssd_server.h >

Public Attributes

const char * mFullName
Full instance name (e.g. "OpenThread._ipps._tcp.default.service.arpa.").
const char * mHostName
Host name (e.g. "ot-host.default.service.arpa.").
uint8_t mAddressNum
Number of host IPv6 addresses.
const otIp6Address * mAddresses
Host IPv6 addresses.
uint16_t mPort
Service port.
uint16_t mPriority
Service priority.
uint16_t mWeight
Service weight.
uint16_t mTxtLength
Service TXT RDATA length.
const uint8_t * mTxtData
Service TXT RDATA.
uint32_t mTtl
Service TTL (in seconds).

This structure represents information of a discovered service instance for a DNS-SD query.


The documentation for this struct was generated from the following file:
  • include/openthread/ dnssd_server.h