Antenna Control

Basic APIs to control the Antenna functionality.

Modules

EFR32
EFR32 Antenna Control FunctionalityThese enumerations and structures are used with RAIL Antenna Control API.

Functions

RAIL_Status_t RAIL_ConfigAntenna ( RAIL_Handle_t railHandle, const RAIL_AntennaConfig_t *config)
Configure antenna path and pin locations.
RAIL_Status_t RAIL_GetRfPath ( RAIL_Handle_t railHandle, RAIL_AntennaSel_t *rfPath)
Get the default RF path.

Detailed Description

Basic APIs to control the Antenna functionality.

Function Documentation

◆ RAIL_ConfigAntenna()

RAIL_Status_t RAIL_ConfigAntenna ( RAIL_Handle_t railHandle,
const RAIL_AntennaConfig_t * config
)

Configure antenna path and pin locations.

Warning
This API must be called before any TX or RX occurs, otherwise the antenna configurations for those functions will not take effect.
Parameters
[in] railHandle A RAIL instance handle.
[in] config A configuration structure applied to the relevant Antenna Configuration registers. A NULL configuration will produce undefined behavior.
Returns
Status code indicating success of the function call.

This function informs RAIL how to select each antenna, but not when. Antenna selection for receive is controlled by the RAIL_RxOptions_t::RAIL_RX_OPTION_ANTENNA0 and RAIL_RxOptions_t::RAIL_RX_OPTION_ANTENNA1 options (and the RAIL_RxOptions_t::RAIL_RX_OPTION_ANTENNA_AUTO combination). Antenna selection for transmit is controlled by the RAIL_TxOptions_t::RAIL_TX_OPTION_ANTENNA0 and RAIL_TxOptions_t::RAIL_TX_OPTION_ANTENNA1 options.

Although a RAIL handle is included for potential future expansion of this function, it is currently not used. That is, only one Antenna configuration can be active on a chip, regardless of the number of protocols (unless the application updates the configuration upon a protocol switch), and the configuration is not saved in the RAIL instance. For optimal future compatibility, pass in a chip-specific handle, such as RAIL_EFR32_HANDLE .

◆ RAIL_GetRfPath()

RAIL_Status_t RAIL_GetRfPath ( RAIL_Handle_t railHandle,
RAIL_AntennaSel_t * rfPath
)

Get the default RF path.

Parameters
[in] railHandle A RAIL instance handle.
[out] rfPath Pointer to RF path.
Returns
A status code indicating success of the function call.

If multiple protocols are used, this function will return RAIL_STATUS_INVALID_STATE if it is called and the given railHandle is not active. In that case, the caller must attempt to re-call this function later, for example when RAIL_EVENT_CONFIG_SCHEDULED trigger.