RAIL_PtiConfig_t Struct Reference

A configuration for PTI.

#include < rail_chip_specific.h >

Data Fields

RAIL_PtiMode_t mode
Packet Trace mode (UART or SPI)
uint32_t baud
Output baudrate for PTI in Hz.
uint8_t doutLoc
Data output (DOUT) location for pin/port.
uint8_t doutPort
Data output (DOUT) GPIO port.
uint8_t doutPin
Data output (DOUT) GPIO pin.
uint8_t dclkLoc
Data clock (DCLK) location for pin/port.
uint8_t dclkPort
Data clock (DCLK) GPIO port.
uint8_t dclkPin
Data clock (DCLK) GPIO pin.
uint8_t dframeLoc
Data frame (DFRAME) location for pin/port.
uint8_t dframePort
Data frame (DFRAME) GPIO port.
uint8_t dframePin
Data frame (DFRAME) GPIO pin.

A configuration for PTI.

Definition at line 786 of file rail_chip_specific.h .

Field Documentation

◆ dclkLoc

uint8_t RAIL_PtiConfig_t::dclkLoc

Data clock (DCLK) location for pin/port.

Only used in SPI mode

Definition at line 798 of file rail_chip_specific.h .

◆ dclkPin

uint8_t RAIL_PtiConfig_t::dclkPin

Data clock (DCLK) GPIO pin.

Only used in SPI mode

Definition at line 802 of file rail_chip_specific.h .

◆ dclkPort

uint8_t RAIL_PtiConfig_t::dclkPort

Data clock (DCLK) GPIO port.

Only used in SPI mode

Definition at line 800 of file rail_chip_specific.h .


The documentation for this struct was generated from the following file:
  • chip/efr32/efr32xg1x/ rail_chip_specific.h