RAIL_CsmaConfig_t Struct Reference

A configuration structure for the CSMA transmit algorithm.

#include < rail_types.h >

Data Fields

uint8_t csmaMinBoExp
The minimum (starting) exponent for CSMA random backoff (2^exp - 1).
uint8_t csmaMaxBoExp
The maximum exponent for CSMA random backoff (2^exp - 1).
uint8_t csmaTries
The number of backoff-then-CCA iterations that can fail before reporting RAIL_EVENT_TX_CHANNEL_BUSY .
int8_t ccaThreshold
The CCA RSSI threshold, in dBm, above which the channel is considered 'busy'.
uint16_t ccaBackoff
The backoff unit period in RAIL's microsecond time base.
uint16_t ccaDuration
The minimum desired CCA check duration in microseconds.
RAIL_Time_t csmaTimeout
An overall timeout, in RAIL's microsecond time base, for the operation.

A configuration structure for the CSMA transmit algorithm.

One of RAIL's schemes for polite spectrum access is an implementation of a Carrier-Sense Multiple Access (CSMA) algorithm based on IEEE 802.15.4 (unslotted).
In pseudo-code it works like this, showing relevant event notifications:

// Return true to transmit packet, false to not transmit packet.
bool performCsma( const RAIL_CsmaConfig_t *csmaConfig)
{
bool isFixedBackoff = ((csmaConfig-> csmaMinBoExp == 0)
&& (csmaConfig-> csmaMaxBoExp == 0));
int backoffExp = csmaConfig-> csmaMinBoExp ; // Initial backoff exponent
int backoffMultiplier = 1; // Assume fixed backoff
int try ;
// Special-case tries == 0 to transmit immediately without backoff+CCA
if (csmaConfig-> csmaTries == 0) {
return true ;
}
// Start overall timeout if specified:
if (csmaConfig-> csmaTimeout > 0) {
StartAbortTimer(csmaConfig-> csmaTimeout , RAIL_EVENT_TX_CHANNEL_BUSY );
// If timeout occurs, abort and signal the indicated event.
}
for ( try = 0; try < csmaConfig-> csmaTries ; try ++) {
if ( try > 0) {
}
// Determine the backoff multipler for this try:
if (isFixedBackoff) {
// backoffMultiplier already set to 1 for fixed backoff
} else {
// Start with the backoff exponent for this try:
if ( try > 0) {
backoffExp++;
if (backoffExp > csmaConfig-> csmaMaxBoExp ) {
backoffExp = csmaConfig-> csmaMaxBoExp ;
}
}
// Pick random multiplier between 0 and 2^backoffExp - 1 inclusive:
backoffMultiplier = pickRandomInteger(0, (1 << backoffExp) - 1);
}
// Perform the backoff:
delayMicroseconds(backoffMultiplier * csmaConfig-> ccaBackoff );
// Perform the Clear-Channel Assessment (CCA):
// Channel is considered busy if radio is actively receiving or
// transmitting, or the average energy detected across duration
// is above the threshold.
if (performCca(csmaConfig-> ccaDuration , csmaConfig-> ccaThreshold )) {
// CCA (and CSMA) success: Transmit after Rx-to-Tx turnaround
StopAbortTimer();
return true ;
} else {
// CCA failed: loop to try again, or exit if out of tries
}
}
// Overall CSMA failure: Don't transmit
StopAbortTimer();
return false ;
}

Definition at line 2583 of file rail_types.h .

Field Documentation

◆ ccaBackoff

uint16_t RAIL_CsmaConfig_t::ccaBackoff

The backoff unit period in RAIL's microsecond time base.

It is multiplied by the random backoff exponential controlled by csmaMinBoExp and csmaMaxBoExp to determine the overall backoff period. For random backoffs, any value above 511 microseconds will be truncated. For fixed backoffs it can go up to 65535 microseconds.

Definition at line 2628 of file rail_types.h .

◆ ccaDuration

uint16_t RAIL_CsmaConfig_t::ccaDuration

The minimum desired CCA check duration in microseconds.

Note
Depending on the radio configuration, due to hardware constraints, the actual duration may be longer. Also, if the requested duration is too large for the radio to accommodate, RAIL_StartCcaCsmaTx() will fail returning RAIL_STATUS_INVALID_PARAMETER .

Definition at line 2637 of file rail_types.h .

◆ csmaMaxBoExp

uint8_t RAIL_CsmaConfig_t::csmaMaxBoExp

The maximum exponent for CSMA random backoff (2^exp - 1).

It can range from 0 to RAIL_MAX_CSMA_EXPONENT and must be greater than or equal to csmaMinBoExp .
If both exponents are 0, a non-random fixed backoff of ccaBackoff duration results.

Definition at line 2607 of file rail_types.h .

◆ csmaMinBoExp

uint8_t RAIL_CsmaConfig_t::csmaMinBoExp

The minimum (starting) exponent for CSMA random backoff (2^exp - 1).

It can range from 0 to RAIL_MAX_CSMA_EXPONENT .

Warning
On EFR32, due to a hardware limitation, this can only be 0 if csmaMaxBoExp is also 0 specifying a non-random fixed backoff. RAIL_STATUS_INVALID_PARAMETER will result otherwise. If you really want CSMA's first iteration to have no backoff prior to CCA, with subsequent iterations having random backoff as the exponent is increased, you must do a fixed backoff of 0 operation first ( csmaMinBoExp = 0, csmaMaxBoExp = 0, ccaBackoff = 0, csmaTries = 1), and if that fails ( RAIL_EVENT_TX_CHANNEL_BUSY ), follow up with a random backoff operation starting at csmaMinBoExp = 1 for the remaining iterations.

Definition at line 2599 of file rail_types.h .

◆ csmaTimeout

RAIL_Time_t RAIL_CsmaConfig_t::csmaTimeout

An overall timeout, in RAIL's microsecond time base, for the operation.

If the transmission doesn't start before this timeout expires, the transmission will fail with RAIL_EVENT_TX_CHANNEL_BUSY . A value 0 means no timeout is imposed.

Definition at line 2644 of file rail_types.h .

◆ csmaTries

uint8_t RAIL_CsmaConfig_t::csmaTries

The number of backoff-then-CCA iterations that can fail before reporting RAIL_EVENT_TX_CHANNEL_BUSY .

Typically ranges from 1 to RAIL_MAX_LBT_TRIES ; higher values are disallowed. A value 0 always transmits immediately without performing CSMA, similar to calling RAIL_StartTx() .

Definition at line 2615 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h