RAIL_ScheduleTxConfig_t Struct Reference

A configuration structure for a scheduled transmit.

#include < rail_types.h >

Data Fields

RAIL_Time_t when
The time when to transmit this packet.
RAIL_TimeMode_t mode
The type of delay.
RAIL_ScheduledTxDuringRx_t txDuringRx
Indicate which action to take with a scheduled TX if it occurs during RX.

A configuration structure for a scheduled transmit.

Definition at line 2481 of file rail_types.h .

Field Documentation

◆ mode

RAIL_TimeMode_t RAIL_ScheduleTxConfig_t::mode

The type of delay.

See the RAIL_TimeMode_t documentation for more information. Be sure to use RAIL_TIME_ABSOLUTE delays for time-critical protocols.

Definition at line 2492 of file rail_types.h .

◆ txDuringRx

RAIL_ScheduledTxDuringRx_t RAIL_ScheduleTxConfig_t::txDuringRx

Indicate which action to take with a scheduled TX if it occurs during RX.

See RAIL_ScheduledTxDuringRx_t structure for more information on potential options.

Definition at line 2498 of file rail_types.h .

◆ when

RAIL_Time_t RAIL_ScheduleTxConfig_t::when

The time when to transmit this packet.

The exact interpretation of this value depends on the mode specified below.

Definition at line 2486 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h