RAIL_MFM_PingPongBufferConfig_t Struct Reference

A configuration structure for MFM Ping-pong buffer in RAIL.

#include < rail_mfm.h >

Data Fields

uint32_t * pBuffer0
pointer to buffer0.
uint32_t * pBuffer1
pointer to buffer1.
uint32_t bufferSizeWords
size of each buffer A and B in 32-bit words.

A configuration structure for MFM Ping-pong buffer in RAIL.

Definition at line 167 of file rail_mfm.h .

Field Documentation

◆ bufferSizeWords

uint32_t RAIL_MFM_PingPongBufferConfig_t::bufferSizeWords

size of each buffer A and B in 32-bit words.

Definition at line 173 of file rail_mfm.h .

◆ pBuffer0

uint32_t* RAIL_MFM_PingPongBufferConfig_t::pBuffer0

pointer to buffer0.

Must be 32-bit aligned.

Definition at line 169 of file rail_mfm.h .

◆ pBuffer1

uint32_t* RAIL_MFM_PingPongBufferConfig_t::pBuffer1

pointer to buffer1.

Must be 32-bit aligned.

Definition at line 171 of file rail_mfm.h .


The documentation for this struct was generated from the following file:
  • common/ rail_mfm.h