RAIL_RfSenseSelectiveOokConfig_t Struct Reference

Structure to configure RFSENSE Selective(OOK) mode.

#include < rail_types.h >

Data Fields

RAIL_RfSenseBand_t band
The frequency band(s) on which to sense the RF energy.
uint8_t syncWordNumBytes
Syncword Length in bytes, 1-4 bytes.
uint32_t syncWord
Sync Word Value.
RAIL_RfSense_CallbackPtr_t cb
The callback function, called when RF is sensed.

Structure to configure RFSENSE Selective(OOK) mode.

Definition at line 3558 of file rail_types.h .

Field Documentation

◆ band

RAIL_RfSenseBand_t RAIL_RfSenseSelectiveOokConfig_t::band

The frequency band(s) on which to sense the RF energy.

To stop RF Sense, specify RAIL_RFSENSE_OFF .

Definition at line 3563 of file rail_types.h .

◆ syncWord

uint32_t RAIL_RfSenseSelectiveOokConfig_t::syncWord

Sync Word Value.

To use HW default sync word, set to RAIL_RFSENSE_USE_HW_SYNCWORD .

Definition at line 3575 of file rail_types.h .

◆ syncWordNumBytes

uint8_t RAIL_RfSenseSelectiveOokConfig_t::syncWordNumBytes

Syncword Length in bytes, 1-4 bytes.

Note
When syncWord is set to use RAIL_RFSENSE_USE_HW_SYNCWORD , the syncWordNumBytes value will be ignored since we rely on the HW default settings for sync word.

Definition at line 3570 of file rail_types.h .


The documentation for this struct was generated from the following file:
  • common/ rail_types.h